If you already have an existing account with another Cat App, you can use the same account to sign in here
One Account. All of Cat.
Your Caterpillar account is the single account you use to log in to select services and applications we offer. Shop for parts and machines online, manage your fleet, go mobile, and more.
Account Information
Site Settings
Security
Your equipment's durability and reliability matter to you. You'll need to conduct machine maintenance if you want to keep your motor grader in the best shape for optimal performance.
To make it simple, we're sharing the best motor grader maintenance tips for making the most of your equipment and boosting your return on investment. Performing regular preventative maintenance tasks can extend the life and improve the functionality of your equipment. Learn more with this motor grader maintenance guide.
Before getting into the specific tasks you should complete for maintaining your equipment, there are some important ways to approach machinery upkeep. The following are considerations for how to maintain a motor grader to the best of your ability:
One of the most important ways to maintain a motor grader is to understand its machinery well. All operators should have training and knowledge about their equipment. Manuals and handbooks give instructions for the best upkeep and operation.
Operators must know what to look for and where to look for to keep motor graders functioning properly and for longer. For example, they should know where to check for leaks. The sooner you identify areas that require extra attention, the sooner you can address the issue and reduce any need for downtime.
Reading the motor grader manual and inspecting your equipment will help you maintain your equipment and get the most out of each piece.
Creating a motor grader maintenance schedule is easy when using the specifications in your equipment manuals and handbooks. There are many instructions for how often you should perform certain tasks. There are suggestions for many maintenance practices, such as the following:
Having a schedule for these tasks allows your team to find issues early. Schedules allow for consistency and better upkeep of motor graders. Let your team know about the maintenance schedule and give your employees specific instructions for sticking with that routine.
It can be especially helpful to keep the schedule posted for your team to reference and ensure all operators are on the same page.
Just as it is important to stick with a schedule, keeping records of every maintenance task your team performs will help you keep a closer eye on your equipment.
Even if they are super simple, detailed records leave less room for overlooking issues with your machine. Records with specific dates and repair information will help your team track recurring problems. Records also allow teams to spend less time figuring out what maintenance you've recently performed to prevent repeated tasks and confusion.
Keeping track of your maintenance also allows you to better monitor your equipment's overall performance. Records let you avoid problems that lead to downtime or more expensive issues.
Being proactive is the best way to keep equipment in its optimal condition. Keeping on top of maintenance efforts for your motor grader will help you stay one step ahead of problems and allow you to protect your equipment before it needs expensive repairs.
If your motor grader is already in need of a repair, tending to this promptly will help you extend the life of your equipment and avoid the need for a replacement. Taking preventive measures will keep your motor grater functioning at its best and operating for longer.
There are many ways to care for your equipment. The following are 10 tips for motor grader maintenance:
Operators should always complete a pre-operation inspection before starting the machinery. This is both for safety reasons and to ensure that the motor grader is ready to get to work. We are sharing more information about what you should look for during your daily equipment walk-around later on.
Before wrapping up for the day, operators should also complete a post-operation inspection. This will help your team identify motor grader areas that need cleaning or further inspection.
Again, routine inspections are incredibly valuable for the health of your equipment. You should be especially mindful when checking engine components.
Your engine is one of the most expensive parts of your machine. To take the best care of it, pay close attention to its components, including the following:
Your motor grader's manual will note optimal timing for maintenance tasks regarding your engine.
Before firing up your motor grader, there are some important things to do first, including:
Performing an oil analysis is incredibly crucial for keeping your equipment running well. Oil is like the blood of your machinery. You should analyze your oil at least every month or every 250 hours for diesel engines. Keep a record of oil sampling and stay ahead of routine upkeep.
It is also important to look for any metal shavings or fluid leakage that should not be in your motor grader's oil.
Keeping your grease points lubricated will allow your equipment to function at its best while reducing wear and tear. In addition to cleaning and servicing your seals, you will want to lubricate the following areas to ensure they are greased and ready for work:
Use your equipment's manual to find all pivot points that require lubrication. Greasing all of the moving parts on your motor grader is crucial because improper lubrication can lead to serious issues and even damage your machinery.
Keeping a close eye on the clevis points and pins where the hydraulic cylinders attach to your motor grader can help you keep dirt and slop from speeding up wear.
The more dirt and debris that gets in these pins, the more damage it can do. As wear develops, your blade is less stable, and your grading will be less accurate.
Checking leaks is a vital part of any routine motor grader maintenance. You can expect a small amount of leakage as the seals on your equipment age. However, you should promptly address leaks of more than just a couple of drops.
Check the circle drive and the blade linkage for leaks. Clean dirt and debris buildup that can lead to damaged seals. Pay attention to leaks from your transmission as well by regularly gauging fluid levels.
Be sure to remove dirt and grime from the engine openings on your machine. This will help keep your engine running properly and reduce unnecessary wear.
Another helpful tip is to wipe away all buildup and grease before opening filler necks and dipsticks to avoid letting dirt in those openings.
Your cooling system is a very valuable part of your machine. It helps to prevent the following conditions:
These things can be detrimental to your equipment, so keeping a close eye on this system will help you maintain your motor grader better. Check coolant levels regularly and add fluid if necessary to keep your equipment up and running.
It is beneficial for operators to check tires regularly. If a tire is damaged or deflated, this can create dangerous driving conditions and negatively impact the performance of your motor grader.
Make it a point to give tires a closer look and gauge their pressure often. Add air promptly to keep your machine ready for work.
There are some tasks that operators should perform every day as part of your motor grader walk-around inspection. Consider the following checklist:
Cat® motor grader maintenance is extremely important for keeping your equipment running properly. Because of this, various Cat dealers offer customer value agreements and extended protection plans to make maintenance simple. These plans vary between dealerships.
A Cat Customer Value Agreement (CVA) is an ownership plan designed to help you keep your equipment in excellent condition. Get the most out of your motor grader with the following benefits:
With a CVA, you can have peace of mind knowing you have easy access to monitoring tools to help you stay on top of your equipment's health management. Explore these options with your local Cat dealer.
Investing in your equipment is a big deal for any owner. You want your motor grader to function properly when you need it. Tackle unexpected repairs with an extended protection plan.
Even the best-built machines eventually need repairs, which always seem to happen at the worst time — right in the middle of a big job, when cash is tight or just after the warranty expires. An Equipment Protection Plan (EPP) for a new or used machine provides coverage beyond the standard machine warranty for parts and labor and protects you from unplanned repair costs. Request more information from your local Cat dealer.
With these tips for maintaining motor graders, you will be able to take better care of your equipment and elongate its life. Our motor grader maintenance checklist makes it easy to keep an eye on the most important parts of your machine.
If you're looking for a motor grader, find a Cat dealer near you or explore the inventory on Cat Used today!