D3 Series Skid Steer Loaders
D3 Series Skid Steer Loaders

New smart creep for Cat® D3 Series Skid Steer Loaders and Compact Track Loaders maximizes work tool productivity

 

For Release Worldwide: January 2022
Release Number: 70PR22

 

Caterpillar will soon launch a new smart creep feature for the full range of Cat® D3 Skid Steer Loaders (SSL) and Compact Track Loaders (CTL) for operating Cat cold planer and wheel saw attachments. Smart creep senses the load on the attachment and automatically adjusts the drive command to keep the cold planer or wheel saw running at the most productive speed.

A combination of attachment sensors and proprietary software optimally balances attachment load and machine speed to maximize productivity. By continually sensing the load on the attachment, smart creep increases machine speed when encountering less resistance and automatically slows the machine when encountering higher load. Engine load remains constant, while the operator can monitor hydraulic pressure on the in-cab display panel.

Smart creep takes the guess work out of setting the right creep speed for operating the attachment. Without the aid of this feature, setting creep speed too fast can lead to stalling the attachment, and too slow of speed results in productivity loss. Smart creep software smoothly and efficiently determines the optimal machine speed for cutting conditions.

With this new smart attachment feature from Caterpillar, the operator needs only to activate the standard creep control system and set the maximum creep speed on the advanced display inside the cab. Once the tool engages the cut, smart creep measures load on the attachment and adjusts the drive command automatically as cutting begins. In the event of the cutter jamming or stalling, an auto reverse feature within smart creep quickly changes machine direction to allow the tool to clear the jam.

Targeted availability for smart creep on Cat D3 SSL and CTL machines is the third quarter of 2022. A field installation kit consisting of sensors and machine software for operating the new feature will be made available for existing fleet loaders and attachments. Once commercially available, new cold planer and wheel saw purchases will be shipped from the factory with the required hardware installed, and new D3 SSL and CTL models will come smart creep ready from the factory.

More information about Cat D3 Skid Steer Loaders and Compact Track Loaders, smart attachments, and new smart creep can be found by contacting the local Cat dealer or visiting: https://www.cat.com.

 

of

Cat 279D3 Compact Track Loader with PC306 Cold Planer attachment planing asphalt.

View Full Size Image
of

Cat 279D3 Compact Track Loader with PC306 Cold Planer attachment planing asphalt.

View Full Size Image
of

Cat 279D3 Compact Track Loader with PC306 Cold Planer attachment planing asphalt.

View Full Size Image
of

**Video is currently unlisted, but will go live with the release**

Product & Service News

See the latest product and engine announcements from Caterpillar.

See the Latest News

 

# # #

Note to Editors: Caterpillar rolls out products and services in each of its territories at different time intervals. Although every effort is made to ensure that product information is released only after Caterpillar has received confirmation from our dealer network, our plants, and our marketing subsidiaries that products and services are available in the relevant region, editors are kindly requested to verify with their local dealer for product availability and specifications.

CAT, CATERPILLAR, LET’S DO THE WORK, their respective logos, “Caterpillar Corporate Yellow,” the “Power Edge” and Cat “Modern Hex” trade dress, as well as corporate and product identity used herein, are trademarks of Caterpillar and may not be used without permission.

©2022 Caterpillar All Rights Reserved 

 

Press Inquiries

Caterpillar Trade Press Media Representatives

Americas

Sharon Holling: Holling_Sharon_L@cat.com

Johanna Kelly: Kelly_Johanna_L@cat.com

Europe, Africa, Middle East

Francine Shore: Shore_Francine_M@cat.com