Global Operator Challenge
Global Operator Challenge

New Cat® AD63 Underground Articulated Truck Features Increased Payload, Advanced Emissions Controls, Enhanced Comfort and Serviceability

 

 

For Worldwide Release, excluding China: April 2020
Release Number: 317PR20

The new Cat® AD63 Underground Articulated Truck features 5 percent increased payload and more torque for enhanced production capabilities, compared to its predecessor, the AD60. The new AD63 also can be configured to meet the strictest diesel engine emissions regulations—for both regulatory compliance and improved underground air quality.

Additional new features enhance operator ergonomics, maintenance access and safety, and data collection for machine health monitoring. The AD63, with 63 tonnes (69 tons) payload, becomes the largest underground truck in the Caterpillar product line. The new model will be available in late 2020.

Powertrain performs

The new truck is powered by the proven Cat C27 diesel engine, which produces 588 kW (789 hp), meets EU Stage V emission standards and is approved by CANMET for use in underground mines. The AD63 does not require Diesel Exhaust Fluid (DEF) to meet these standards. The emissions control system maintains the ability to use diesel particulate filters, such as the Cat Wall Flow Filter, to further reduce particulate emissions.

The AD63 powertrain also features a new torque converter gear ratio to increase peak torque and improve gear retention on variable grades. The optimized transmission shift strategy results in smoother uphill driving and greater operator comfort. The new torque converter also increases rimpull when driving away from a stop.

The AD63 engine package has extended altitude capability—from negative 3048 m (10,000 ft) to positive 1524 m (5,500 ft). The new engine cooling package maintains capabilities at high ambient temperatures. The new design and routing of cooling air improves serviceability, and the radiator core has serviceable tubes for fast repairs.   

Cab built for people

In the AD63 cab, the ducted ventilation and air conditioning system gives the truck operator full control with nine adjustable louvers for comfortable cooling and efficient defogging. The HVAC system is powered by a battery electric system so that it can be operated when the engine is not running, which pays off in less engine idling and lower operating costs.

The new cab arrangement features a forward-facing trainer seat offering increased space and comfort for the trainer. The new tilt cab feature gives maintenance personnel the ability to tilt the cab for access to the cab side of the engine for easier and faster access to components. Outside the cab, a redesigned access ladder and fold-flat handrails enhance safety during maintenance.

Technology aids

The new AD63 incorporates Product Link™ Elite as standard equipment to enable data collection and equipment health monitoring. The system enables sharing data across multiple destinations, reduces gaps in data or lost data due to network issues, and has direct connectivity to Caterpillar and Cat dealers for remote support and services, such as condition monitoring.

The AD63 also has external displays showing the weight of the truck contents to the loader operator. Instant feedback for the loader operator enables more efficient passes and optimum truck loads. Displays are on both sides of the truck.  

In addition to new technology, Caterpillar has added the option of a new lightweight dump body, with 38.3 m3 capacity. The AD63 maintains commonality with other AD60 bodies.

For more information about the AD63 Underground Truck, contact the local Cat dealer or go to: www.cat.com/underground.

 

of

Cat AD63 underground articulated truck, front quarter view

of

Cat AD63 underground articulated truck, side view

 

 

Product & Service News

See the latest product and engine announcements from Caterpillar.

See the Latest News

 

 

# # #

Note to Editors: Caterpillar rolls out products and services in each of its territories at different time intervals. Although every effort is made to ensure that product information is released only after Caterpillar has received confirmation from our dealer network, our plants, and our marketing subsidiaries that products and services are available in the relevant region, editors are kindly requested to verify with their local dealer for product availability and specifications.

CAT, CATERPILLAR, LET’S DO THE WORK, their respective logos, “Caterpillar Corporate Yellow,” the “Power Edge” and Cat “Modern Hex” trade dress, as well as corporate and product identity used herein, are trademarks of Caterpillar and may not be used without permission.

VisionLink is a trademark of Trimble Navigation Limited, registered in the United States and in other countries.

©2020 Caterpillar All Rights Reserved

 


Press Inquiries

Caterpillar Trade Press Media Representatives

Americas

  Sharon Holling: Holling_Sharon_L@cat.com

  Johanna Kelly: Kelly_Johanna_L@cat.com

Europe, Africa, Middle East

   Francine Shore: Shore_Francine_M@cat.com