If you already have an existing account with another Cat App, you can use the same account to sign in here
One Account. All of Cat.
Your Caterpillar account is the single account you use to log in to select services and applications we offer. Shop for parts and machines online, manage your fleet, go mobile, and more.
Account Information
Site Settings
Security
For Worldwide Release: June 2021
Release Number:489PR21
Themed “Together, we’re mining better,” Caterpillar’s MINExpo 2021 experience celebrates the company’s partnership with mines and the ways it assists customers to mine more efficiently, effectively, safely and sustainably. The 5124-m2 (55,000-ft2) exhibit will feature a broad range of product displays, new equipment introductions, previews of what the future holds and remote operating stations.
The exhibit will be grouped under three specific core areas: environmental, social, and corporate governance (ESG) and sustainability; technology and automation; and equipment lifecycle management solutions.
“After waiting an extra year, the mining industry is ready to reconnect at MINExpo. We are excited to show our customers and the industry the advancements Caterpillar has made not only in equipment, technology and services but also in how we are helping customers mine more sustainably,” comments Caterpillar Resource Industries Group President Denise Johnson. “While we are eager to exhibit in Las Vegas, we recognize that many of our dealers and customers will not be able to travel to the show. Therefore, we are also creating a digital Caterpillar experience at cat.com/mining, where we will place MINExpo specific content.”
Mining sustainably
Central to Caterpillar’s commitment to mining better together is helping customers meet their ESG goals and build sustainable mine sites of the future. Recognizing that one size doesn’t fit all, Caterpillar has followed a strategic approach with a long-term vision of discovering, developing and delivering a broad portfolio of products, technologies, services and solutions. This portfolio allows Caterpillar to provide a full site approach, which combines offerings with integration expertise to identify and provide the best possible solution for each specific mine.
Vital to the vision of the all-electric underground mine of the future, the new Cat® R1700 XE LHD will feature 100% battery electric propulsion that generates significantly less heat and noise. It offers a 15-tonne (16.5-ton) payload, 24 190-kg (53,330-lb) lift and tilt breakout force, and 18 km/h (11.2 mph) top speed. To optimize runtime and improve safety, batteries stay on the machine for charging.
Fully charging the R1700 XE in as little as 20 minutes, the new portable Cat MEC500 Mobile Equipment Charger is the first of its kind in the industry. It can be moved via towing, fork truck, or the R1700 XE and eliminates the need for regular battery handling and swapping.
The new R2900 XE LHD diesel-electric drive train on display features a significant reduction in maintenance and repair costs, while minimizing emissions. Its redesigned lift arm and components deliver up to a 39% improved lift breakout force over the R2900G, making this model up to 31 tonnes per liter more fuel efficient.
Caterpillar is set to unveil the world’s largest, most powerful and efficient electric drive dozer with high drive. The new Cat D11 XE dozer will be the most advanced, lowest emission-per-ton dozer in the industry, built to deliver the lowest cost of bank cubic meters (BCM) ever. Exhibited alongside the D11 XE, the new Cat D10 dozer offers up to 4% less fuel consumption than the previous model, up to 3% more productivity with high-horsepower reverse and up to 6% more efficiency with combined load-sensing hydraulics and stator clutch torque divider.
The recently introduced Cat 992 Wheel Loader delivers up to a 32% increase in productivity. It reduces maintenance costs by up to 10% and has demonstrated in-field testing up to 48% greater payload-per-fuel efficiency in applications where a four-pass match to 90.7-tonne (100-ton) trucks was achieved versus five passes with the 992K.
Caterpillar is committed to helping our customers with their energy transitions, and the MINExpo exhibit will include a range of renewable and storable power displays, including the Cat Microgrid system. The Cat 3516 engine will feature dynamic gas blending (DGB), which allows mines to save fuel and reduce emissions without sacrificing diesel performance.
Driving technology and automation
Achieving sustainability goals requires mines to continually strive for operational improvement. Fully optimizing operations delivers the highest safety and productivity at the lowest cost and least possible environmental impact.
“Technology and automation are critical components for substantially improving machine uptime availability and productivity,” offers Marc Cameron, Vice President, Caterpillar Resource Industries. “Through Cat® MineStar™ Solutions, Caterpillar offers customers scalable technologies to fit the mine’s specific needs. The exhibit’s technology and automation stage will focus on the real value that Caterpillar technology options provide customers.”
MINExpo will be the first opportunity for many attendees to learn more about the recently introduced Cat MineStar Edge. It brings visibility to the entire mining operation to show how activities early in the process impact those further down the value chain. MineStar Edge makes it possible to measure, manage, analyze and improve the entire mining operation.
Equipped with MineStar Command for hauling, the new Cat 777G Water Truck provides a glimpse into the future for autonomously lowering dust levels at the mine site while maintaining haul road safety. Featuring the market’s first autonomous water delivery system, the machine integrates truck, tank and sprayer and knows where and when to water haul roads.
Representing the Caterpillar fleet of autonomous trucks, the displayed Cat 794 AC electric drive will be factory-installed with Cat MineStar Command for hauling. Recently, autonomous trucks using Command for hauling surpassed 3 billion tonnes of material hauled, safely traveling more than 110 million km (68.3 million mi).
Accurate to the centimeter, the exhibited Cat MD6310 rotary blasthole drill offers technology, efficiency, safety and productivity improvements. Fully integrating Caterpillar’s proven components and systems, including technology and automation, the drill is capable of up to
42 149 kg (92,922 lb) of bit load and targets 203- to 311-mm (8- to 12.5-in) hole diameters.
Exhibiting how technology can improve safety at the mine site, the Cat MineStar Detect Driver Safety System (DSS) display details how the system monitors eye-closure and head pose to alert the driver via seat vibration and/or audio alarm the moment fatigue or distraction is identified. DSS has been shown to reduce 97% of the most significant fatigue events, 80% of average fatigue events and 91% of distraction events.
Several Cat Command stations and trailers will be on display for attendees to experience effective remote control and semi-autonomous drilling, dozing and underground operations from many kilometers away.
Lifecycle solutions
From individual offerings to comprehensive solutions, Caterpillar and Cat dealers offer dozens of equipment management services designed to improve overall machine performance and mine site productivity. Component rebuilds, retrofits, aftermarket solutions and service agreements help customers get the most out of their investments. Dealer-provided Customer Value Agreements (CVAs) allow customers to focus on their core competency – mining.
Highlighting Caterpillar’s Remanufacturing services capability, the C175-16 Cat Reman engine on display, which produces up to 2550 kW (3,420 hp), reduces overall owning and operating costs.
Team members will also be available to explain to attendees how MineStar Health maximizes equipment availability and reliability by connecting the machine to the office. The service assists with proactive maintenance services and predictive equipment analysis by collecting equipment data, monitoring critical machine parameters, obtaining real-time alerts, analyzing operational trends and patterns, predicting failures and receiving repair recommendations.
Partnership and expertise
In addition to teams of workers with machine and technology expertise, representatives of Cat Financial and Cat Solutions will be on hand to share information on safety, fleet management and productivity offerings that can be combined into full site solutions.
A ThoroughTec® Simulation training will provide an opportunity to experience the 7495 Electric Rope Shovel. In addition, attendees will be able to experience two next generation machine cabs – one for mining trucks and another for the 6060 hydraulic mining shovel – via actual cabs on display.
Caterpillar invites all MINExpo 2021 attendees to visit its Central Hall exhibit, #6229, at the Las Vegas Convention Center from September 13-15. For more information about how Caterpillar and customers are mining better together, visit www.cat.com/mining.
# # #
Note to Editors: Caterpillar rolls out products and services in each of its territories at different time intervals. Although every effort is made to ensure that product information is released only after Caterpillar has received confirmation from our dealer network, our plants, and our marketing subsidiaries that products and services are available in the relevant region, editors are kindly requested to verify with their local dealer for product availability and specifications.
CAT, CATERPILLAR, LET’S DO THE WORK, their respective logos, “Caterpillar Corporate Yellow,” the “Power Edge” and Cat “Modern Hex” trade dress, as well as corporate and product identity used herein, are trademarks of Caterpillar and may not be used without permission.
©2021 Caterpillar All Rights Reserved
Press Inquiries |
Caterpillar Trade Press Media Representatives Americas Sharon Holling: Holling_Sharon_L@cat.com Johanna Kelly: Kelly_Johanna_L@cat.com Europe, Africa, Middle East Francine Shore: Shore_Francine_M@cat.com |
Reader Requests |