Cat D5, D6, and D7 Medium Dozers
Cat D5, D6, and D7 Medium Dozers

Caterpillar Now Offers Command Remote Operation for Cat D5, D6, and D7 Medium Dozers

For Release in North America and Japan: November 2021
Release Number: 850PR21


To boost jobsite safety in hazardous dozing conditions, Caterpillar announces the expansion of Command remote machine operation to Cat® D5, D6, and D7 Dozers. Command for Dozing removes operators from the cab and offers remote operating from a safe distance in applications such as overburden/reclamation work, ripping overburden or leach pads, slurry pond dozing, and operation around hazardous materials or unstable surfaces.

Next generation dozers are shipped from the factory remote ready, making field installation fast with only a few additional parts required. With Command fully integrated with the machine’s electronic and hydraulic systems, remote operation delivers quick response, smooth control and virtually no latency. Companies have the option of equipping dozers with line-of-sight (LOS) or non-line-of-sight (NLOS) operation, and a ground-level switch quickly toggles between manual and remote dozer operation. To help improve jobsite productivity, Command allows production to restart immediately following disruptive processes, such as blasting in quarry applications.

Beyond improving safe operation and increasing productivity, Command for Dozing offers a potential solution to worker shortages and added training opportunities for newer operators. By allowing the operator to work outside the machine, Command opens opportunities to those with physical limitations which prevent them from climbing into the equipment. It can attract a new generation of worker while increasing the longevity of experienced operators.

Two options, precise control

Portable and lightweight, the Command console (LOS) allows workers to work outside of the cab while remaining on site and in direct visual contact with the dozer. With its range reaching 437 yd (499 m), the console positions the user for optimum visibility. Requiring no on-site communications infrastructure, it is ideal for short-term and emergency remote operation. An ergonomic console layout features intuitive controls with ISO symbols that provides access to all dozer functions, while an LED display offers clear readout of machine status.

Furthering operation simplicity, the console (LOS) system supports multiple assist technologies the operator would have from inside the cab, including traction control, AutoCarry and stable blade. Unlocking with an electronic access card, the console can be configured to control another machine equipped with Command by simply changing out an RFID chip. Its lithium-ion battery provides a quick charge and long run times in varying ambient temperatures. Built-in safety features stop all dozer movements if the remote shutdown switch is pressed, wireless communication is lost, or the console is tilted more than 45 degrees.

The Command station provides non-line-of-site operation from the comfort of an air-conditioned office on-site or many miles away, as distance is limited only by the capabilities of the wireless network. By eliminating the fatigue-inducing vibration of machine movements in the cab, operators can work with less fatigue. The configurable station features a similar feel to the cab with familiar controls, complete with pedals, joysticks, adjustable seat, switches and storage. Multiple screen displays offer visuals from the left and right cutting edges, blade top-center and rearview that includes the ripper.

Beyond supporting assist technologies offered by the console (LOS), the Command station (NLOS) offers compatibility with blade load monitor, slope assist and Grade with 3D with the same response time as in the cab. Users can easily switch to operating a different Command-equipped machine – dozer, wheel loader or excavator - from the same or different sites with virtually no downtime for shift changes or for travel to the jobsite.

 

 

of

Cat® Command Stations in an office environment being used to remotely control machines.

of

Cat® Command Console being used on a jobsite.

of

Cat® Command Console being used to remotely operator a dozer near a hillside drop off.

of

Cat® dozer being controlled by an operator using a Command console.

Product & Service News

See the latest product and engine announcements from Caterpillar.

See the Latest News

 

# # #

 

Note to Editors: Caterpillar rolls out products and services in each of its territories at different time intervals. Although every effort is made to ensure that product information is released only after Caterpillar has received confirmation from our dealer network, our plants, and our marketing subsidiaries that products and services are available in the relevant region, editors are kindly requested to verify with their local dealer for product availability and specifications.

CAT, CATERPILLAR, LET’S DO THE WORK, their respective logos, “Caterpillar Corporate Yellow,” the “Power Edge” and Cat “Modern Hex” trade dress, as well as corporate and product identity used herein, are trademarks of Caterpillar and may not be used without permission.

©2021 Caterpillar All Rights Reserved

 

Press Inquiries

Caterpillar Trade Press Media Representatives

Americas

Sharon Holling: Holling_Sharon_L@cat.com

Johanna Kelly: Kelly_Johanna_L@cat.com

Europe, Africa, Middle East

Francine Shore: Shore_Francine_M@cat.com