Small Wheel Loader
Small Wheel Loader

Cat® Small Wheel Loaders Receive Attachment Visibility, Comfort and Performance Enhancements

Cat® 930M wheel loader now meets Stage V emissions standards 

For Release in North America, Europe, Japan, Australia, New Zealand: October 2019 
Release Number: 844PR19

Caterpillar launches several new design enhancements for its Small Wheel Loader (SWL) line – Cat® 926M, 930M and 938M models – centered on improving attachment visibility, operator comfort and machine performance. Integrating large wheel loader features into the Cat SWL models, these new machines deliver improved operating efficiency, reduced maintenance and increased loader longevity.

Enhanced attachment visibility

The SWL line’s new Fusion Quick Coupler substantially improves visibility to the attachment in material handling applications. With its electro-hydraulic coupler application system activated conveniently from inside the cab, the single piece cast coupler frame with relocated actuation cylinders increase attachment visibility through the coupler by up to 85 percent while maintaining the benefits of the fusion system.

Increasing SWL versatility, an improved Fusion Coupler carriage for fork attachments is now available with a new carriage designed to enhance attachment visibility and to work in conjunction with the new high-visibility cast Fusion Coupler. The line’s new adjustable material handling arm delivers increased visibility, simple adjustments and easy transport with a General Purpose bucket.

A new cast torque tube design for the new Cat 930M and 938M models significantly improves operator visibility to the attachment when it’s in a raised position. The new standard lift arms offer 100 percent more fork tip/heel visibility and 50 percent more bucket edge visibility to improve operating efficiency. Updated hose routing close to the side of the lift arms help to improve visibility when equipped with the 3rd function auxiliary lines grouping.

Lighting

Whether starting the workday before sunrise or working well after sunset, available LED lighting options help improve machine visibility. Featuring integrated LED indicators, new high-performance LED front roading lights improve light coverage in dipped and main beam modes. A new auxiliary lighting package now includes a light inside the Diesel Exhaust Fluid (DEF) fill tank compartment to improve visibility in low-light conditions.

The new standard for operating comfort

New fabric designs improve airflow for the range of seat options on all Cat SWL models. The seat upgrades keep the operator comfortable throughout the work shift, making the relaxed operator more efficient. All seats incorporate high visibility orange seat belts that allow crew members to see, at a glance, if the operator is wearing the seatbelt.

Featuring a bottom cushion and backrest that are heated and cooled, the top-of-the-line leather/fabric air-suspension Premium Seat is fully adjustable with a high backrest, headrest, air lumbar support, armrests and cushion tilt. The heated air-suspension Deluxe Seat is fully adjustable, fabric covered and has mid-backrest, headrest, mechanical lumbar support, armrests, and cushion tilt. The fully adjustable, fabric covered, mechanical suspension Standard Seat features a mid-backrest, headrest and armrests.

A new benchmark for loader performance

Beyond lift-arm and quick-coupler updates, the new Cat 930M resets the benchmark in SWL machine performance and refinement. Powered by the Cat C7.1 engine, the re-engineered 930M now meets EU Stage V emissions standards along with U.S. EPA Tier 4 Final and Japan 2014 standards. The new 930M also delivers a 5 percent boost in gross horsepower, 5 percent increase in breakout force and a 5 percent higher full-turn tip load when compared to the previous 930M.

With the new updates and refinements, the new 930M with Aggregate Handler package now aligns in a higher performance class. This offers customers lower end-to-end costs and reduced owning/operating costs compared to running a larger wheel loader.

Configured for success

These new SWL loaders now seamlessly integrate several options commonly found on large and medium Cat wheel loaders. Contractors can now choose to equip their small loaders with Cat Production Management (CPM*), Autolube, tire pressure monitoring (TPM) and hydraulic load check valves.

CPM confirms sufficient weight in the bucket before the operator leaves the pile, ensuring the right amount of material is loaded to reduce the number of cycles and maximize profit potential. Cat Autolube fully integrates into the loader’s structure and in-cab display to ensure machine pivot points are automatically greased properly with the right amount of grease, without over greasing, to significantly reduce the daily maintenance routine. With a quick glance at the cab’s secondary display, the operator easily sees current tire pressures on loaders equipped with TPM, and the system provide alerts if tire pressures drop too low or increases too high, which can affect stability and increase tire wear and fuel burn if not noticed or corrected.

More information on enhancements to the Cat SWL line can be found by visiting your local Cat dealer or www.cat.com.

*Not legal for trade

 

 

of

Cat 938M Aggregate Handler SWL

of

Cat 938M Aggregate Handler SWL

of

Cat 938M SWL cab

of

Cat 938M SWL cab

of

Cat 938M SWL with forks

of

Cat 938M SWL in a millyard

of

Cat 938M SWL in snow removal application

Product & Service News

See the latest product and engine announcements from Caterpillar.

See the Latest News

                                                                                                                                                     

                                                                                                                                                         # # #

 

Note to Editors: Caterpillar rolls out products and services in each of its territories at different time intervals. Although every effort is made to ensure that product information is released only after Caterpillar has received confirmation from our dealer network, our plants, and our marketing subsidiaries that products and services are available in the relevant region, editors are kindly requested to verify with their local dealer for product availability and specifications.

CAT, CATERPILLAR, their respective logos, “Caterpillar Yellow” and the “Power Edge” trade dress, as well as corporate and product identity used herein, are trademarks of Caterpillar and may not be used without permission.

                                                                                                                          ©2018 Caterpillar All Rights Reserved

 

Press Inquiries

Caterpillar Trade Press Media Representatives

Americas

Sharon Holling: Holling_Sharon_L@cat.com

Johanna Kelly: Kelly_Johanna_L@cat.com

Europe, Africa, Middle East

Francine Shore: Shore_Francine_M@cat.com

Reader Requests

www.cat.com/requestCatinfo