If you already have an existing account with another Cat App, you can use the same account to sign in here
One Account. All of Cat.
Your Caterpillar account is the single account you use to log in to select services and applications we offer. Shop for parts and machines online, manage your fleet, go mobile, and more.
Account Information
Site Settings
Security
For Release in North America, South America: April 2020
Release Number: 304PR20
Cat® pin grabber couplers bring a new level of productivity allowing the operator to change tools in a matter of seconds rather than minutes. Excavators of similar sizes can share attachments. With the addition of the VB and HB sizes of pin grabber couplers, there is now a coupler for every size of excavator from the 311 – 390. VB and HB refer to linkage sizes. Caterpillar classifies excavator fronts according to the “linkage family,” which is the size at the end of the stick. Pin grabber couplers are weighted to handle big payloads when added to a machine and bucket combination, without having to compromise on the bucket size.
Pin grabber couplers feature a redundant locking system, ensuring attachments are secure to the coupler. The spring-loaded arms keep the latch closed, even in the event of a hydraulic pressure loss. The shorter profile of the coupler helps keep the distance from the end of the machine’s stick to the tip of the bucket’s teeth compact, to maximize the amount of digging power you have with the addition of the coupler. The coupler frame’s cast pieces are made from abrasion-resistant steel to maintain the coupler’s durability over time.
The coupler has visual and audible cues for the operator to indicate it is secure to the attachment. The primary greasing block is the central greasing point for the whole coupler and is easily accessible at ground level. Operating procedures for the pin grabbers are intuitive and simple to learn for operators of all experience levels. Adding the versatility of a pin grabber coupler allows you to switch from digging, grading, material handling, compacting soil, breaking rocks, and more with ease. Using the pin grabber coupler also gives you the ability to pick a bucket up in reverse position to clean out square corners.
Linkage/ |
Minimum Carrier Weight |
Maximum Carrier Weight |
Coupler Weight |
|
Tons |
Tons |
kg |
lb. |
|
312 |
11 |
15 |
188 |
414 |
315 |
15 |
18 |
299 |
659 |
B |
19 |
23 |
380 |
837 |
CB-Trenching |
24 |
35 |
430 |
949 |
CB |
24 |
35 |
465 |
1025 |
DB-Narrow Profile |
30 |
40 |
624 |
1376 |
DB |
30 |
40 |
621 |
1370 |
TB-Trenching |
45 |
52 |
934 |
2060 |
TB |
45 |
52 |
944 |
2082 |
VB2 |
74 |
74 |
1244 |
2744 |
HB2 |
90 |
95 |
1556 |
3430 |
For a complete list of Pin Grabber Coupler models and specifications, visit cat.com.
# # #
Note to Editors: Caterpillar rolls out products and services in each of its territories at different time intervals. Although every effort is made to ensure that product information is released only after Caterpillar has received confirmation from our dealer network, our plants, and our marketing subsidiaries that products and services are available in the relevant region, editors are kindly requested to verify with their local dealer for product availability and specifications.
CAT, CATERPILLAR, LET’S DO THE WORK, their respective logos, “Caterpillar Yellow,” the “Power Edge” and Cat “Modern Hex” trade dress, as well as corporate and product identity used herein, are trademarks of Caterpillar and may not be used without permission.
©2020 Caterpillar All Rights Reserved
Press Inquiries |
Caterpillar Trade Press Media Representatives Americas Sharon Holling: Holling_Sharon_L@cat.com Johanna Kelly: Kelly_Johanna_L@cat.com Europe, Africa, Middle East Francine Shore: Shore_Francine_M@cat.com |
Reader Requests |
www.cat.com/requestCatinfo |