If you already have an existing account with another Cat App, you can use the same account to sign in here
One Account. All of Cat.
Your Caterpillar account is the single account you use to log in to select services and applications we offer. Shop for parts and machines online, manage your fleet, go mobile, and more.
Account Information
Site Settings
Security
For Worldwide Release: February 24, 2020
Release Number: EEPR0120
DEERFIELD, IL – Caterpillar Inc. today announced the introduction of six new 50-Hz standby ratings that deliver industry-leading power density while helping to reduce overall site preparation, transportation, installation and maintenance costs.
Caterpillar now offers the Cat® 3516E diesel generator set with the following 50-Hz standby power ratings and emissions thresholds:
The Cat® 3516E diesel generator set with the 3,500 kVA rating offers an 8,800-kg (19,400-lb) weight reduction over a leading competitive product offering the same power output, while occupying 15% less floor space.
With the launch of these new power ratings, Caterpillar now offers diesel generator sets with industry-leading power densities that range from 850 kVA to 3500 kVA.
“Customers evaluate standby power solutions across many dimensions beyond power output and price,” said Bart Myers, general manager for Caterpillar Large Electric Power Solutions. “These new power ratings demonstrate Caterpillar’s continued investment in our engine and power technologies to give our customers superior product value accompanied by our unmatched design and dealer support.”
Cat 3516E generator sets are designed to meet the NFPA power restoration requirement for Level 1 systems and accept 100 percent block load in one step. They meet ISO 8528-5 G3 requirements for steady state and load acceptance.
The new power ratings are available with a low-, medium- or high-voltage frame alternator that enables quick load acceptance through exceptional motor starting capabilities. This feature eliminates the need to oversize the generator set due to motor starting requirements.
The Cat 3516E generator set utilizes the field-proven Cat ADEM™ A5 engine control module (ECM). This module seamlessly integrates all engine functions including ignition, governing and air-fuel ratio control for optimal performance while protecting the engine.
Caterpillar delivers innovative power systems engineered for durability, reliability and value. The company offers worldwide product support, with parts and service available globally through the Cat authorized service and dealer network. In addition, dealer service technicians are trained to service every aspect of Cat equipment.
For more information, visit www.cat.com/powergeneration or e-mail Electric_Power@cat.com.
# # #
About Themar Al Emarat
Dr. Ghanem Al Hajri, an ardent environmentalist and successful entrepreneur, originally mooted the idea of establishing the hitherto unknown concept of hydroponic greenhouse farming in the UAE. He had visited and gathered information from various countries that have excelled in advanced farming methods. His vision as an entrepreneur coupled with a commitment to natural resources as well as the novelty of creating a ceaseless supply of fresh and organic vegetables for the local population were well supported by other shareholders, thus paving way for the establishment of Themar Al Emarat and its operations.
About Mohamed Abdulrahman Al-Bahar
For more than 75 years, Mohamed Abdulrahman Al-Bahar, has proven to be one of the most favored and trusted companies in the machinery and power system industries in the Middle East. With a holistic range of solutions for power system needs including generator sets, renewable energy systems, energy storage systems, switchgear, load banks and all other related accessories, Al-Bahar provides total turnkey power systems solutions for the Marine, Oil and Gas, Industrial, Commercial and Electric Power Generation industries. Headquartered in Sharjah, UAE, Al-Bahar has the strength of 2,800 employees, spread across all its functional branches. For more information, visit www.albahar.com.
About Caterpillar
For more than 90 years, Caterpillar Inc. has been making sustainable progress possible and driving positive change on every continent. Customers turn to Caterpillar to help them develop infrastructure, energy and natural resource assets. With 2018 sales and revenues of $54.722 billion, Caterpillar is the world’s leading manufacturer of construction and mining equipment, diesel and natural gas engines, industrial gas turbines and diesel-electric locomotives. The company principally operates through its three primary segments - Construction Industries, Resource Industries and Energy & Transportation - and also provides financing and related services through its Financial Products segment. For more information, visit caterpillar.com. To connect with us on social media, visit caterpillar.com/social-media.
CAT, CATERPILLAR, LET’S DO THE WORK, their respective logos, “Caterpillar Yellow,” the “Power Edge” and Cat “Modern Hex” trade dress, as well as corporate and product identity used herein, are trademarks of Caterpillar and may not be used without permission.
©2019 Caterpillar
All Rights Reserved
Press Inquiries |
Erin Collins Casie Summers |
Reader Responses | Caterpillar Inc. |