If you already have an existing account with another Cat App, you can use the same account to sign in here
One Account. All of Cat.
Your Caterpillar account is the single account you use to log in to select services and applications we offer. Shop for parts and machines online, manage your fleet, go mobile, and more.
Account Information
Site Settings
Security
For Release Worldwide: May 7, 2019
Release Number: EEPR0619
PEORIA, IL – Caterpillar Inc. today announced ten new standby power nodes for diesel generator sets available now to help customers in Western Europe and other global markets meet power needs and emissions targets with greater precision.
Using the Cat® 3516C and 3516E platforms, Caterpillar produces four 50-Hz power nodes with standby ratings ranging from 2,250 kVA to 3,000 kVA that offer nitrogen oxide (NOx) emissions under 2,000 mg/Nm3 for regulated environments and applications. Additionally, Caterpillar’s portfolio includes six 50-Hz nodes with standby ratings from 2,250 kVA to 3,500 kVA that provide certification to U.S. EPA Tier 2 emissions standards.
“Caterpillar continues to expand our selection of standby nodes to help our customers succeed by providing the right solution for the right power challenge,” said Joel Feucht, general manager for Caterpillar’s Large Electric Power Division. “Excess standby power capacity can needlessly elevate equipment purchasing and ongoing fuel costs. With today’s launch, Caterpillar is helping our customers dial into the exact standby solution that meets a narrowly defined power need while addressing local emissions standards and delivering optimal owning and operating cost.”
Cat 3516C and 3516E generator sets are designed to meet the NFPA power restoration requirement for Level 1 systems and accept 100 percent block load in one step. They meet ISO 8528-5 G3 requirements for steady state and load acceptance.
All of the new power nodes are available with a low- or high-voltage frame alternator that enables quick load acceptance through exceptional motor starting capabilities. This feature eliminates the need to oversize the generator set due to motor starting requirements.
The Cat 3516C generator set utilizes the field-proven Cat ADEM™ A3 engine control module (ECM), while the Cat 3516E generator set employs the Cat ADEM A5 ECM. These modules integrate all engine functions including ignition, governing, air-fuel ratio control, and engine protection.
Caterpillar delivers innovative power systems engineered to deliver exceptional durability, reliability and value. The company offers worldwide product support, with parts and service available globally through the Cat authorized service and dealer network. In addition, dealer service technicians are trained to service every aspect of Cat equipment.
For more information, visit www.cat.com/powergeneration or e-mail cat_power@cat.com.
Contact Bob Chase at bchase@gelia.com
# # #
About Caterpillar
For more than 90 years, Caterpillar Inc. has been making sustainable progress possible and driving positive change on every continent. Customers turn to Caterpillar to help them develop infrastructure, energy and natural resource assets. With 2018 sales and revenues of $54.722 billion, Caterpillar is the world’s leading manufacturer of construction and mining equipment, diesel and natural gas engines, industrial gas turbines and diesel-electric locomotives. The company principally operates through its three primary segments - Construction Industries, Resource Industries and Energy & Transportation - and also provides financing and related services through its Financial Products segment. For more information, visit caterpillar.com. To connect with us on social media, visit caterpillar.com/social-media.
CAT, CATERPILLAR, LET’S DO THE WORK, their respective logos, “Caterpillar Yellow,” the “Power Edge” and Cat “Modern Hex” trade dress, as well as corporate and product identity used herein, are trademarks of Caterpillar and may not be used without permission.
©2019 Caterpillar
All Rights Reserved
Press Inquiries |
Bob Chase Casie Summers
|
Reader Responses | Caterpillar Inc. |