If you already have an existing account with another Cat App, you can use the same account to sign in here
One Account. All of Cat.
Your Caterpillar account is the single account you use to log in to select services and applications we offer. Shop for parts and machines online, manage your fleet, go mobile, and more.
Account Information
Site Settings
Security
For Worldwide Release: October 2023
IRVING, TEXAS – Caterpillar Inc. today announced the launch of the Cat® ECS, a suite of integrated, connected and scalable controllers. The Cat ECS allows customers to manage energy needs ranging from a single generator set to cohesive, full site microgrid solutions linking multiple assets.
Designed and tested by global Caterpillar experts, the new Cat ECS portfolio addresses current and future regulatory and grid requirements. The controllers utilize a simple, scalable architecture, allowing customers to layer additional functionality and serviceability with their changing energy needs. Additionally, they offer built-in plug-and-play features to facilitate the installation, commissioning and management of multiple power generation assets.
“As the energy landscape evolves, power systems are becoming increasingly complex, utilizing multiple energy sources and grid interfaces,” said Jason Kaiser, senior vice president for Caterpillar’s Electric Power Division. “The Cat ECS provides the integration, scalability and connected features to maximize power system performance while also simplifying specification, installation and operation.”
The range includes the Cat ECS 100, a powerful, value-added standby control system, available from October on new standby, gas fast-response and prime power generator sets in select regions of North America. It offers numerous features including intuitive, smart-screen navigation that can be tailored to customer needs, enhanced programmable logic controller (PLC) functionality, four remote HMIs, auto-mains failure, and an integrated annunciator function.
Furthermore, the Cat ECS 100 controller meets UL 6200 standards, which enables 60Hz generator sets to meet UL 2200 3rd edition. In addition to low voltage, it allows medium and high voltage configurations to be UL 2200 listed.
The Cat ECS 200 adds generator set paralleling capability, along with product updates for advanced features, such as combined heat and power (CHP) system management, Balance of Plant control and grid upgrades.
The Cat ECS 300 provides utility and distribution breaker control and can be customized for virtually any application, including tie breakers, and the Cat ECS 400 layers on full microgrid asset supervisory control.
For customers in North America the Cat ECS range also offers streamlined integration of power assets with the Cat® Active Management Platform (AMP), a proven distributed energy resources management system (DERMS) that monitors, manages and monetizes on-site energy assets, including natural gas and renewable power generation, storage and microgrids.
Following the launch of the Cat ECS 100 this month, the portfolio of controllers will be rolled out globally throughout 2024, along with retrofit kit options for the Cat ECS 100 in early summer for select installed units in the field.
Caterpillar delivers innovative power systems engineered for sustainability, durability, reliability and value. The company offers worldwide product support, parts and services, and customer value agreements through the Cat dealer network. In addition, dealer technicians are trained to provide a comprehensive range of maintenance and services that help customers optimize the total cost of ownership of Cat equipment.
For more information, visit cat.com/catecs or e-mail Electric_Power@cat.com.
###
About Caterpillar
With 2022 sales and revenues of $59.4 billion, Caterpillar Inc. is the world’s leading manufacturer of construction and mining equipment, off-highway diesel and natural gas engines, industrial gas turbines and diesel-electric locomotives. For nearly 100 years, we’ve been helping customers build a better, more sustainable world and are committed and contributing to a reduced-carbon future. Our innovative products and services, backed by our global dealer network, provide exceptional value that helps customers succeed. Caterpillar does business on every continent, principally operating through three primary segments – Construction Industries, Resource Industries and Energy & Transportation – and providing financing and related services through our Financial Products segment. Visit us at caterpillar.com or join the conversation on our social media channels.
©2023 Caterpillar. All Rights Reserved. CAT, CATERPILLAR, LET’S DO THE WORK, their respective logos, “Caterpillar Corporate Yellow,” the “Power Edge” and Cat “Modern Hex” trade dress, as well as corporate and product identity used herein, are trademarks of Caterpillar and may not be used without permission.
Press Inquiries
Bob Chase
Gelia
Tel: +1 716-629-3230
bchase@gelia.com
Susan Wilson
Caterpillar Inc.
Susan.Wilson@cat.com