If you already have an existing account with another Cat App, you can use the same account to sign in here
One Account. All of Cat.
Your Caterpillar account is the single account you use to log in to select services and applications we offer. Shop for parts and machines online, manage your fleet, go mobile, and more.
Account Information
Site Settings
Security
High-performance Cat® C13D engine developed to improve long-term value for third-party original-equipment manufacturers and equipment owners.
For Worldwide Release April 3, 2024
The Cat® C13D is a new 13-liter diesel engine platform designed to achieve best-in-class power density, torque and fuel efficiency for optimizing the performance of heavy-duty off-highway applications.
Engineered to Caterpillar’s standards for reliability and productivity, the inline, six-cylinder Cat C13D engine platform is making its LATAM debut at M&T Expo 2024, in the Caterpillar booth A140, at the São Paulo Expo Exhibition & Convention Center, from April 22-26.
The engine offers eight power ratings from 340 to 515 kW with up to 3,200 Nm of peak torque. Engine-mounted after-treatment and cooling packs will also be available from the factory to reduce installation and validation costs.
The C13D will come into production in 2026, meeting the emissions standards of higher regulated markets, such as EU Stage V, U.S. EPA Tier 4 Final, China Nonroad Stage IV, Korea Stage V, and Japan 2014, with models available for lesser regulated markets.
In Brazil, the C13D will meet MAR-1 emission standards up to 430 kW, with ratings up to 515 kW available for other currently lesser and currently non-regulated Latin American countries such as Argentina and Peru.
By supplying comparable power and torque available from Caterpillar’s current 13-, 15- and single-turbo 18-liter engine platforms, the Cat C13D platform provides an opportunity for original equipment manufacturers (OEMs) to downsize the engine and simplify design, assembly, and supply chain requirements across multiple applications. This consolidation can also reduce maintenance, parts, and technical training complexity for end users.
The Cat C13D engine is targeted for a wide range of off-highway equipment, including rock crushers, screeners, and grinders; trenchers; agriculture tractors, harvesters and self-propelled sprayers; woodchippers; material-handling equipment; and large industrial pumps.
“Off-highway OEMs and equipment owners face a rapidly evolving business environment that demands improved worksite productivity and reduced operating costs,” said Steve Ferguson, senior vice president of Caterpillar Industrial Power Systems. “Internal combustion engines are the prevailing workhorses on most job sites around the world, which is why we’ve invested in the next-generation Cat C13D diesel engine platform to address their challenges.”
Purpose-Built for Rugged, Long-Lasting Performance in Off-Highway Applications
The Cat C13D engine platform has been engineered to deliver the performance, durability, packaging, and ease of maintenance demanded by both manufacturers and buyers of off-highway equipment.
The new engine platform offers up to a 20% increase in power and up to 25% more low-speed torque than the previous generation of Cat engines in its power class. It is designed to perform at altitudes of up to 12,000 ft – maintaining higher power than legacy engines at higher altitudes – and in extreme ambient temperatures as high as 140 F (60 C) and as low as minus 40 F (minus 40 C) with aids.
Engineers have designed the Cat C13D engine for quality, reliability, and easier maintenance through a number of improvements, including integrating components and reducing the number of leak joints by more than 45%. Together, the upgrades result in lower fluids consumption and extended service intervals as long as 1,000 hours, reducing operating costs and downtime.
The new engine platform will be equipped with Cat® Digital Services, an integrated suite of robust software and hardware solutions supplying the insight equipment owners need to make decisions on the fly, secure the health of their equipment, and minimize nonproductive time.
The new Cat C13D will be fully supported by the global Cat dealer network, which offers genuine Cat parts and services packaged in Customer Value Agreements. Dealer technicians are trained to provide a comprehensive range of maintenance and services that help customers maximize performance and optimize the total cost of ownership of Cat industrial engines.
About Caterpillar
With 2023 sales and revenues of $67.1 billion, Caterpillar Inc. is the world’s leading manufacturer of construction and mining equipment, off-highway diesel and natural gas engines, industrial gas turbines and diesel-electric locomotives. For nearly 100 years, we’ve been helping customers build a better, more sustainable world and are committed and contributing to a reduced-carbon future. Our innovative products and services, backed by our global dealer network, provide exceptional value that helps customers succeed. Caterpillar does business on every continent, principally operating through three primary segments – Construction Industries, Resource Industries and Energy & Transportation – and providing financing and related services through our Financial Products segment. For more information, visit caterpillar.com. To connect with us on social media, visit caterpillar.com/social-media.
CAT, CATERPILLAR, LET’S DO THE WORK, their respective logos, “Caterpillar Corporate Yellow,” the “Power Edge” and Cat “Modern Hex” trade dress, as well as corporate and product identity used herein, are trademarks of Caterpillar and may not be used without permission.
©2024 Caterpillar
All Rights Reserved
Press Inquiries for Cat Industrial Power Systems: