If you already have an existing account with another Cat App, you can use the same account to sign in here
One Account. All of Cat.
Your Caterpillar account is the single account you use to log in to select services and applications we offer. Shop for parts and machines online, manage your fleet, go mobile, and more.
Account Information
Site Settings
Security
For Worldwide Release: November 2023
Release Number: 319PR23
Attendees at CES 2024 will experience the Power of Possible at Caterpillar Inc.’s roughly 9,600 sq ft exhibit January 9 – 12 in Las Vegas, Nevada. This year’s display focuses on Caterpillar’s electric machines and energy solutions to meet the evolving needs of our customers as they electrify their job sites. As a technology leader for nearly a century, Caterpillar continues to innovate and invest in electrification, alternative fuels, connectivity, and digital solutions to help our customers meet their sustainability goals.
“We are delighted to return to CES to showcase our advancements in energy solutions. This event is known as the proving ground for breakthrough technologies and global innovators which makes it the ideal place for us to showcase our leadership in power systems and integrated service solutions to help our customers in the energy transition,” said Rod Shurman, Senior Vice President of Caterpillar’s Electrification + Energy Solutions division. “We’re putting our expertise to work on multiple advanced power technologies to enable the energy transition solutions that our customers need to be successful in a reduced-carbon world.”
The Caterpillar Experience
The exhibit’s centerpiece, the Cat® R1700 XE LHD underground loader, offers a 16.5-ton payload and 11.2 mph top speed. The zero-exhaust emission loader includes the industry’s only onboard battery eliminating the need to handle or exchange batteries. It charges quickly—in less than 20 minutes when paired with two of the durable and mobile Cat MEC500 chargers. The Cat MEC500 Mobile Equipment Charger is a standalone charging system designed to charge quickly and safely as needed.
Also on display is the company’s 301.9 mini excavator, the first machine with a Caterpillar battery.
Job Site Solutions
No matter how big or small the task at hand, worksites all over the world have two things in common, the need for power and the desire to be more sustainable. Caterpillar offers a powerful combination of technologies and expertise to help customers map their journey toward a lower carbon future.
Visitors to the Cat booth #5440 in the West Hall at CES will experience:
Sustainable Power Generation:
Caterpillar offers and continues to develop lower-carbon intensity on-site power production solutions such as generators running on a variety of renewable fuels, solar panels and hydrogen powered fuel cells.
Energy Storage and Charging Solutions:
Designed for rapid plug-and-play installation and integration, battery Energy Storage Solutions (ESS) can be used with any combination of diesel, natural gas or renewable energy sources such as solar or wind. They store surplus power from these energy sources and then discharge from their reserves as needed. The XEX60, compact ESS will be shown at CES and can be used to provide power to Caterpillar charging solutions.
Caterpillar offers and continues to develop charging options to support battery electric machines using industry standard connectors and protocols. The Cat chargers displayed at CES are tested and validated to work with Cat equipment in the same harsh environments where our machines are put to work.
Batteries:
The on-board battery pack on display at CES is designed to power the 301.9 mini excavator with a total capacity of 32 kWh and a nominal voltage of 48 volt. Cat battery packs consist of a modular design with factory integrated telematics and a rugged structure to endure the use on our heavy equipment.
Power System Solutions:
Additionally displayed at CES will be a Cat 750V Electric Motor and Inverter, components that support a variety of machines and power systems. A 750 DC motor provides mechanical power for the machine movement when commanded by the operator. The inverter transfers power to the electric motor from an onboard Caterpillar machine power source like a generator or battery.
Digital Insights & Customer Solutions:
The Cat digital solutions include everything from machine application use to battery monitoring and servicing needs. The ability for Caterpillar equipment and power solutions to learn about the environment and the habits of the work and operator is also crucial for safety, efficiency, and productivity. The ability to monitor each part of the ecosystem allows the company to provide advanced analytics, transforming data into customer insights making it easier for customers to own and operate their equipment.
As Caterpillar continues to invest in job sites of the future, the company is growing its team. If you are interested in career opportunities at Cat to amplify the journey into electrification, click here for more information.
For more information on the Caterpillar exhibit visit cat.com/CES. #CatAtCES
# # #
Note to Editors: Caterpillar rolls out products and services in each of its regions at different time intervals. Although every effort is made to ensure that product information is released only after Caterpillar has received confirmation from its independent dealer network, plants, and marketing subsidiaries that products and services are available in the relevant region, editors are kindly requested to verify with a Cat dealer for product availability and specifications.
CAT, CATERPILLAR, LET’S DO THE WORK, their respective logos, VisionLink, “Caterpillar Corporate Yellow,” the “Power Edge” and Cat “Modern Hex” trade dress, as well as corporate and product identity used herein, are trademarks of Caterpillar and may not be used without permission.
©2023 Caterpillar All Rights Reserved
Press Inquiries |
Caterpillar Trade Press Media Representatives Americas Kate Kenny: Kenny_Kate@cat.com Johanna Kelly: Kelly_Johanna_L@cat.com Europe, Africa, Middle East Francine Shore: Shore_Francine_M@cat.com |