New Cat® Dynamic Gas Blending™ Gen 2 Kit Empowers Drillers to Upgrade Tier 2 Assets for Enhanced Greenhouse Gas Emissions Reduction 

Cost-Effective Engine Upgrade Supports Climate-Related Objectives While Ensuring Diesel-Rated Transient Response

February 2025

Houston, Texas — Caterpillar Oil & Gas announces the launch of the Cat® Dynamic Gas Blending™(DGB) Gen 2 Kit. The solution enables drilling companies to utilize existing 3512C Tier 2 power solutions to lower greenhouse gas (GHG) emissions and reduce total cost of ownership (TCO).1

The 1 MW-rated DGB Gen 2 Kit addresses a critical need in the industry, as drillers today face the complexity of improving operational efficiency and reducing GHG emissions without compromising performance and uptime. Solutions that support climate-related targets and maintain efficiency without incurring significant additional costs are in demand.

Dual-fuel technologies like the DGB Gen 2 Kit represent a key strategy to address rising fuel costs, evolving industry regulations and the CapEx associated with new gas engines. Optimized to blend diesel and natural gas, the DGB Gen 2 Kit features advanced cylinder technology that improves combustion efficiency. Its port injection system allows for precise air/gas ratio control at the individual cylinder level, resulting in faster response times while reducing unburned gas. Multi-port gas injectors and in-cylinder pressure/temperature systems enable real-time performance optimization for each cylinder.

In addition to lowering GHG emissions, the DGB Gen 2 Kit allows up to two times diesel displacement compared to traditional fumigated technologies to achieve an average 70% diesel displacement, and up to 85% peak displacement. This significantly reduces overall fuel consumption and empowers companies to accurately estimate diesel fuel savings.2

Drilling companies can upgrade all engines on a four-engine rig for nearly the same cost as one new gas-powered engine, which supports decreased capital expenses while also ensuring a diesel-like transient response. Additionally, reducing diesel consumption allows the DGB Gen 2 Kit to help lower operating expenses.

"With the DGB Gen 2 Kit, drilling companies can maximize their investments in Tier 2 engines while significantly reducing GHG emissions,” stated Derek Kamp, vice president, Caterpillar Oil & Gas. “The ability to displace 70% of diesel consumption with natural gas without purchasing a new natural gas engine helps drilling companies optimize their existing assets and profitability."

 


1Reductions calculated based on DGB Gen 2 kit @ 70MN compared to a fumigated kit @ 85MN at 550-650 bkW operating range.
2In comparison of DGB Gen 2 kit @ 70MN to fumigated kit @ 85MN at the same operating conditions 0-1125 bkW.

of
of
of

About Caterpillar Oil & Gas:

Caterpillar Oil & Gas, with headquarters in Houston, Texas, consolidates all the sales and service activities for Caterpillar Inc.’s oil and gas power solutions. Since the 1930s, Caterpillar has manufactured engines for the oilfield and today provides premier power solutions with outputs from 31 to 16,000 kW.  The sales and service network includes more than 2,100 dealer locations world-wide dedicated to support customers in the drilling, production, well service and gas compression segments. More information is available at: cat.com/oilandgas

About Caterpillar:

With 2023 sales and revenues of $67.1 billion, Caterpillar Inc. is the world’s leading manufacturer of construction and mining equipment, off-highway diesel and natural gas engines, industrial gas turbines and diesel-electric locomotives. For nearly 100 years, we’ve been helping customers build a better, more sustainable world and are committed and contributing to a reduced-carbon future. Our innovative products and services, backed by our global dealer network, provide exceptional value that helps customers succeed. Caterpillar does business on every continent, principally operating through three primary segments – Construction Industries, Resource Industries and Energy & Transportation – and providing financing and related services through our Financial Products segment. Visit us at caterpillar.com or join the conversation on our social media channels at caterpillar.com/en/news/social-media.html.

©2025 Caterpillar. All Rights Reserved. CAT, CATERPILLAR, LET’S DO THE WORK, their respective logos, "Caterpillar Corporate Yellow", the "Power Edge" and Cat “Modern Hex” trade dress as well as corporate and product identity used herein, are trademarks of Caterpillar and may not be used without permission.

Trade Press Inquiries:
Tiffany Landers
Landers_Tiffany_L@cat.com