If you already have an existing account with another Cat App, you can use the same account to sign in here
One Account. All of Cat.
Your Caterpillar account is the single account you use to log in to select services and applications we offer. Shop for parts and machines online, manage your fleet, go mobile, and more.
Account Information
Site Settings
Security
Houston, Texas – Caterpillar Oil and Gas is pleased to announce the development of the new land well service 3512E Dynamic Gas Blending™ dual fuel engine. The 3512E DGB™ engine will be certified to U.S. EPA Tier 4 Final emissions standard while offering the highest natural gas substitution in its class.
Unlike previous versions offering dual fuel operation, the 3512E DGB will include factory solutions that emit approximately the same or less greenhouse gas (GHG) emissions as a comparable 3512E Tier 4 Final diesel engine. Additionally, the dual fuel performance of the new 3512E DGB has significantly increased compared to similar engines in its class with the ability to achieve 85% diesel displacement, further allowing for lower operating costs.
With identical configurations as the 3512E diesel engine, the new 3512E DGB engine was designed for 2250 and 2500 bhp ratings. Separate circuit and air to air after cooling options are identical to the core diesel, including mounting dimensions for like trailer design. On engine gas filtration is standard as well as the same options available for the core diesel including the Engine Idle Reduction System (EIRS). The engine’s robust diesel design will allow for extended life and lower owning and operating costs.
“Caterpillar’s 3512 platform has decades of experience operating in the oilfield. And the addition of the 3512E DGB will continue that legacy while helping customers burn natural gas,” said Derek Kamp, Well Service Industry Manager.
To learn more about the new 3512E DGB engine and how Caterpillar can meet your oil and gas needs, stop by the Caterpillar exhibit #2439 at the 2019 Offshore Technology Conference, to be held May 6th – 9th, at the NRG Park in Houston, Texas.
About Caterpillar Oil & Gas
Caterpillar Oil and Gas, Caterpillar’s oil and gas division with headquarters in Houston, Texas, consolidates all the sales and service activities for Cat® oil and gas power solutions. Since the 1930s, Caterpillar has manufactured engines for the oilfield and today provides premier power solutions with outputs from 31 to 16,000 kW. The sales and service network includes more than 2,100 dealer locations world-wide dedicated to support customers in the drilling, production, well service and gas compression segments. More information is available at: cat.com
About Caterpillar
For more than 90 years, Caterpillar Inc. has been making sustainable progress possible and driving positive change on every continent. Customers turn to Caterpillar to help them develop infrastructure, energy and natural resource assets. With 2018 sales and revenues of $54.722 billion, Caterpillar is the world’s leading manufacturer of construction and mining equipment, diesel and natural gas engines, industrial gas turbines and diesel-electric locomotives. The company principally operates through its three primary segments - Construction Industries, Resource Industries and Energy & Transportation - and also provides financing and related services through its Financial Products segment. For more information, visit caterpillar.com. To connect with us on social media, visit caterpillar.com/social-media.
Caterpillar. All Rights Reserved. CAT, CATERPILLAR, LET’S DO THE WORK, their respective logos, “Caterpillar Yellow”, the “Power Edge” and Cat “Modern Hex” trade dress as well as corporate and product identity used herein, are trademarks of Caterpillar and may not be used without permission.
©2019 Caterpillar
All Rights Reserved
Press Inquiries
Danielle Wills