If you already have an existing account with another Cat App, you can use the same account to sign in here
One Account. All of Cat.
Your Caterpillar account is the single account you use to log in to select services and applications we offer. Shop for parts and machines online, manage your fleet, go mobile, and more.
Account Information
Site Settings
Security
Caterpillar Marine Announces New Engine with Increased Power Density
For Worldwide Release: August 2020
Houston, Texas –Today, Caterpillar Marine announced the launch of the new Cat® C32B high performance 2000 HP (2025 MHP) marine engine with a rated engine speed of 2300 rpm. This engine meets emerging market demands and expands the power capability of the C32 high performance product line, delivering a 5% power increase over existing C32 ratings. Customers familiar with the current C32 engine can expect a similar look with the new model, as well as most of the same connection points and footprint. The engine will be available with the same emissions certifications as the current C32 high performance ratings, including EPA Tier 3 Recreational and IMO II. Beyond power density improvement, additional benefits include updated electronics (ADEM 6 ECM) and an enhanced unit injector fuel system, enabling multiple injections to help improve noise and vibration characteristics from combustion.
“We’re very excited to offer our customers more power with the C32B engine, while also helping to reduce engine noise and continuing to provide excellent engine performance and reliability,” says Allen Bowman, marine product strategy engineer for Caterpillar Marine. “The C32B will provide expanded opportunities for our customers for new builds and repower options, which is generating excitement about the future of the C32B and what it will bring to the market.”
The Cat C32B marine engine will be available for order in fall of 2020.This engine comes with industry-leading warranty coverage and the support of the Cat dealer network, which works to ensure superior support and service not only during the initial sale but for the entire life of the engine. For more information about the C32B, contact your local Cat dealer or visit cat.com/C32B.
About Caterpillar Marine:
Caterpillar Marine, with headquarters in Hamburg, Germany, groups all the marketing and service activities for Cat and MaK marine diesel, dual fuel, and gas power systems within Caterpillar Inc. The organization provides premier power solutions in the medium and high-speed segments with outputs from 93 to 16,800 kW in main propulsion and 10 to 16,100 ekW in marine generator sets. The sales and service network includes more than 2,100 dealer locations world-wide dedicated to support customers in ocean-going, commercial marine and pleasure craft wherever they are.
More information is available at: www.cat.com/marine
About Caterpillar
Since 1925, Caterpillar Inc. has been helping our customers build a better world – making sustainable progress possible and driving positive change on every continent. With 2019 sales and revenues of $53.8 billion, Caterpillar is the world’s leading manufacturer of construction and mining equipment, diesel and natural gas engines, industrial gas turbines and diesel-electric locomotives. Services offered throughout the product life cycle, cutting-edge technology and decades of product expertise set Caterpillar apart, providing exceptional value to help our customers succeed. The company principally operates through three primary segments - Construction Industries, Resource Industries and Energy & Transportation - and provides financing and related services through its Financial Products segment. For more information, visit caterpillar.com. To connect on social media, visit caterpillar.com/social-media.
© 2020 Caterpillar.
All Rights Reserved.
CAT, CATERPILLAR, LET’S DO THE WORK, their respective logos, "Caterpillar Corporate Yellow", the "Power Edge" and Cat “Modern Hex” trade dress as well as corporate and product identity used herein, are trademarks of Caterpillar and may not be used without permission.
Press Inquiries |
Danielle Wills |
More power and peace of mind, less noise and maintenance — our new 2025 mhp marine engine gives you plenty to boast about. Get the details on the C32B.
Learn MoreMore power, more speed and a drop-in replacement for your existing C32 sport fishing engine. Find out why our new 2025 mhp marine engine is perfect for repowers.
Learn MoreSwitching to the right marine fuel filters didn’t just clear up a sooty transom on the Rascal sport fishing boat. See how it also led to more time on the water.
Learn More