If you already have an existing account with another Cat App, you can use the same account to sign in here
One Account. All of Cat.
Your Caterpillar account is the single account you use to log in to select services and applications we offer. Shop for parts and machines online, manage your fleet, go mobile, and more.
Account Information
Site Settings
Security
For Release Worldwide: May 6, 2019
Release Number: EEPR0519
DEERFIELD, IL – Caterpillar Inc. today introduced the Cat® XQP30, a 50/60 Hz mobile diesel generator set rated for 30 kVA prime power. Available in two different configurations, one version meets European Union (EU) Stage IIIA emission standards and another provides low brake-specific fuel consumption (BSFC) for customers in non-regulated territories.
The robust, rental-ready design of the Cat XQP30 mobile generator set features forklift pockets, dragging points and a lifting arch for ease of transportation. A dual-wall, open-top bund tank with leak detection sensors offers environmental protection and containment of any spills within the package. The XQP30 provides easy-to-use EMCP 4.2B digital controls along with either Clipsal or CE sockets, allowing the power to be easily distributed across the work site. Heavy duty air cleaners and generator insulation ensures durable operation in harsh work environments and Cat Remote Access Monitoring (RAM) technology tracks and manages assets.
For the European market, the Cat XQP30 mobile generator set is part of Caterpillar’s plan to help Cat Rental Power mobile generator customers smoothly transition from EU Stage IIIA to EU Stage V emissions standards. Applicable to prime or standby power in mobile applications throughout Europe, EU Stage V regulations went into effect on January 1, 2019 for all engines less than 56 kW and equal to or greater than 130 kW. For engines equal to or greater than 56 kW and less than 130 kW, the effective date is January 1, 2020.
Following the transition scheme outlined in EU Regulation 2016/1628, original equipment manufacturers can produce mobile generator sets with engines meeting the previous emission stage for 18 months after the Stage V effective date with an additional six-month accommodation to allow the generator set to be placed on the market.
“Under the new EU Stage V standards, fleets can maintain lower rental rates and reduce maintenance costs by continuing to utilize transition mobile generator sets compliant with EU Stage IIIA,” said Gareth Osborne, product definition manager, Caterpillar Electric Power. “Caterpillar will phase in a complete range of mobile generator sets to meet these new requirements. During the transition period, the Cat XQP30 mobile generator set will help customers manage their fleet strategies while controlling both cost and complexities.”
All Cat XQP mobile generator sets are available through the Cat dealer network. Cat dealers are available 24 hours a day, 7 days a week to assist with emergency rental needs. Caterpillar’s service network ensures access to prompt, quality repairs by trained technicians at Caterpillar authorized service locations.
For more information, click here or e-mail cat_power@cat.com.
Contact Erin Collins at ecollins@gelia.com
# # #
About Caterpillar
For more than 90 years, Caterpillar Inc. has been making sustainable progress possible and driving positive change on every continent. Customers turn to Caterpillar to help them develop infrastructure, energy and natural resource assets. With 2018 sales and revenues of $54.722 billion, Caterpillar is the world’s leading manufacturer of construction and mining equipment, diesel and natural gas engines, industrial gas turbines and diesel-electric locomotives. The company principally operates through its three primary segments - Construction Industries, Resource Industries and Energy & Transportation - and also provides financing and related services through its Financial Products segment. For more information, visit caterpillar.com. To connect with us on social media, visit caterpillar.com/social-media.
CAT, CATERPILLAR, LET’S DO THE WORK, their respective logos, “Caterpillar Yellow,” the “Power Edge” and Cat “Modern Hex” trade dress, as well as corporate and product identity used herein, are trademarks of Caterpillar and may not be used without permission.
©2019 Caterpillar
All Rights Reserved
Press Inquirie |
Erin Collins Rachel Perva
|
Reader Responses | Caterpillar Inc. |