If you already have an existing account with another Cat App, you can use the same account to sign in here
One Account. All of Cat.
Your Caterpillar account is the single account you use to log in to select services and applications we offer. Shop for parts and machines online, manage your fleet, go mobile, and more.
Account Information
Site Settings
Security
For Worldwide Release: March 30, 2021
Release Number: EEPR0721
DEERFIELD, IL – Caterpillar Inc. today announced the introduction of new 3250 kW and 3500 kW standby power nodes that use the Cat® C175 engine platform to provide customers with more options for addressing their power needs in large 60-Hz standby and mission-critical applications.
The Cat C175-16 generator set rated at 3250 kW and the Cat C175-20 generator set rated at 3500 kW are the first power solutions engineered by Caterpillar for these specific nodes. They are ideal for data centers, hospitals, wastewater treatment plants, municipalities and other large facilities.
Offered through the Cat dealer network for 60-Hz applications in North America and around the world, the 3500 kW power node is now available, while the 3250 kW unit will be launched in the second quarter of 2021.
“As mission-critical facilities grow in size and complexity, our customers are seeking reliable standby solutions that allow them to minimize their costs by selecting a solution that precisely meets the power need,” said Bart Myers, general manager in Caterpillar’s Electric Power Division. “By expanding our portfolio of large power solutions, Caterpillar is in a stronger position to address market demand with four power nodes between 3000 kW and 4000 kW on a field-proven engine platform.”
The new Cat C175 diesel generator sets provide certification to U.S. EPA Tier 2 emission standards, and engine emissions consistent with Tier 4 Final levels are achieved by upgrading with Caterpillar’s advanced aftertreatment technologies. They can operate in high ambient environments and provide full power up to 131 degrees Fahrenheit (55 degrees Celsius) without derating.
Cat C175 diesel generator sets are designed to meet the NFPA power restoration requirement for Level 1 systems and accept 100 percent block load in one step. They meet ISO 8528-5 G3 requirements for steady state and load acceptance.
Caterpillar delivers innovative power systems engineered for exceptional durability, reliability and value. The company offers worldwide product support, with parts and service available globally through the Cat authorized service and dealer network. In addition, dealer technicians are trained to service every aspect of Cat equipment.
For more information, visit www.cat.com/powergeneration or e-mail Electric_Power@cat.com.
###
About Caterpillar
Since 1925, Caterpillar Inc. has been helping our customers build a better world – making sustainable progress possible and driving positive change on every continent. With 2020 sales and revenues of $41.7 billion, Caterpillar is the world’s leading manufacturer of construction and mining equipment, diesel and natural gas engines, industrial gas turbines and diesel-electric locomotives. Services offered throughout the product life cycle, cutting-edge technology and decades of product expertise set Caterpillar apart, providing exceptional value to help our customers succeed. The company principally operates through three primary segments – Construction Industries, Resource Industries, and Energy & Transportation – and provides financing and related services through its Financial Products segment. For more information, visit caterpillar.com. To connect on social media, visit caterpillar.com/social-media.
© 2021 Caterpillar. All Rights Reserved. CAT, CATERPILLAR, LET’S DO THE WORK, their respective logos, “Caterpillar Corporate Yellow,” the “Power Edge” and Cat “Modern Hex” trade dress, as well as corporate and product identity used herein, are trademarks of Caterpillar and may not be used without permission.
Press Inquiries
Bob Chase
Gelia
Tel: +1 716-629-3230
bchase@gelia.com
Sarah Pullen
Caterpillar Inc.
Tel: +1 309-675-1513
Pullen_Sarah_C@cat.com
Reader Requests
Caterpillar Inc.
Electric Power Division
P.O. Box 0610
Mossville, IL 61552-0610