If you already have an existing account with another Cat App, you can use the same account to sign in here
One Account. All of Cat.
Your Caterpillar account is the single account you use to log in to select services and applications we offer. Shop for parts and machines online, manage your fleet, go mobile, and more.
Account Information
Site Settings
Security
For Worldwide Release May 24, 2023
Caterpillar has announced the introduction of two new high-efficiency industrial diesel power units (IPUs) that enable original equipment manufacturers (OEMs) to minimize engineering and assembly costs for construction, material-handling, and other off-highway applications in the 74 to 134 horsepower power range while meeting the emissions standards of higher regulated markets.
Now available from Cat® dealers in North America, Cat C2.8 and Cat 3.6 IPUs are equipped with factory-installed ECM sensors, radiators, cooling packs, filtration, control systems and aftertreatment hardware.
These new IPUs meet the emissions standards of EU Stage V, U.S. EPA Tier 4 Final, China Non-road IV, Korea Stage V and Japan 2014. With the addition of these power solutions, Caterpillar currently offers IPUs from 48 to 950 horsepower addressing the emissions standards of higher regulated markets.
“OEMs with restricted engineering resources can shorten their design and assembly timelines with Cat IPUs,” said Steve Ferguson, senior vice president Caterpillar Industrial Power Systems. “These new drop-in packages offer design flexibility, power density, emissions compliance and field-proven durability in an integrated package that can help off-highway manufacturers accelerate their speed to market.”
Advanced Engineering, Outstanding Performance
The flexible and innovative designs of the new Cat C2.8 and Cat 3.6 IPUs offer numerous features to address the demands of off-highway equipment owners.
They feature a common rail direct-injection design with a turbocharged C2.8 or turbocharged aftercooled C3.6 air system.
The ECM and aftertreatment hardware are mounted on the IPU and, along with the fuel filter, are validated to perform in harsh work environments. A new wiring harness has also been developed to allow for a simple hookup to machine wiring. For fast installation, an optional engine control panel for engine monitoring and speed control is also available.
To provide minimal downtime for regeneration, each IPU is equipped with an on-engine diesel oxidation catalyst (DOC) and diesel particulate filter (DPF), while the Cat C3.6 also has selective catalytic reduction (SCR).
For operations in challenging work conditions, the IPUs are available with heavy-duty cooling packs incorporating a pusher fan and erosion screen, as well as heavy-duty fuel filters with increased dirt-holding capacities.
Cat IPUs enable customers to use renewable liquid fuels such as 100% hydrotreated vegetable oil (HVO) and are equipped with Cat® Digital Services, an integrated suite of robust software and hardware solutions supplying the insight equipment owners need to make decisions on the fly, secure the health of their equipment and minimize nonproductive time.
All Cat power solutions are fully supported by the global Cat dealer network, which offers genuine Cat parts and services packaged in Customer Value Agreements (CVAs). In addition, dealer technicians are trained to provide a comprehensive range of maintenance and services that help customers maximize the performance and optimize the total cost of ownership of Cat industrial engines.
For more details on the new Cat IPUs campaign page.
*Fuels must meet the specifications and characteristics described on cat.com in order to be used in Cat engines and reduce the risk of downtime.
About Caterpillar
With 2022 sales and revenues of $59.4 billion, Caterpillar Inc. is the world’s leading manufacturer of construction and mining equipment, off-highway diesel and natural gas engines, industrial gas turbines and diesel-electric locomotives. For nearly 100 years, we’ve been helping customers build a better, more sustainable world and are committed and contributing to a reduced-carbon future. Our innovative products and services, backed by our global dealer network, provide exceptional value that helps customers succeed. Caterpillar does business on every continent, principally operating through three primary segments – Construction Industries, Resource Industries and Energy & Transportation – and providing financing and related services through our Financial Products segment. For more information, visit caterpillar.com. To connect with us on social media, visit caterpillar.com/social-media.
CAT, CATERPILLAR, LET’S DO THE WORK, their respective logos, “Caterpillar Corporate Yellow,” the “Power Edge” and Cat “Modern Hex” trade dress, as well as corporate and product identity used herein, are trademarks of Caterpillar and may not be used without permission.
©2023 Caterpillar
All Rights Reserved
Press Inquiries for Cat Industrial Power Systems: