We Didn't Rewrite History.
We Defined it.

 

Overhead shot of an older Cat Engine with a group of Cat workers helping to install it
Overhead shot of an older Cat Engine with a group of Cat workers helping to install it

30+ Years of the Cat® G3600 Engine.

Trusted for decades. Upgraded for today. The Cat® Next Gen G3600 engine is built to level up your operations.

Every legend has an origin story. The Next Gen Cat® G3600 is built on its 30+ years of industry-leading performance to deliver what you need today and elevate expectations well into tomorrow. We knew we didn’t have to reinvent the wheel, but build steadily on the power you’ve come to trust. From its continued upgrades to its rock-solid build quality, to the unrelenting testing it's put through before it ever sees the field—the Gen 2 delivers 10% more power than its predecessor, all in the same footprint so you can simplify replacements and retrofits. We put everything into the Next Gen G3600 product line, because even legends need to evolve.

Building the foundation.

The original 3600 has been blazing trails since 1984, when it was born into our growing family of diesel engines. A powerhouse from the start, it quickly earned its reputation by delivering optimized power and lower maintenance, especially in high-horsepower applications. After just one year of exceeding standards for diesel engine performance, its successor was greenlit for development.

Close up of an old Cat Engine
Close up of an old Cat Engine

Ready for liftoff.

The gas-powered G3600 ESS engine launched in 1991 and immediately set itself apart. This engine pushed the existing possibilities for gas compression applications with its field-proven reliability and unmatched levels of power. To match the growing needs of the sector, the G3600 family continued to expand rapidly with the introduction of the G3600 A3 engine in 2002.  The unprecedented acceptance from consumers solidified the G3600 as a key player in the field. 

Close up of an old Cat Engine
Close up of an old Cat Engine

One giant leap.

The 2015 launch of G3600 A4 Gen 1 engines moved the needle in the oil and gas industry, with significant upgrades from previous models. The A4 Gen 1 came equipped with temperature-sensing technology to automatically redirect its systems as needed, with a 5% increase in horsepower over its predecessor. The new design included a combustion strategy that allowed the original A4 to use fuel at a lower heating value, while operating over the widest range of fuel quality possible. The A4 Gen 1 also exceeded rigorous emission standards, producing 40% less NOx, less carbon monoxide and less VOC than previous engines. These game-changing operations were a win for the environment—and for you.

Close up of Cat G3600 Engine
Close up of Cat G3600 Engine

Ready for the future.

The G3600 A4 Gen 2 is the latest and greatest in the G3600 legacy. GHG, VOC, CO and Methane emissions are reduced in the G3600 A4 Gen 2 over the prior model; more than 90% of components remain the same for packaging compatibility. The Gen 2 has the option for 10% more power and increases performance even further, while still improving emissions to create a better tomorrow. The Gen 2 is at the forefront for the next generation of gas compression applications around the world.

Cat worker in PPE with his back to the camera staring at Cat G3600 Engine
Cat worker in PPE with his back to the camera staring at Cat G3600 Engine