If you already have an existing account with another Cat App, you can use the same account to sign in here
One Account. All of Cat.
Your Caterpillar account is the single account you use to log in to select services and applications we offer. Shop for parts and machines online, manage your fleet, go mobile, and more.
Account Information
Site Settings
Security
PAT (Pattanakit Banpong Co., LTD.)
PAT Sugarcane Harvester S3
Pattanakit, Thailand, Southeast Asia
Cat® C9.3B, 375hp Industrial Diesel Engine
Metro Cat, Thailand
Every year, Thailand’s sugar industry produces more than 14 million metric tons of refined sugar. Harvesting sugarcane is a labor-intensive and time-consuming job, which is why companies like Pattanakit Banpong Co., Ltd. (PAT) manufacture sugarcane harvesters. The 11-roller machines cut stalks, strip leaves and chop the cane into segments, while depositing waste material back into the field for fertilizer.
PAT sugarcane harvesters process more than 800,000 tons of cane per year. When PAT needed to upgrade their engines for more efficiency and power, they chose the Cat® C9.3B Industrial Diesel Engine for their fleet.
With 375 hp and four pump sets, the Cat C9.3B gives the harvesters a fast response to their heavy workload. One of the key components is the four-blade extractor fan, which separates the crops with a cyclone of wind so that only the trash is extracted. PAT sugarcane harvesters operate with the first automatic control system in Thailand, using electronic systems to help control driver operations.
The Cat C9.3B delivers expanded capability with 19% more power and 16% more torque than previous platforms, allowing the sugarcane harvesters to increase their uptime and overall productivity. It has standard service intervals of 500 hours under normal operating conditions, with remote mount options for serviceable items like oil and fuel filters. For PAT, that means more power at less cost.
The Metro Cat team partnered with PAT to offer support during the design phase of the C9.3B. Today, 100% of PAT machines, including the Sugarcane Harvester S3, are equipped with Cat engines.
PAT has worked with dealer Metro Cat for more than a decade and relies on the Cat Global Dealer Network to provide aftermarket service support in the regions where they export machines. Owner Boonyong Manitchotpisit says it's easy to stick with Caterpillar because of the reliability, durability and power of the engines, as well as the network of product support.
“It’s not just the performance of the engines; it’s the support. The ease of doing business with Metro Cat is important to keep our operations running at peak efficiency.” –Boonyong Manitchotpisit, Owner, Pattanakit Banpong Co., Ltd.
Pattanakit Banpong Co., Ltd. chose the Cat C9.3B Industrial Diesel Engine to outfit the PAT Sugarcane Harvester S3. With 375 hp and four pump sets, the engine gives the harvester a fast response to its heavy workload.
The Cat C9.3B delivers expanded capability with 19% more power and 16% more torque than previous platforms, allowing the sugarcane harvester to increase its uptime and overall productivity. The engine has standard service intervals of 500 hours under normal operating conditions, with remote mount options for serviceable items like oil and fuel filters. For PAT, that means more power at less cost.
The Cat® C9.3B Industrial Diesel Engine is rated from 250-340 bkW (335-456 bhp) @1800-2200 rpm.
The Cat C9.3B delivers expanded capability with 19% more power and 16% more torque than previous platforms.
100% of PAT machines, including the Sugarcane Harvester S3, are equipped with Cat engines.
See what other Cat® industrial engine customers have to say about our engines and related products, and the support they receive from the Cat dealer network.
Your Cat dealer is your go-to resource for everything from installation support to troubleshooting to in-the-field service. With 171 dealers serving 192 countries, the expert assistance you need is always close at hand.