H&OP DOES MY PORTABLE GENERATOR NEED TO BE GROUNDED FAQS?
Yes. The National Electrical Code requires generators to be grounded to an approved earth ground ... read more
If you already have an existing account with another Cat App, you can use the same account to sign in here
One Account. All of Cat.
Your Caterpillar account is the single account you use to log in to select services and applications we offer. Shop for parts and machines online, manage your fleet, go mobile, and more.
Account Information
Site Settings
Security
Operations and Safety
Yes. The National Electrical Code requires generators to be grounded to an approved earth ground ... read more
Audience: CSR
The National Electrical Code requires generators to be grounded to an approved earth ground. ... read more
The INV Series is equipped with an Engine Smart Control (ESC) mode which can be turned on or off ... read more
Attaching: Inspect the lifing eye before installing to be sure it is not bent, cracked, or corroded. Always replace ... read more
Please refer to the safety procedures, detailed instructions and visual diagrams for starting and stopping in ... read more
Before starting your generator for the first time, please refer to the safety procedures, detailed instructions and ... read more
RP Series generators have two mechanisms to protect fuel from contamination. There is a fuel strainer located in ... read more
If you are using tools that require intermittent power (kick on and off automatically or manually) or you have multiple ... read more
This generator is equipped with an automatic low-idle mode which can be turned on or off using the engine idle control ... read more
Your 12kW unit comes with a Smart charger in the box, which includes an AC power cord as well as a cord to attach to ... read more
The portable generators do not start automatically - you will need to start your portable generator manually. ... read more
Our portable generators do not currently have the capability to start remotely. ... read more
Yes. ... read more
No. Always shut off your generator before moving it. ... read more
Refer to the owner's manuals for the specific products and appliances that you want to use to determine ... read more
Yes. When plugging directly into the generator, we recommend that you turn your devices, tools ... read more
You can operate your generator during inclement weather, but you must ensure that the genereator is ... read more