If you already have an existing account with another Cat App, you can use the same account to sign in here
One Account. All of Cat.
Your Caterpillar account is the single account you use to log in to select services and applications we offer. Shop for parts and machines online, manage your fleet, go mobile, and more.
Account Information
Site Settings
Security
Ben Rice | Agriculture Industry Representative
Safety is especially important on the farm or ranch, as it not only protects your livestock, but also your machine operators and family. Equipment damage and accidents can mean potential injury, reduced production, decreased performance and lost revenue. In agriculture, four factors are particularly important to consider regarding skid steer loader safety: visibility, the exhaust system, emergency and everyday operation safety features.
Today’s advanced skid steer loaders are equipped with visibility enhancing features that help prevent injury to nearby workers and livestock. They also help minimize damage to buildings, fences, pens and the machine itself. Some of these include:
Many older model skid steer loaders and several current makes are equipped with exhaust systems that direct exhaust to exit out of the machine from the side and rear. It is easy to imagine the injury and damage this can cause, as these extremely hot exhaust fumes can harm people or livestock standing near the machine. They can also ignite airborne debris such as hay, bedding, feed and silage.
With the close working quarters on today’s farms, it is important to find a skid steer loader with an exhaust system that cools the engine exhaust gas and directs it up and away from ground level. All air flow should exit the machine vertically rather than to the side or rear to avoid disturbing or harming people or animals.
In the event of an unexpected engine shut down, it is important to have more than one method of lowering the lift arms so the operator can safely exit the machine. Hydraulic accumulators can allow the operator to lower the loader arms if electrical power is available and the accumulator is charged. If the accumulator is not charged or if there is no electrical power, a dead engine lower valve allows the operator to manually lower the arms so the operator can safely exit.
On today’s advanced skid steer loaders, safety features activate before the engine is even turned on—starting with the operator presence system, which requires the operator to be in the machine with the arm bars lowered before the engine will start. Once the engine is started, the parking brake will remain set and the hydraulic system locked out until you depress a switch to activate the machine. Additionally, a spring-applied hydraulic release parking brake will engage and lock the hydraulics out automatically when the arm bars are raised or when the engine is not running.
Fully sealed and pressurized cabs equipped with an air filtration system can help minimize inhalation of contaminants and dust that mix in with the air during everyday operations. These cabs are also quieter, which allows operators to focus on the tasks at hand and reduces their fatigue at the end of a long day.
Bottom line: Skid steer loaders should always be equipped with proper safety features to ensure operator and machine safety. This is why it’s a good idea to research the latest safety guidelines, procedures and feature advancements when spec’ing or purchasing a new machine.
To learn more about safety on the farm or ranch and the latest safety features available on today’s advanced skid steer loaders, contact your local Cat® dealer.
Agriculture Industry Representative
Having spent his formative years on a tobacco farm, Ben Rice went on in the agriculture field to earn degrees in Agriculture Business Management and Agriculture Science from North Carolina State University. Rice now brings his invaluable expertise to Caterpillar as an industry sales and service representative.
You’re here to get ideas to grow your business. Read on for machine insights and expert tips and tricks to get more out of every job.
You asked. The new Cat® D3 Series Skid Steer Loaders and Compact Track Loaders are the latest in a long line of industry-defining machines from Caterpillar®.
Learn MoreWhile compact wheel loaders, skid steers and track loaders are all versatile farm machinery, which is best for your operations? We see how they compare.
Learn MoreA comparison of skid steer loaders and tractors on the farm, and when to use these farming machines for various applications.
Learn MoreFind our five tips on buying used machines, so you can get the same quality, reliability and performance as new equipment.
Learn More