If you already have an existing account with another Cat App, you can use the same account to sign in here
One Account. All of Cat.
Your Caterpillar account is the single account you use to log in to select services and applications we offer. Shop for parts and machines online, manage your fleet, go mobile, and more.
Account Information
Site Settings
Security
Estimated read time: 5 minutes
Every 1,000 service hours, it's time for PM3 maintenance. While the exact service requirements can vary by machine, here's what you can expect for a Cat® D6 XE Dozer. Always refer to your Operation and Maintenance Manual (OMM) for safety procedures, and don't forget to wear appropriate personal protective equipment (PPE).
Check out this video to see how to perform this maintenance before you dive in:
Do your maintenance in a clean environment and on a level surface. Let your equipment coast to a stop because this will help when you check track tension. Engage the park brake, lower implements to the ground and lock out the hydraulics.
You can order all the necessary parts for your planned maintenance at Parts.Cat.com. Enter your machine’s serial number to find the specific parts and Cat Self-Service Options (SSO) tailored for your equipment. SSOs provide detailed service instructions along with recommended parts and tools.
Before starting the service, take a walk around your machine to inspect for leaks, rust or any other signs of damage.
To begin this routine Cat D6 XE Dozer maintenance, you'll need to collect S•O•SSM Services samples. The following samples need to be taken while the engine is running and the compartments are at operating temperature. Always drain a bit of fluid before you start filling the bottle so that you’re getting an accurate analysis of fluid health.
Take samples for the engine, hydraulics and transmission. The transmission and engine aren’t pressurized, so you have to pump those samples out.
Once these samples are collected, you can turn off the engine and use a pump to take separate fluid samples from both final drives.
Before this inspection, shut off the D6 XE’s electrical system for your safety. Check enclosures, cables, harnesses and ground straps throughout the machine. Replace any missing hardware, clean off built-up debris and make any necessary repairs.
Also, wipe down the batteries and check for leaks or damage. Ensure the terminals are secure.
Once the oil has drained completely, remove the filter using a strap-type wrench. Wipe the housing and make sure the old seal is removed. Coat the new filter’s seal with new engine oil, and reference the installation instructions on the filter.
After refilling the oil, clean the fuel fill cap and then reinstall it.
In that same panel, check the recoil spring oil level.
Also check the equalizer bar end pins, front roller frame seals and track shoes for any signs of wear or damage.
Now, shut off the fuel valve at the back of the machine and drain any sediment. Replace the primary and secondary fuel filters, being sure to coat the new seals with clean diesel. Never prefill your fuel filters. Follow the instructions in your OMM to prime the fuel system.
Replace the fresh cabin air filter outside the cab. Inspect the recirculating filter in the cab, and replace it if it’s dirty.
While in this area, remove and clean the fuel tank strainer, and replace the fuel cap filter.
Inside the compartment where you took hydraulic and transmission oil samples, you’ll replace the steering charge filter. Discard the old filter, make sure the entire seal has been removed and wipe the base with a clean cloth. Place the new seal and install the new filter by hand.
Don’t forget to shut all compartments and put guards and steps back in operating position. Also turn the electrical system back on.
With thorough planned maintenance, you can help keep your Cat equipment in top working condition, ready for its next 1,000 hours on the job.
Looking for other hours intervals? We have guides for 250-hour, 500-hour and 2,000-hour maintenance, too.
For more information and support, contact your Cat dealer. And always check your Operation and Maintenance Manual for specific instruction and safety procedures.