If you already have an existing account with another Cat App, you can use the same account to sign in here
One Account. All of Cat.
Your Caterpillar account is the single account you use to log in to select services and applications we offer. Shop for parts and machines online, manage your fleet, go mobile, and more.
Account Information
Site Settings
Security
Maritime operators face a complex future trying to balance regulatory compliance, carbon reduction objectives and safety while still achieving their business goals. As they take steps to address their climate-related targets, technological advancements can support operators’ plans.
In 2023, International Maritime Organization (IMO) member states adopted a strategy “to reach net-zero greenhouse gas (GHG) emissions from international shipping by or around” 2050.1 The plan includes a commitment to use alternative fuels with lower GHG emissions by 2030. One way Caterpillar Marine supports these objectives is through providing fuel-flexible solutions for the future – including engines that can reduce diesel consumption and harness the benefits of alternative fuels such as methanol.
Methanol is unique among fuel options as it’s particularly well-suited for maritime use. Considered a simple and safe marine fuel solution, methanol is relatively energy dense and expected to be more cost-effective than other alternative fuel choices. Methanol provides additional benefits including high miscibility in water, protecting the environment in the event of accidental spills. With this in mind, innovative adaptive fuel engines can be optimized for high substitution rates, helping operators lower their lifecycle GHG emissions.
There are multiple types of methanol. Most methanol commercially available today is produced using natural gas or coal as a feedstock and is referred to as gray or brown methanol, respectively. Blue methanol is produced using natural gas that has been produced through steam reforming. Green methanol, sometimes referred to as e-methanol, is produced using hydrogen derived through a renewable energy supply.
Compared to marine diesel, methanol can help lower CO2 emissions as well as nitrogen oxides (NOx) and sulfur oxides (SOx)2 although it’s important to note that formaldehyde can potentially form during methanol combustion, which could have safety and environmental impacts.3
Methanol also has a lower energy density than diesel but a relatively high energy density compared to hydrogen, and it can be stored as a liquid at standard conditions. These two crucial advantages are essential to minimizing ship design and operational range impacts. As large cargo vessels are beginning to make transcontinental journeys using methanol,4 this lower-carbon intensity fuel appears to be able to satisfy both safety and range considerations for marine applications.
Methanol is globally available today as a common chemical used in many industrial processes. Its existing infrastructure, as well as well-documented safety and handling procedures, supports the use of this extremely efficient hydrogen carrier as a lower-carbon intensity fuel for maritime applications. The primary challenge with using methanol fuel in today’ diesel engines is that it can’t ignite under compression and requires an external ignition source, such as a cetane enhancer, spark ignition or diesel pilot. Currently, only dual-fuel engines can enable methanol to provide a comparable performance to diesel, which is especially well-suited to the growing interest in marine fuel flexibility.
Methanol can play a critical role on its own as a future maritime fuel, and it can also be used with other lower-carbon intensity fuel options. While a dual-fuel engine requires diesel as the ignition energy, traditional diesel may be replaced with hydrotreated vegetable oil (HVO), biodiesel or any blend of such fuels to further reduce carbon intensity. Methanol can also be used to power generator sets that act as battery chargers in a battery hybrid installation. The myriad of possibilities affords vessel operators greater flexibility.
Over the past 20 years, Caterpillar has invested more than $30 billion in research and development (R&D). The company has also established cooperative R&D agreements with several universities and governments to leverage learning within the industry and share knowledge in academic spaces. One recent example is Caterpillar’s cooperation with the U.S. Department of Energy’s Oak Ridge National Laboratory to evaluate methanol’s use as an alternative fuel in marine engines.5
The methanol-ready Cat® 3500E marine engine represents a notable example of maritime technological advancements. In 2022, Caterpillar Marine announced that the 3500E can be modified to run as a dual-fuel engine using methanol.6 In 2024, plans were revealed to deploy the first set of field demonstrator methanol dual-fuel 3500E marine engines with renowned shipbuilder Damen Shipyards.7 The engines have been optimized for high methanol substitution rates across a wide range of load factors.8 For example, a typical harbor tug could achieve a methanol substitution of greater than 70%, on an energy basis, demonstrating the significant potential benefits methanol can provide to such an operation.9
The transition to a reduced-carbon future presents a range of opportunities for vessel operators. In many cases, it’s possible to achieve fuel flexibility that accommodates methanol without needing new builds or costly retrofits. Ship operators can review their unique circumstances and consider the benefits of adopting methanol and other solutions to help achieve their climate-related goals and address evolving industry requirements.
1. IMO.org, “Revised GHG reduction strategy for global shipping adopted”. https://www.imo.org/en/MediaCentre/PressBriefings/pages/Revised-GHG-reduction-strategy-for-global-shipping-adopted-.aspx
2. Methanol.org, “Renewable Methanol”. https://www.methanol.org/renewable/
3. Formaldehyde is a long-recognized byproduct of methanol combustion in internal combustion engines and is expected to be directly regulated to stringent levels in the future. Exhaust formaldehyde emissions may be minimized with optimized combustion and aftertreatment controls while achieving the highest possible methanol substitution in dual-fuel operation. Additionally, there are stringent occupational safety exposure limits that have been in place in Europe and around the world for decades. Caterpillar holds safety as a top priority, which has driven our decision to proactively address formaldehyde emissions to ensure the environmental safety of crews, in line with standards available from other industries.
4. Maersk.com, “Ane Maersk, the world’s first large green methanol-enabled vessel, makes her first call in Dubai”. https://www.maersk.com/news/articles/2024/05/08/ane-maersk-makes-her-first-call-in-dubai-at-dp-world
5. ORNL.gov, “ORNL, Caterpillar collaborate to advance methanol use in marine engines”. https://www.ornl.gov/news/ornl-caterpillar-collaborate-advance-methanol-use-marine-engines 6. Cat.com, “Caterpillar Marine To Support Select Cat® 3500E-Series Engines With Dual Fuel Methanol”. https://www.cat.com/en_US/news/engine-press-releases/caterpillar-marine-to-support-select-cat-3500-E-series-engines-with-dual-fuel-methanol.html
7. Cat.com, “Caterpillar Marine Advances Plans For Methanol Dual-Fuel Technology”. https://www.cat.com/en_US/news/engine-press-releases/caterpillar-marine-advances-plans-for-methanol-dual-fuel-technology.html
8. Cat.com, “Caterpillar Marine Advances Plans For Methanol Dual-Fuel Technology”. https://www.cat.com/en_US/news/engine-press-releases/caterpillar-marine-advances-plans-for-methanol-dual-fuel-technology.html
9. Cat.com, “Caterpillar Marine Advances Plans For Methanol Dual-Fuel Technology”. https://www.cat.com/en_US/news/engine-press-releases/caterpillar-marine-advances-plans-for-methanol-dual-fuel-technology.html