If you already have an existing account with another Cat App, you can use the same account to sign in here
One Account. All of Cat.
Your Caterpillar account is the single account you use to log in to select services and applications we offer. Shop for parts and machines online, manage your fleet, go mobile, and more.
Account Information
Site Settings
Security
When it comes to skid steers, hydraulic attachments make the machine more productive and versatile. The Cat® skid steer hydraulic quick-attach system is designed to make life easier for operators. With a few simple adjustments, work crews can equip skid steers with the attachment tools needed to get the job done right.
When you’re connecting a hydromechanical attachment, it’s important to be careful and take the proper steps for safety and efficiency. Follow these simple guidelines for secure hydraulic connections:
To disconnect a hydraulic work tool:
When the work is done, keep your attachment clean and ready for the next task. To prevent contamination and wear, reinstall dust caps on the machine couplings. Inspect hydraulic hoses for cracks or leaks. Keep lines safe from damage, and reduce pressure buildup by connecting the male and female ends of the work attachment tools together. Taking a little time for proper maintenance will make it easier to get started the next time you need to use the work tool attachment.
There are Cat skid steer loaders that come equipped with powered quick couplers for work tool attachments. This feature makes it possible to change attachments without having to leave the cab of the machine. With the attachment properly positioned on the ground in front of the skid steer, the operator can slowly drive the machine to the attachment, tilt the coupler forward and lock the work tool into place.
Once the connection is made, the operator lifts and tilts the coupler and work tool back to allow the tool to fully seat. The pins for the attachment are then engaged from the controls inside the cab. Operators should always test that the connection is secure before using the skid steer attachment.
The benefit of the Cat skid steer hydraulic quick-attach system is the ease of switching up work tool attachments in a matter of minutes. The technology allows a single machine to be more versatile and productive. From hydraulic hammers and augers to bale grabs and brushes, there’s almost nothing you can’t accomplish with a Cat skid steer loader.
When trying to determine which work tool attachments to get, think about which applications you need for your business. If you own a landscaping company with the need to move heavy materials and supplies, Cat fork attachments are an important investment. You should also consider snow-management attachments if you’re located in a colder climate. Snowplow and wing attachments can help keep businesses profitable during the winter months.
Always check the proper procedures in your OMM. It’s a great resource to use if you run into any issues while connecting or removing a work tool attachment from your machine. There are specific instructions for each type of work tool attachment. You can also contact your local Cat dealer with any questions.
In person or online, we're here to help you find the answers you need. Reach out to your local Cat dealer for advice close to home. Sign up for our newsletter to hear from industry experts. Or keep exploring this site for additional information.