If you already have an existing account with another Cat App, you can use the same account to sign in here
One Account. All of Cat.
Your Caterpillar account is the single account you use to log in to select services and applications we offer. Shop for parts and machines online, manage your fleet, go mobile, and more.
Account Information
Site Settings
Security
THE CAT® PM622 COLD PLANER HELPED THE CREW AT TRI-CITY BLACKTOP INC. MEET TIGHT MILLING SPECIFICATIONS ON TIME
Road construction is all about precision work and meeting deadlines. Not only must jobs meet tight specifications, they must also be completed on time. Tri-City Blacktop, Inc. accomplished both of these goals at a milling job for the city of Bettendorf, Iowa.
In 10 days, one of the city’s worst streets became one of the smoothest. A Tri-City Blacktop crew milled concrete at a depth of 2½-inches (64 mm) for the 0.8-mile (1.3 km) Middle Road resurfacing. Milling was completed in four days. Cleaning and prepping the milled surface took another two days, and paving was finished in four days.
A Cat® PM622 Cold Planer helped the crew mill 5,600 square yards (4682 square meters) daily. With a milling width of 88 inches (2.2 m), the PM622 is 50 percent more productive than previous mills the crew operated.
“We’re able to make a wider cut, for one thing,” says Luke Carpenter, field superintendent. “We had high expectations for the PM622 on this job, and it exceeded them. We had a 4,000 square yardage goal every day, and we exceeded that every day that we milled.”
With an operating weight of 74,580 pounds (33,829 kg) and rated power of 630 hp (470 kW), the PM622 easily milled the 2½-inch (64 mm) concrete layer. “We can mill with such precision with this machine. It doesn’t chatter, the tracks don’t jump. It handles tough jobs like this better than any machine that we’ve seen,” Carpenter says.
The Tri-City Blacktop crew milled within 1/8-inch (3 mm) of the specified depth. “The city doesn’t want us to get into the rebar that’s in the concrete, so they didn’t want us going any deeper,” Carpenter says. “We didn’t hit any rebar. It’s been a very smooth job.”
Meeting the milling specifications was also critical to keeping the existing hand-framed curbs intact. The city didn’t want the road height changed, which would have required curb replacement. Tri-City Blacktop met the specs, and new curbs weren’t necessary.
The PM622’s technology helped the crew complete milling quickly. “True zero for matching is stored in the grade control system. There’s never any second guessing. Once you get the machine set up, it’s always set up,” Carpenter says. “You can set down at two and a half inches and taper that out 30 feet to two inches and not have to do it manually. It will do a perfect taper every time.”
A highly skilled crew is necessary to mill at the rate that Tri-City Blacktop did on the Middle Road resurfacing project. “We’ve had this crew together for 20-plus years. They do a great job,” Carpenter says.
Sometimes you catch a break, too. Topography worked in favor of Tri-City Blacktop. “This job has some hills, and we’re using them to our advantage. Downhill, with the gravity, is helping us move a little quicker through the concrete,” Carpenter says.
Tri-City Blacktop successfully met a 0.25-inch (6 mm) over 10 feet (3 m) bump specification. The crew used a Cat AP655F Asphalt Paver to place three lifts: 1-inch (25 mm) sand level mix for crack fill, 2-inch (51 mm) intermediate lift, and a 1.25-inch (32 mm) surface lift. A total of approximately 6,000 tons (5443 metric tons) of material was placed. The asphalt was produced at a Tri-City Blacktop plant three miles from the jobsite.
The PM622’s controls are similar to those on Cat pavers. “We’re all familiar with the pavers. Caterpillar did a really good job tying the two together. You can jump from one to the other without having any doubt in what you’re doing. Grade control is laid out the same on both,” Carpenter says.
And when the Tri-City Blacktop crew was finished with the job, a rough section of Middle Road was smooth driving—on time and with all specifications met.
When Larry Carpenter founded Tri-City Blacktop, Inc. in 1969, he used Cat machines. Two generations later, the company’s fleet has grown to more than 30 Cat machines, including loaders, a dozer, rollers, a motor grader, cold planer and a paver.
The company does new construction, overlays, and a variety of other types of asphalt work. “Basically, we do anything from the ground up, except for general contracting,” says Luke Carpenter, field superintendent. “Seventy percent of our work is milling and paving.”
The PM622 Cold Planer is the newest Cat machine owned by Tri-City Blacktop. “When they released this mill, there was no question that we were going to have one,” says Luke Carpenter, field superintendent.
The service points on the PM622 are quickly accessible. “Everything is easy to get to—the filters, the drains, everything,” Carpenter says. “The tool holder system is very easy to change, very fast. There’s no bolts to tighten. It’s a 30-second change.”
You’re here to get ideas to grow your business. Read on for machine insights and expert tips and tricks to get more out of every job.
Technologies that enhance machine performance can add to the bottom line.
Learn MoreOnce Product Link is activated, all you need to do is set up your VisionLink account and start taking a look at what your machine information can tell you.
Learn MoreWestern Rock Products in Utah has noticed several improvements to their operations when using machine-to-machine technology.
Learn MoreMachine-to-Machine technology helps contractors increase efficiency and productivity.
Learn More