If you already have an existing account with another Cat App, you can use the same account to sign in here
One Account. All of Cat.
Your Caterpillar account is the single account you use to log in to select services and applications we offer. Shop for parts and machines online, manage your fleet, go mobile, and more.
Account Information
Site Settings
Security
The arrival of warmer weather means keeping up with these maintenance tips so that your diesel engines run smoothly.
CAITLIN MADDOCK-BAHR | Social Media & Digital Strategy Manager
If you own a machine or piece of equipment with a Cat® engine, you know how important it is to keep it in good shape and prevent any problems that could affect your performance and efficiency. This is especially true in the summer when higher temperatures and more demand can add extra stress to your machine’s engine. Check out our tips on maintaining your Cat engine in the summer heat so you can avoid unexpected downtime.
Cat engines are designed to deliver reliable and consistent power for various applications, such as construction, mining, agriculture and more. They are also built to meet the strict emissions standards and regulations for different regions and industries. However, to make sure your engine performs at its best and complies with the emissions requirements, you should follow a regular preventative maintenance schedule and frequently check your engine components. This will help you:
Here are some of the critical steps you should take to preserve your Cat engine in the summer.
Your cooling system is vital for preventing overheating and engine damage. It’s made up of several components, including the coolant, hoses, belts, radiator and fan. You should check these components regularly and look for any signs of leaks, cracks, wear or corrosion that could affect the performance of your cooling system. If you need to top up your coolant, mix only the recommended type with distilled water. Never use tap water since it can cause scaling and corrosion.
Oil is essential for lubricating and protecting engine components from friction and wear. It also helps to remove heat and contaminants from the engine. However, oil can degrade over time and lose its effectiveness. Change your oil and filter according to the manufacturer’s schedule or the Cat Electronic Service Tool (EST) recommendations. Use only the approved oil grade and viscosity for your engine model and operating conditions.
Your air filter and intake system deliver clean air to your engine for combustion. Dirty or clogged air filters can reduce airflow and engine efficiency and increase fuel consumption and emissions. Inspect your air filter and intake system regularly and replace them when needed. Use only genuine Cat filters designed to fit your engine and provide the best filtration.
Idling your engine wastes fuel and increases emissions and can cause carbon buildup in your cylinders, valves and injectors. It can also affect your aftertreatment system, which needs high exhaust temperatures to function correctly. To avoid these problems, limit your idling time to the minimum necessary for warm-up, cool-down or operation. Use the Cat Auto Idle Shutdown feature on your engine to automatically shut off the engine after a preset idle time.
Overloading your engine can cause excessive heat, stress and wear on your engine components. It can also reduce your fuel efficiency and increase your emissions. To prevent overloading, follow your engine model and application's rated power and torque specifications. Use your engine's Cat Power Management System (PMS) to enhance your power output and fuel consumption.
If you notice any unusual noises, smells, smoke or performance issues with your engine, don’t ignore them. They could be a sign of a severe problem that needs immediate attention. If you see any warning lights or fault codes on your instrument panel or Cat EST, don’t dismiss them. They could alert you to a potential malfunction or failure that could damage your engine or affect its emissions compliance. Talk to your Cat dealer or check your service manual for troubleshooting and repair guidance.
Following these tips, you can keep your Cat engines in peak condition during summer. Contact your local Cat dealer for more information on maintaining your Cat engines.
Social Media & Digital Strategy Manager
Caitlin Maddock-Bahr exercises her storytelling expertise as a social media & digital strategy manager. In this role, she not only helps Caterpillar connect with their audience, but helps customers connect with the brand.
You’re here to get ideas to grow your business. Read on for machine insights and expert tips and tricks to get more out of every job.
Cat® experts offer valuable advice on keeping industrial diesel engines running smoothly during the cold winter months.
Learn MoreThree areas you don't want to overlook.
Learn MoreToday’s dozer blades are sophisticated tools. And you can’t make money without them—which makes them far from boring. So before you choose a blade, give some thought to how the decision could affect your bottom line.
Learn MoreSave time and money with our customizable bid specification option.
Learn More