If you already have an existing account with another Cat App, you can use the same account to sign in here
One Account. All of Cat.
Your Caterpillar account is the single account you use to log in to select services and applications we offer. Shop for parts and machines online, manage your fleet, go mobile, and more.
Account Information
Site Settings
Security
Focused on urban residential demolition, where it will compete in the 30 MT size class, the 330 UHD features a UHD boom with a maximum pin height of up to 20 m (65’ 6”) to make it comfortably capable of 5 to 6-story work.
IRVING, Texas, March 7, 2025―Caterpillar Inc. is proud to announce the launch of the next generation ultra-high demolition excavator, the Cat® 330 UHD, designed to be a highly versatile machine with uncompromised functionality and enhanced safety for emergency responses, urban and city operations.
Focused on urban residential demolition, where it will compete in the 30 MT size class, the 330 UHD features a UHD boom with a maximum pin height of up to 20 m (65’ 6”) to make it comfortably capable of 5 to 6-story work.
Yet it is essentially two machines in one. While the UHD boom accommodates all standard demolition work tools, the machine also accepts two types of retrofit booms (single and variable angle (VA) boom type). The changeover to deploy traditional buckets and work tools in the role of a ‘standard’ construction excavator takes a short amount of time.
Vincent Migeotte
Senior Product and Sales Consultant
Caterpillar
The 330 UHD offers operators best-of-class performance with its capability of carrying a large demolition 3300 kg (7,275 lb) work tool at great height up to 20 m (65’6”). To optimise its utilisation with the retrofit boom, it is also configured with up-to-date technology such as Cat Payload, Cat 2D Grade control system, and Cat 2D E-fence. The latter helps keep the front linkage within a predefined work area, helping provide operator confidence while protecting the machine from damage and monitoring jobsite safety.
This operator-intuitive machine is equipped with a stability monitoring system that helps improve jobsite safety by using the in-cab 10-inch touchscreen monitor to display the machine’s stability via swing angle and front position. The monitor also displays images from the integrated standard rear and side-view camera; a surround-view attachment is an optional extra, while a work-tool camera and second monitor is a dealer-installed aftermarket option.
The tiltable cab is TOPS demolition-rated, fitted with a premium seat, P5A glass and full operator protective guards (OPG), helping improve jobsite visibility while providing ultimate operator comfort. The machine is also remote-control ready, which Migeotte says underlines a further design aspect.
Vincent Migeotte
Senior Product and Sales Consultant
Caterpillar
Powering fuel efficiently, the 330 UHD uses the same engine as the 330 Next Generation Excavator, the Cat C7.1 TTA. Meeting the U.S. EPA Tier 4 Final, EU Stage V, and Japan 2014 emission standards, the 7-litre unit is rated at 205 kW (275 hp) gross.
Prospective 330 UHD operators can also choose between two undercarriage types. The Long Narrow undercarriage uses the same base frame as the 330 Next Generation Excavator, maintaining the machine’s mobility within the all-important 3 m (3’ 10”) transportation width and a fully assembled weight under 40 MT. Alternatively, they can specify the Hydraulic Variable Gauge undercarriage, similar to that used on the 340F UHD, to provide the additional stability needed to function safely and confidently with the largest work tools.
Vincent Migeotte
Senior Product and Sales Consultant
Caterpillar
This model will further expand the lineup of purpose-built demolition machines from Caterpillar and demonstrate the company’s ongoing dedication to industrial and demolition applications.
Caterpillar began manufacturing demolition excavators in the early 1990s, starting with the 330 UHD and the 350 UHD. The first models featured the three-piece Ultra High Demolition front and wide undercarriage. Today, Caterpillar designs and manufactures six models of demolition excavators, including the 330 UHD.
For more information about 330 UHD Ultra High Demolition Excavator, contact a Cat dealer or visit: www.cat.com
Engine |
Cat C7.1 |
Net Power* – ISO 14396 |
275 hp (205 kW) |
Operating weight – Hydraulic Variable Gauge undercarriage, 20 m (65'7") UHD C front, 600 mm (24") triple grouser shoes, and 8.8 mt (19,400 lb) counterweight. |
101,400 lb (46 000 kg) |
Operating Weight – Hydraulic Variable Gauge Undercarriage, R3.2CB2 (10'6") retrofit boom front, 1.76 m³ HD (2.30 yd³) bucket, 600 mm (24") triple grouser shoes, and 8.8 mt (19,400 lb) counterweight. |
96,800 lb (43 900 kg) |
Max. weight at stick nose |
7,300 lb (3 300 kg) 1 8,400 lb (3 800 kg) 2 |
Max. digging depth |
18 ft 5 in (5.6 m) 2 |
*Net power advertised is the power available at the flywheel when the engine is equipped with fan, air intake system, exhaust system, and alternator with engine speed at 2,200 rpm. Advertised power is tested per the specified standard in effect at the time of manufacture.
1) 20 m (65'7") UHD Front
2) Retrofit Boom - 6.8 m (22'4") Straight - R3.2CB2 (10'6") Stick
# # #
About Caterpillar:
With 2024 sales and revenues of $64.8 billion, Caterpillar Inc. is the world’s leading manufacturer of construction and mining equipment, off-highway diesel and natural gas engines, industrial gas turbines and diesel-electric locomotives. For 100 years, we’ve been helping customers build a better, more sustainable world and are committed and contributing to a reduced-carbon future. Our innovative products and services, backed by our global dealer network, provide exceptional value that helps customers succeed. Caterpillar does business on every continent, principally operating through three primary segments – Construction Industries, Resource Industries and Energy & Transportation – and providing financing and related services through our Financial Products segment. Visit us at caterpillar.com or join the conversation on our social media channels at caterpillar.com/en/news/social-media.html.
NOTE TO EDITORS: Caterpillar rolls out products and services in each of its regions at different time intervals. Although every effort is made to ensure that product information is released only after Caterpillar has received confirmation from its independent dealer network, plants, and marketing subsidiaries that products and services are available in the relevant region, editors are kindly requested to verify with a Cat dealer for product availability and specifications.
CAT, CATERPILLAR, LET’S DO THE WORK, their respective logos, “Caterpillar Corporate Yellow,” the “Power Edge” and Cat “Modern Hex” trade dress, as well as corporate and product identity used herein, are trademarks of Caterpillar and may not be used without permission.
VisionLink is a trademark of Caterpillar Inc., registered in the United States and in other countries.
The machine is the first next generation design of off-highway trucks for the company. Distinguishing it from the previous 775 models, this 65-tonne (71-ton) payload hauler is engineered to enable fully autonomous capabilities in the future.
Learn MoreThe new Cat® Tiltrotator line helps to deliver significant cost savings by reducing the number of machines and ground staff at the site.
Learn MoreThe Cat® PM600 and PM800 cold planer series deliver high-production and efficient performance with the milling precision contractors need to stay competitive.
Learn MoreUnhindered operation in tight or restricted excavating and demolition jobsites is Caterpillar’s thinking behind the Variable Angle Boom (VAB) option now available for the Cat® 340 Hydraulic Excavator.
Learn More