If you already have an existing account with another Cat App, you can use the same account to sign in here
One Account. All of Cat.
Your Caterpillar account is the single account you use to log in to select services and applications we offer. Shop for parts and machines online, manage your fleet, go mobile, and more.
Account Information
Site Settings
Security
The machine is the first next generation design of off-highway trucks for the company. Distinguishing it from the previous 775 models, this 65-tonne (71-ton) payload hauler is engineered to enable fully autonomous capabilities in the future.
MUNICH, Germany, April 7, 2025―Caterpillar Inc. is showcasing the new Cat® 775 off-highway truck at bauma-Munich 2025, spotlighting the company’s ongoing leadership in technology and autonomous capabilities. The machine is the first next generation design of off-highway trucks for the company. Distinguishing it from the previous 775 models, this 65-tonne (71-ton) payload hauler is engineered to enable fully autonomous capabilities in the future.
Tony Fassino
Group President of Construction Industries
Caterpillar
Caterpillar is leveraging its current Autonomous Hauling Systems (AHS), Cat® MineStarTM Command for hauling, already at work at mine sites throughout the world, and scaling the system’s processes and technology to meet the specific needs for quarry operations.
Denise Johnson
Group President of Caterpillar Resource Industries
Caterpillar
The Cat 775 next generation truck has a planned introduction in 2026. Autonomous capabilities with MineStar Command for hauling are currently under development, and a release date will be announced at a later date.
The 775 features an innovative new frame design that helps to optimize payload weight, a refined suspension for improved ride and handling, and advanced safety features like the 360-degree surround cameras and Cat Detect radar system to deliver superior performance and safer and more comfortable operation.
David Holthaus
Senior Engineer and Team Lead for the Cat 775
Caterpillar
With more body volume, the truck’s new frame is optimized for weight distribution and structural efficiency. Compared to the 775G series truck, there is nearly 30% less welding to minimize the risk of cracks and improve frame life. Less internal welding and ease of frame repairability help lower costs to maintain the new 775 over an estimated 40,000-hour truck life.
Its redesigned suspension boasts a lower center of gravity. The 775 has shown to deliver better handling than previous designs, and an updated turning radius enhances on-site maneuverability. Improving service life, the truck experiences less bouncing on the tires and driveline, and the operator feels less vibration and energy feedback into the truck.
The truck is powered by the 615-kw (825-hp) Cat C27 engine and comes in different emissions configurations to meet different global regulations. The U.S. EPA Tier 4 Final/Stage V version displayed at bauma offers better fuel efficiency than previous models, with advanced electronic powertrain controls that deliver faster cycles and reduced road maintenance. The truck’s enhanced ride and handling allow for higher speeds on curves and driving in higher gears, which directly reduces fuel consumption during the cycle.
The new cab is designed for efficiency and equipped with features to automate functions. The large windows give the operator visibility to the work area and surroundings. Automatic cab temperature controls and the Cat next generation deluxe seat is designed to help to improve operator comfort.
Its 360-degree surround cameras with object detection alerts operators to hazards within the immediate vicinity, making it easier to safely operate the new 775. Cat Detect combines radar and camera systems to automatically detect hazards within critical areas around the truck―primarily the front, rear and turning radius on each side.
Multiple key maintenance and service contributors have been reduced with the new truck design. The next generation of enhanced serviceability incorporates extended-interval filters with ground-level access, ground-level lockout features and a serviceable suspension. Its design is fire suppression ready to simplify system installation.
The ability to access and analyze accurate real-time data enables faster diagnostics and enhances the ability to predict and prevent machine failure. New for the 775, remote flash and troubleshooting capabilities help to boost truck availability. Remote flash instantly provides access to the latest software updates and enables the updates to be scheduled and executed at a time that doesn’t interrupt the production schedule. Remote Troubleshoot enables the dealer to perform diagnostics remotely while the truck is still in operation.
More information on the new next generation Cat 775 off-highway truck can be found by contacting a Cat dealer or by visiting cat.com.
Engine |
Cat® C27 |
Gross power SAE J1995 – kW (hp) |
615 (825) |
Gross vehicle weight – kg (lb) |
111 811 (246,500) |
Nominal payload capacity – tonne (ton) |
65 (71) |
# # #
About Caterpillar:
With 2024 sales and revenues of $64.8 billion, Caterpillar Inc. is the world’s leading manufacturer of construction and mining equipment, off-highway diesel and natural gas engines, industrial gas turbines and diesel-electric locomotives. For 100 years, we’ve been helping customers build a better, more sustainable world and are committed and contributing to a reduced-carbon future. Our innovative products and services, backed by our global dealer network, provide exceptional value that helps customers succeed. Caterpillar does business on every continent, principally operating through three primary segments – Construction Industries, Resource Industries and Energy & Transportation – and providing financing and related services through our Financial Products segment. Visit us at caterpillar.com or join the conversation on our social media channels at caterpillar.com/en/news/social-media.html.
NOTE TO EDITORS: Caterpillar rolls out products and services in each of its regions at different time intervals. Although every effort is made to ensure that product information is released only after Caterpillar has received confirmation from its independent dealer network, plants, and marketing subsidiaries that products and services are available in the relevant region, editors are kindly requested to verify with a Cat dealer for product availability and specifications.
CAT, CATERPILLAR, LET’S DO THE WORK, their respective logos, “Caterpillar Corporate Yellow,” the “Power Edge” and Cat “Modern Hex” trade dress, as well as corporate and product identity used herein, are trademarks of Caterpillar and may not be used without permission.
VisionLink is a trademark of Caterpillar Inc., registered in the United States and in other countries.
The new Cat® Tiltrotator line helps to deliver significant cost savings by reducing the number of machines and ground staff at the site.
Learn MoreThe Cat® PM600 and PM800 cold planer series deliver high-production and efficient performance with the milling precision contractors need to stay competitive.
Learn MoreUnhindered operation in tight or restricted excavating and demolition jobsites is Caterpillar’s thinking behind the Variable Angle Boom (VAB) option now available for the Cat® 340 Hydraulic Excavator.
Learn MoreThe Cat® 330 UHD, designed to be a highly versatile machine with uncompromised functionality and enhanced safety for emergency responses, urban and city operations.
Learn More