Caterpillar’s 140 Motor Grader moves to the next generation

The new model, which features the next generation hallmarks of efficiency, productivity and operator comfort, will debut at bauma 2025 in Munich.

Highlights

  • Increased uptime includes extended and synchronized maintenance intervals plus centralized success service points.
  • Integrated optional rear-, front-, and 360-degree-vision cameras, enhanced visibility and redesigned HVAC system and seat adjustment options in the cab.
  • Platform choice of joystick control or levers/steering wheel to accommodate operator preference.

 

of

IRVING, Texas, March 7, 2025―Caterpillar will be launching its new Cat® 140 Motor Grader, upgrading it to the next generation platform. The new model, which features the next generation hallmarks of efficiency, productivity and operator comfort, will debut at bauma 2025 in Munich. 

Versatility in operation has always been Caterpillar’s strength, and the 140 Motor Grader has been a classic demonstration of that virtue.

Pablo dos Santos

Global Product Application Specialist

Caterpillar

Over the years, customers have shown that the 140’s usefulness and flexibility has few limits. Its frame lends itself to easy transportation, and its power and performance have seen it put to work in everything from snow clearance to sugarcane operations, in addition to its everyday use in roadbuilding and ditching. 

 

The machine’s versatility, which has made it very popular with rental fleets, as well as government and municipal contracts, will be enhanced by moving to the next generation platform. 

Pablo dos Santos

Global Product Application Specialist

Caterpillar

Safety and efficiency rely on good visibility, so the Cat 140 Motor Grader features the highly successful cab design from the 120 next gen models. Larger windows provide better visibility out of the cab, ensuring better all-round views, including mouldboard and tyres, while an as-standard rearview camera augments direct lines of sight.

The camera feed is integrated into the 10-inch touchscreen, which also provides operator access to other next generation functions such as Cat Grade. A new seat takes advantage of the next gen cab’s greater footspace and hip room, offering a variety of adjustments to improve operator comfort and reduce fatigue. The cab features revised seatbelt and safety harness options.

Also benefiting from the next gen upgrade are the 140’s joystick controls. While Caterpillar has stuck with its industry-exclusive three axis joystick system, which studies show is more ergonomical for operators than levers and a steering wheel, the 140 makes several updates to the joysticks themselves to help further boost productivity.

The new Cat 140 continues its proven design and exceptional reliability to ensure low operating costs coupled with favourable fuel efficiency. The 140 features banked and centralised access checkpoints that make daily maintenance a breeze rather than a bind. 

 

What’s more, the new 140 provides a ‘sweet spot’ power-to-weight ratio with excellent fuel consumption rates.

Pablo dos Santos

Global Product Application Specialist

Caterpillar

There is a lot of good information collected so far from the multiple machines being tested in the world with more than 40.000 hours accumulated so far.

The new Cat 140 also offers expanded technology capabilities, from simple features to improve operator’s comfort, like the stable blade, to fully calibrated 3D systems for reduced total cost of ownership. 

 

It’s exciting to see Caterpillar’s most popular motor grader model joining the Cat® 120 Motor Grader receiving next generation treatment. We expect it will only add to the machine’s popularity.

Pablo dos Santos

Global Product Application Specialist

Caterpillar

The new Cat 140 is due for production in Q1, 2026. 

 

 

A Century of Innovations

Caterpillar began manufacturing motor graders in 1931 with the No. 9 Cat Auto Patrol. The first motor graders boasted lever and steering wheel controls and a 9-foot mouldboard. Presently, Caterpillar manufactures 13 motor grader models in facilities across the globe.

For more information about the Cat 140 Motor Grader, contact a Cat dealer or visit: www.cat.com

 

of

Cat® 140 Motor Grader

View Full Size Image
of

Cat® 140 Motor Grader

View Full Size Image
of

Cat® 140 Motor Grader

View Full Size Image
of

Cat® 140 Motor Grader

View Full Size Image
of

Cat® 140 Motor Grader

View Full Size Image
of

Cat® 140 Motor Grader

View Full Size Image

 

 

Download the Press Release

Download Now

Download the Images 

Download Now

 

 

# # #

About Caterpillar:
With 2024 sales and revenues of $64.8 billion, Caterpillar Inc. is the world’s leading manufacturer of construction and mining equipment, off-highway diesel and natural gas engines, industrial gas turbines and diesel-electric locomotives. For 100 years, we’ve been helping customers build a better, more sustainable world and are committed and contributing to a reduced-carbon future. Our innovative products and services, backed by our global dealer network, provide exceptional value that helps customers succeed. Caterpillar does business on every continent, principally operating through three primary segments – Construction Industries, Resource Industries and Energy & Transportation – and providing financing and related services through our Financial Products segment. Visit us at caterpillar.com or join the conversation on our social media channels at caterpillar.com/en/news/social-media.html.

NOTE TO EDITORS: Caterpillar rolls out products and services in each of its regions at different time intervals. Although every effort is made to ensure that product information is released only after Caterpillar has received confirmation from its independent dealer network, plants, and marketing subsidiaries that products and services are available in the relevant region, editors are kindly requested to verify with a Cat dealer for product availability and specifications.

CAT, CATERPILLAR, LET’S DO THE WORK, their respective logos, “Caterpillar Corporate Yellow,” the “Power Edge” and Cat “Modern Hex” trade dress, as well as corporate and product identity used herein, are trademarks of Caterpillar and may not be used without permission.

VisionLink is a trademark of Caterpillar Inc., registered in the United States and in other countries.

 

 

Press Inquiries:

Amy Doughty
Caterpillar Trade Press Media Representative

Amy.Doughty@cat.com

 
For Release: Europe
Release Number: 38PR25 — March 2025


Motor Graders

Built with decades of design experience, you'll find the perfect Cat® motor grader for your grading application. With world-class cabs, advanced hydraulics, control-type options and technology options, you'll complete your grading projects on time and at a lower cost.

Learn More
Motor Graders
Motor Graders

The Latest Product News

Get the Latest Stories Sent Directly to Your Inbox.

Subscribe Now