The Cat Hydraulic Connecting CW Coupler
The Cat Hydraulic Connecting CW Coupler

New Cat® Hydraulic Connecting CW couplers for excavators deliver fast and safe attachment changes with less spillage

 

For Release in Africa, Europe, Middle East and Turkey: May 2024
Release Number: 127PR24

 

  • Operators can trade out attachments within seconds from the cab
  • Internally routed hoses protect against damage, reducing costs
  • Compatible with any Cat® hydraulic attachment  

 

Building on decades of field success with the CW coupler platform, Caterpillar announces three new Cat® Hydraulic Connecting CW (HCCW) coupler models. Connecting seamlessly to the machine’s hydraulics, HCCW quick couplers allow operators to switch between hydraulic attachments with full functionality in seconds from the safety of the cab.

Compatible with any Cat hydraulic attachment, quick changes with the HCCW give the operator the ability to use the right attachment for the job, increasing overall productivity and tool utilization. Fast attachment swap outs with the hydraulic connecting interface can help save time over static couplers or pin-on attachments. The field proven CW coupler platform is built to last and keep costs low.

The new HCCW20, HCCW30 and HCCW40 quick couplers work with a range of tool carrier capacities, from 7.5 to 27 tons. Each model offers a standard 10-ton lift capacity, and exclusive Locking Control System feature and sensor technology measure locking wedge position and indicate coupling status to the operator. Complying with the European EN474 standard, multiple electronic and mechanical measures help to secure the attachment, even in the event of pressure loss. Visual and audible confirmations inside the cab inform the operator of successful attachment connection.

The new design features enhanced hydraulic flow to reduce hydraulic restriction, minimizing heat build-up and reducing the amount of engine power required for operation. Machined and sized for high-flow performance, the couplings ensure hydromechanical attachments operate to full capability with limited back pressure. Their reliable hydraulic fluid connections help to prevent spills when changing the attachment, while the quick-disconnect design helps improve the lifespan and facilitates servicing ease.

Customers with existing Cat excavator fleets using CW hinges do not need to retrofit their machines to use the new HCCW quick couplers. Fabricated tools, such as buckets, can seamlessly switch between existing CW and new HCCW couplers. New Hydraulic Coupling (HC) brackets allow the use of existing hydromechanical tools like shears, hammers and grapples with the HCCW.

Internally routed hoses in the coupler and bracket protect against damage and reduce overall hose and repair costs. They leverage the trusted quick-coupler platform with the addition of proven, durable and high-performing male and female quick disconnects located in the coupler and the attachment bracket. The cover lid and sealing provide added protection for couplings and prevent hydraulic system contamination.

For more information about the new Cat Hydraulic Connecting CW Couplers, contact a Cat dealer or visit: www.cat.com.

 

Hydraulic Connecting CW Coupler Specifications 

 

Model

HCCW20

HCCW30

HCCW40

Minimum carrier weight, ton

7.5

15

20

Maximum carrier weight, ton

15

20

27

Hydraulic pressure lock max, bar (psi)

120 (1,740)

120 (1,740)

120 (1,740)

Hydraulic pressure unlock max, bar (psi)

350 (5,076)

350 (5,076)

350 (5,076)

Weight, kg (lb)

160.6-166 (354-366)

171.9-172.8
(379-381)

171-186.4 (377-411)

Lift hook capacity, ton (lb)

10 (20,000)

10 (20,000)

10 (20,000)

 

 

Download the press release and images 

Download Now

 

 

of

The Cat® Hydraulic Connecting CW Coupler seamlessly connects to the machine’s hydraulics, enabling the operator to pick up an attachment with full functionality in seconds from the safety of the cab.

View Full Size Image
of

Swiftly swap attachments with the Cat® Hydraulic Connecting CW Coupler. Attachments can be shared between machines in the same size class.

View Full Size Image
of

The fast attachment changes with the hydraulic connecting interface of the Cat® Hydraulic Connecting CW Coupler can help save time over static couplers or pin-on attachments.

View Full Size Image
of

Hydraulic Connecting CW Coupler with a P324 Primary Pulverizer.

View Full Size Image
of

The MP324 Multi-Processor in the process of attaching to the Hydraulic Connecting CW Coupler.

View Full Size Image
of

Hydraulic Connecting CW Coupler with a S3025 Rotary Scrap & Demolition Shear.

View Full Size Image
of

Hydraulic Connecting CW Coupler with a P324 Primary Pulverizer.

View Full Size Image

Product & Service News

See the latest product and engine announcements from Caterpillar.

See the Latest News

 

# # #

 

CAT, CATERPILLAR, LET’S DO THE WORK, their respective logos, “Caterpillar Corporate Yellow,” the “Power Edge” and Cat “Modern Hex” trade dress, as well as corporate and product identity used herein, are trademarks of Caterpillar and may not be used without permission.

 

©2024 Caterpillar All Rights Reserved

 

Press Inquiries

Caterpillar Trade Press Media Representatives

Americas
Kate Kenny: Kenny_Kate@cat.com
Johanna Kelly: Kelly_Johanna_L@cat.com

Europe, Africa, Middle East
Amy Doughty: Amy.Doughty@cat.com