If you already have an existing account with another Cat App, you can use the same account to sign in here
One Account. All of Cat.
Your Caterpillar account is the single account you use to log in to select services and applications we offer. Shop for parts and machines online, manage your fleet, go mobile, and more.
Account Information
Site Settings
Security
For EAME Release: January 5, 2022
Release Number: 50PR22
New Cat® Industrial Power Units are Ready to be Put to Work
Caterpillar has launched a range of drop-in engines, which are ready to get to work straight away, thanks to their ease of installation and dependable and robust design.
The new Cat® C2.8 and C3.6 industrial power units (IPU) feature a highly integrated design that saves customers time on engineering and installation. Common rail direct injection engines with a turbocharged or turbocharged aftercooled air system, the C2.8 and C3.6 meet EU Stage V, U.S. EPA Tier 4 Final and Japan 2014 (Tier 4 Final) emission standards.
For ease of installation, the IPUs which are targeted at the construction and materials handling industries, provide customers with full aftertreatment mounting, an integrated cooling system, a full wiring harness and mounting for the ECM and fuel filter.
Plug In and Go Design
The new C2.8 and C3.6 IPU engines are cleverly engineered to provide the performance and efficiency customers expect from Caterpillar, all while saving equipment manufacturers time with a plug in and go design, meaning minimal engineering or design work.
The engines are offered in ratings ranging up to 55 kW (74 hp) at 2400 rpm for the C2.8 and up to 100 kW (134 hp) at 2200 rpm for the C3.6.
A flexible design makes these lightweight and compact engines ideal for use in construction and materials handling, and across different environments, be it for a compressor in Dubai or a crusher in Norway.
“We’re really pleased to launch these new IPUs,” says Steve Ferguson, Vice President Industrial Power Systems. “We know our customers will really value these compact and highly integrated engines, which thanks to the minimal engineering required, are ready to be put to work.”
Time-Efficient Engine Solutions
Our IPU range is designed with the customers in mind, so the C2.8 and C3.6 offerings feature:
Cat Dealer Support
Product support to keep the new C2.8 and C3.6 IPU engines operating at maximum efficiency is provided by the world-class global Cat dealer network. Cat dealers offer genuine Cat parts and a variety of services to optimize engine life and lower operating costs. In addition, dealer service technicians are trained to service the entire Cat industrial diesel engine range.
For more information on the C2.8 and C3.6 IPU including a virtual product tour visit www.cat.com/C28andC36IPU
###
Note to Editors: Caterpillar rolls out products and services in each of its territories at different time intervals. Although every effort is made to ensure that product information is released only after Caterpillar has received confirmation from our dealer network, our plants, and our marketing subsidiaries that products and services are available in the relevant region, editors are kindly requested to verify with their local dealer for product availability and specifications.
CAT, CATERPILLAR, LET’S DO THE WORK, their respective logos, “Caterpillar Corporate Yellow,” the “Power Edge” and Cat “Modern Hex” trade dress, as well as corporate and product identity used herein, are trademarks of Caterpillar and may not be used without permission.
©2022 Caterpillar All Rights Reserved
Press Inquiries
Caterpillar Industrial Engines Trade Press Media Representatives
Europe, Africa, Middle East
Annette Ward: Ward_Annette@cat.com
Reader Requests