If you already have an existing account with another Cat App, you can use the same account to sign in here
One Account. All of Cat.
Your Caterpillar account is the single account you use to log in to select services and applications we offer. Shop for parts and machines online, manage your fleet, go mobile, and more.
Account Information
Site Settings
Security
For Worldwide Release: May 1, 2023
IRVING, TEXAS – Caterpillar Inc. today announced that the company has added two new mobile solutions to its lineup of mobile diesel generator sets meeting European Union (EU) Stage V emission standards.
Now available through the Cat® dealer network, the Cat XQP20 and Cat XQP550 meet the requirements of Stage V standards, including a 90% reduction in nitrogen oxides when compared with the Stage IIIA standard. Caterpillar now offers five mobile generator sets from 20 to 550 KVA of prime power that meet the current European standard.
The Cat XQP20 is a suitable option for both owners and rental customers requiring reliable power for construction, industrial and commercial applications, as well as outdoor events. The Cat XQP550 meets specification requirements for a broad range of environments and applications, including manufacturing, oil and gas, mining, and construction.
“The addition of these mobile generator sets expands our ability to serve our European customers through a growing range of easy-to-operate power nodes that meet their rigorous application requirements while meeting EU Stage V emission standards,” said Tom Caldwell, global general manager for electric power rental solutions at Caterpillar.
Ready for Rugged Use on Jobsites
Caterpillar’s new mobile power solutions offer numerous features ideal for rental applications. The Cat XQP20 is equipped with easy-to-use GCCP1.3 digital controls and optional CE sockets, allowing power to be easily distributed across a worksite.
Meanwhile, the Cat XQP550 uses the XQCP digital control panel, which provides all generator set controls and system indicators in a single, easy-to-access interface. Additionally, programmable logic controller (PLC) functionality improves the reliability and flexibility of the Cat XQP550 for accommodating changes in processes or application requirements.
Both mobile solutions feature Cat Connect technology to remotely track and manage, improve operational efficiency, control costs and reduce risks. It supports optimal operation by offering timely insights into performance, such as fuel level, run status and battery voltage.
The Cat XQP20 and Cat XQP550 are designed with a dual-wall fuel tank with an open bund that helps to protect the environment by containing spills, while coastal insulation protection (CIP) enables operation in harsh conditions.
Their wide, impact-absorbing base frames, customer connections isolated from circuit breakers, and optional CEE sockets are designed to facilitate transportation, set-up and use. Forklift pockets, dragging points, and a lifting arch help to simplify loading, unloading, and placement around the worksite.
Cat mobile generator sets meeting EU Stage V emission standards can use up to 100% hydrotreated vegetable oil (HVO), a renewable diesel fuel meeting EN15940.
All Cat mobile generator sets are available through the worldwide Cat dealer network. Cat dealers work 24 hours a day, seven days a week to assist with emergency rental needs and provide a comprehensive range of maintenance and services.
For more information, visit www.cat.com/euv or e-mail Electric_Power@cat.com.
###
About Caterpillar
With 2022 sales and revenues of $59.4 billion, Caterpillar Inc. is the world’s leading manufacturer of construction and mining equipment, off-highway diesel and natural gas engines, industrial gas turbines and diesel-electric locomotives. For nearly 100 years, we’ve been helping customers build a better, more sustainable world and are committed and contributing to a reduced-carbon future. Our innovative products and services, backed by our global dealer network, provide exceptional value that helps customers succeed. Caterpillar does business on every continent, principally operating through three primary segments – Construction Industries, Resource Industries and Energy & Transportation – and providing financing and related services through our Financial Products segment. Visit us at caterpillar.com or join the conversation on our social media channels.
© 2023 Caterpillar. All Rights Reserved. CAT, CATERPILLAR, LET’S DO THE WORK, their respective logos, “Caterpillar Corporate Yellow,” the “Power Edge” and Cat “Modern Hex” trade dress, as well as corporate and product identity used herein, are trademarks of Caterpillar and may not be used without permission.
Press Inquiries
Bob Chase
Gelia
Tel: +1 716-629-3230
bchase@gelia.com
Steve McDonagh
Caterpillar Inc.
steve.mcdonagh@cat.com