Cat® Connect Remote Asset Monitoring Solution Now Standard on Diesel Generator Sets from 6.8 to 850 kVA (50 Hz) and 8 to 750 kW (60 Hz)

Free Remote Asset Monitoring Subscriptions Available through 2022

For Worldwide Release: February 7, 2022

DEERFIELD, IL – Caterpillar Inc. today announced that the company is providing, at no additional cost, factory-installed Cat® Connect Remote Asset Monitoring (RAM)—the advanced data collection, visualization reporting, and alert solution—on small- and medium-sized Cat diesel generator sets globally.* This is the latest step in Caterpillar’s strategy to configure its entire lineup of diesel generator sets with Cat Connect RAM, which is already offered as standard on larger diesel generator sets.**

In addition to the installation of the Cat Connect hardware as standard on Cat generator sets up to 850 kVA for 50 Hz applications and up to 750 kW for 60 Hz applications, Caterpillar will also offer customers a free Cat Remote Asset Monitoring standard subscription until December 31, 2022. Enhanced Cat Remote Asset Monitoring options are available where customers require additional monitoring of generator set parameters, and they are provided free of charge to customers who have purchased a Customer Value Agreement or Long-Term Service Agreement.  

Cat Connect hardware can be purchased as a retrofit item alongside a subscription on existing Cat and competitor power solutions.

“Equipment intelligence is increasingly important in helping the owners of power solutions to maximize the performance of their equipment and better manage their total costs of ownership,” said Jaime Mineart, general manager for Caterpillar Electric Power. “This standard capability makes it easier than ever for Cat generator set owners to improve efficiency, reduce risk, cut costs, and boost their bottom lines by leveraging Cat technology and energy expertise.”

The Cat Connect and Cat RAM package enables the real-time collection and remote monitoring of site performance data across Caterpillar’s product portfolio. Providing data visualization, reporting, and alerts from anywhere in the world through an easy-to-use web interface or mobile app, Cat RAM helps operators and Cat dealers track and manage the operation of Cat generator sets, flag potential problems, perform remote troubleshooting, manage operational expenses, and leverage long-term archives of site performance history to identify opportunities for further operational or system enhancements.

Cat RAM can monitor and analyze between 13 and 200 key generator set performance indicators, based on the generator set model and the Cat RAM subscription level selected. Depending upon the generator set model and Cat Connect hardware device, it can also be configured to use a cellular or local network connection to deliver intelligence to key customer contacts and Cat dealer technicians.

More than 18,000 Cat generator sets worldwide are already configured with factory-installed Cat Connect capabilities.

*  Country-specific exclusions may apply.

** Cat Connect Remote Access Monitoring will be available later in 2022 as standard with no additional charge on Cat GC diesel generator sets including DE1100 GC to DE1500 GC, DE800S GC to DE1250S GC, and D800 GC to D1250 GC models.

For more information, contact your local Cat dealer or visit cat.com/catconnect.

Caterpillar delivers innovative power systems engineered for durability, reliability, and value. The company offers worldwide product support, with parts and services packaged in customer value agreements available through the Cat authorized service and dealer network. In addition, dealer technicians are trained to provide a comprehensive range of maintenance and services that help customers optimize the total cost of ownership of Cat equipment.

Cat® Connect Remote Access Monitoring for power solutions

Product and Services News

See the latest product and engine announcements from Caterpillar.

See the Latest News

 

###

About Caterpillar

Since 1925, Caterpillar Inc. has been helping our customers build a better world – making sustainable progress possible and driving positive change on every continent. With 2021 sales and revenues of $51.0 billion, Caterpillar is the world’s leading manufacturer of construction and mining equipment, diesel and natural gas engines, industrial gas turbines and diesel-electric locomotives. Services offered throughout the product life cycle, cutting-edge technology and decades of product expertise set Caterpillar apart, providing exceptional value to help our customers succeed. The company principally operates through three primary segments - Construction Industries, Resource Industries and Energy & Transportation - and provides financing and related services through its Financial Products segment. For more information, visit caterpillar.com. To connect on social media, visit caterpillar.com/social-media.

© 2022 Caterpillar. All Rights Reserved. CAT, CATERPILLAR, LET’S DO THE WORK, their respective logos, “Caterpillar Corporate Yellow,” the “Power Edge” and Cat “Modern Hex” trade dress, as well as corporate and product identity used herein, are trademarks of Caterpillar and may not be used without permission.

Press Inquiries

Bob Chase
Gelia
Tel: +1 716-629-3230
bchase@gelia.com

Casie Summers
Caterpillar Inc.
Tel: +1 713-895-4568
summers_casie@cat.com

 

Reader Requests

Caterpillar Inc.
Electric Power Division
P.O. Box 0610
Mossville, IL 61552-0610