If you already have an existing account with another Cat App, you can use the same account to sign in here
One Account. All of Cat.
Your Caterpillar account is the single account you use to log in to select services and applications we offer. Shop for parts and machines online, manage your fleet, go mobile, and more.
Account Information
Site Settings
Security
For Worldwide Release: June 9, 2020
Release Number: EEPR0720
DEERFIELD, IL – Caterpillar Inc. announced the launch of three new power nodes for the Cat® C18 diesel generator set that offer higher power density, occupying up to 55% less floor space than a leading competitive product offering the same power outputs.
Available now, the new Cat C18 diesel generator set features three 60-Hz power nodes offering standby ratings from 650 kW to 750 kW and prime power ratings from 600 kW to 680 kW. It is designed for applications requiring certification to U.S. EPA Tier 2 emission standards, and an enclosure is available for applications requiring noise attenuation or protection from the elements.
“Standby power is a considerable investment for most smaller enterprises, so it’s critical to select an efficient, accurately sized solution that fits in the most compact space possible,” said Jason Kaiser, general manager for Caterpillar Retail Electric Power Solutions. “Caterpillar’s new generator sets with high power densities allow customers to get power when they need it most while substantially reducing upfront costs for site preparation, transportation, and installation.”
The Cat C18 diesel generator set with high power density is designed to meet the NFPA power restoration requirement for Level 1 systems and accept 100 percent block load in one step. It meets ISO 8528-5 requirements for steady state and load acceptance.
The Cat C18 generator set utilizes the field-proven Cat ADEM™ A4 engine control module (ECM). This module seamlessly integrates all engine functions including ignition, governing, and air-fuel ratio control for optimal performance while protecting the engine.
Caterpillar delivers innovative power systems engineered for durability, reliability, and value. The company offers worldwide product support, with parts and service available globally through the Cat authorized service and dealer network. In addition, dealer technicians are trained to service every aspect of Cat equipment.
For more information, visit www.cat.com/powerdensity or e-mail Electric_Power@cat.com.
###
About Caterpillar
Since 1925, Caterpillar Inc. has been helping our customers build a better world – making sustainable progress possible and driving positive change on every continent. With 2019 sales and revenues of $53.8 billion, Caterpillar is the world’s leading manufacturer of construction and mining equipment, diesel and natural gas engines, industrial gas turbines, and diesel-electric locomotives. Services offered throughout the product life cycle, cutting-edge technology, and decades of product expertise set Caterpillar apart, providing exceptional value to help our customers succeed. The company principally operates through three primary segments – Construction Industries, Resource Industries, and Energy & Transportation – and provides financing and related services through its Financial Products segment. For more information, visit caterpillar.com. To connect on social media, visit caterpillar.com/social-media.
© 2020 Caterpillar. All Rights Reserved. CAT, CATERPILLAR, LET’S DO THE WORK, their respective logos, "Caterpillar Corporate Yellow", the "Power Edge" and Cat “Modern Hex” trade dress as well as corporate and product identity used herein, are trademarks of Caterpillar and may not be used without permission.
Press Inquiries
Bob Chase
Gelia
Tel: +1 716-629-3230
bchase@gelia.com
Casie Summers
Caterpillar Inc.
Tel: +1 713-895-4568
summers_casie@cat.com
Reader Responses
Caterpillar Inc.
Electric Power Division
P.O. Box 0610
Mossville, IL 61552-0610