If you already have an existing account with another Cat App, you can use the same account to sign in here
One Account. All of Cat.
Your Caterpillar account is the single account you use to log in to select services and applications we offer. Shop for parts and machines online, manage your fleet, go mobile, and more.
Account Information
Site Settings
Security
The new Cat® 777 (05) Water Truck provides an efficient solution to help reduce haul road dust by addressing overwatering and underwatering issues using advanced technology.
IRVING, Texas, January 31, 2025 – Properly watered haul roads directly impact fleet cycle times and the ability to meet production targets. As haul road dust takes a toll on safety and productivity at mines and quarries, a water truck may be one of the most important pieces of support equipment at the site. The new Cat® 777 (05) Water Truck provides an efficient solution to help reduce haul road dust by addressing overwatering and underwatering issues using advanced technology.
The new 777 (05) is built on the Cat 777E truck platform, proven at mine, quarry and construction sites globally. The Cat C32B engine delivers durable and reliable performance with 765 kW (1,026 hp). The Advanced Productivity Electronic Control Strategy (APECS) features transmission and engine coordination to efficiently utilize available engine power. Optimized fuel mapping of the engine and adaptive economy mode determine the most efficient operating point for fuel efficiency.
An innovative truck for controlling haul road dust, the design integrates the truck, tank, and water delivery system, connected with technology. The Cat Water Delivery System (WDS) connects with Cat MineStar telematics to help operations manage the site more safely and productively with scalable technology packages to meet site needs. Customers can choose from two options: the Basic package which includes Equipment Tracking or the Premium package which includes both Equipment Tracking and Production Recording.
Factory-installed, ergonomic water controls are integrated into the truck’s design for convenient system operation. Operators can use the high-definition touchscreen to view important data about the water delivery system, such as water tank level, spray head selection and water displacement rate. An easy-to-reach keypad inside the cab, allows the operator to select and control the spray heads. The water delivery system is also equipped with a front cannon, controlled by a joystick to easily select between a fan spray or jet stream, with a maximum spray distance of 61 m (200 feet). The cab is also ROPS certified for additional operator safety in water-specific applications.
The new water truck’s exclusive Cat WDS features a self-contained hydraulic system that controls spray patterns independent of engine RPM for consistent watering. Variable water flow, based on the truck’s speed, automatically starts and stops when the truck slows or comes to a halt, addressing overwatering and subsequent poor traction at road intersections. The pump features soft startups and automatically shuts off when the tank is empty to minimize system damage.
Covering up to a 24-m (80-ft) wide road in a single pass, the system sprays at rates reaching 0.8 l/m2 (0.2 gal/ft2) at speeds of 4 to 40 kph (3 to 25 mph). Complete with auto shut-off to prevent overfilling, the water tank can be filled remotely, allowing the operator to remain inside the cab during the cycle to reduce potential operator slips and falls.
The innovative automated water delivery feature, called Auto Mode, enables the operator to remain focused on driving and site traffic to enhance safety. Auto Mode operation is an exclusive feature to Cat WDS and is recommended for most field applications to help place the correct amount of water on the haul road, reducing overwatering at intersections and corners as the truck slows down.
When connected to MineStar Production Recording, customers can collect data to measure Key Performance Indicators (KPIs) like operator watering procedures, fuel utilization and water usage. Field testing data from an open pit coal mine in a tropical environment has shown customer improvements in fuel efficiency when the water delivery system runs in Auto Mode versus manual mode operation. Results may vary depending on site operations and conditions.
The cloud-based MineStar application is designed to work with the Cat WDS to collect and communicate machine data, allowing site supervisors to monitor the water truck to know where and when it’s spraying water. Asset management options include productivity, water usage, fuel and water tank levels, when and where to apply water, and asset location.
Providing tracking capabilities without the need for infrastructure investment, MineStar Equipment Tracking delivers basic connectivity without interfering with existing fleet management systems. Helping to achieve a lower total cost of ownership, Equipment Tracking provides insights to help mines better manage their assets. It features service meter readings, fueling and recording data, location accuracy and replay, time utilization tracking with downtime and operator tracking, and automatic stoppage measurement.
Paired with Equipment Tracking, Production Recording delivers premium connectivity with an accurate and automated near-real-time measurement solution that reports on critical aspects of the watering cycle without requiring operator input. Giving visibility to the entire operation, it helps to discover opportunities for improving productivity. This premium package also includes water usage by truck/fill station, volume and rate of water put down over time and area covered, water delivery system setting by location, truck, and conditions, activity breakdown with time and distance – watering, not watering and stopped.
This integrated solution is fully supported by the Cat dealer and parts network. Covered by a Caterpillar factory standard warranty, the water truck is eligible for Cat equipment protection plans (EPP) and customer value agreements (CVAs). Retrofit kits on older Cat 777 truck platforms are also available with the option to add MineStar hardware, connected with cloud-based software, for an individual truck or an entire fleet.
More information on the new Cat 777 (05) Water Truck from Caterpillar OEM Solutions can be found by contacting a Cat dealer or visiting www.cat.com/watersolutions.
# # #
About Caterpillar:
With 2023 sales and revenues of $67.1 billion, Caterpillar Inc. is the world’s leading manufacturer of construction and mining equipment, off-highway diesel and natural gas engines, industrial gas turbines and diesel-electric locomotives. For nearly 100 years, we’ve been helping customers build a better, more sustainable world and are committed and contributing to a reduced-carbon future. Our innovative products and services, backed by our global dealer network, provide exceptional value that helps customers succeed. Caterpillar does business on every continent, principally operating through three primary segments – Construction Industries, Resource Industries and Energy & Transportation – and providing financing and related services through our Financial Products segment. Visit us at caterpillar.com or join the conversation on our social media channels at caterpillar.com/en/news/social-media.html.
Note to Editors: Caterpillar rolls out products and services in each of its regions at different time intervals. Although every effort is made to ensure that product information is released only after Caterpillar has received confirmation from its independent dealer network, plants, and marketing subsidiaries that products and services are available in the relevant region, editors are kindly requested to verify with a Cat dealer for product availability and specifications.
CAT, CATERPILLAR, LET’S DO THE WORK, their respective logos, “Caterpillar Corporate Yellow,” the “Power Edge” and Cat “Modern Hex” trade dress, as well as corporate and product identity used herein, are trademarks of Caterpillar and may not be used without permission.
VisionLink is a trademark of Caterpillar Inc., registered in the United States and in other countries.
The machine is the first next generation design of off-highway trucks for the company. Distinguishing it from the previous 775 models, this 65-tonne (71-ton) payload hauler is engineered to enable fully autonomous capabilities in the future.
Learn MoreThe new Cat® Tiltrotator line helps to deliver significant cost savings by reducing the number of machines and ground staff at the site.
Learn MoreThe Cat® PM600 and PM800 cold planer series deliver high-production and efficient performance with the milling precision contractors need to stay competitive.
Learn MoreIn a move demonstrative of the company’s continuing dedication to industrial applications, Caterpillar is strengthening its line-up of material handlers with the launch of the Cat® Next Generation MH3032 Material Handler.
Learn More