If you already have an existing account with another Cat App, you can use the same account to sign in here
One Account. All of Cat.
Your Caterpillar account is the single account you use to log in to select services and applications we offer. Shop for parts and machines online, manage your fleet, go mobile, and more.
Account Information
Site Settings
Security
For Worldwide Release: September 2021
Release Number: 750PR21
Featuring an entirely new, patent pending design, a new Cat® dipper improves performance and reliability in hard digging applications of the Canadian Oil Sands without increasing demands on the hoist and crowd capabilities of the Cat 7495 HF Electric Rope Shovel. Improvements to shimming and inserts alone are projected to increase uptime as much as 0.25%, potentially leading to significant gains in production.
The new design optimizes lip cutting angle, resulting in significantly reduced heel wear. Improving stiffness and dig performance, the ground engagement tools are pitched at an upward angle that results in less bending force and even tooth wear top to bottom.
Approximately 7% lighter than the current 45.9 m3 (60 yd3) latched dipper, the new design delivers more available cutting force for more consistent fill factors and increased production in difficult digging conditions. Using Finite Element Analysis (FEA) and virtual validation tools, engineers reduced the dipper’s weight, translating to lower stress on the machine, as well as longer life and improved reliability for key components of the shovel’s front end.
The dipper features a new vertical latch system that delivers improved system performance and lower part maintenance, reducing overall operating costs. Rather than sliding, the latch’s tapered-end design lifts the insert surfaces away from each other. The design extends wear life while reducing service time, contributing to improved uptime. The latchbar guide plate features a quick-change design, further reducing maintenance time and costs.
Optimized linkage on the new single wet-disk snubber reduces the rotational kinetic energy of the door by more than 40% on closing and 75% during opening, increasing service life.
Caterpillar engineers tested more than 300 dipper shapes and configurations in over 900 simulations using Cat proprietary software to analyze performance data, completing stress plots and wear plots for the models. The “virtual” machine, operator, and pile were all validated using actual machine data reviewed by Caterpillar subject matter experts for accuracy. The simulations showed that with the new dipper geometry, customers can achieve better penetration and fills per pass.
More information on the new Cat dipper can be found by visiting Caterpillar MINExpo 2021 exhibit #6229, contacting the regional Cat dealer or visiting www.cat.com.
# # #
CAT, CATERPILLAR, LET’S DO THE WORK, their respective logos, “Caterpillar Corporate Yellow,” the “Power Edge” and Cat “Modern Hex” trade dress, as well as corporate and product identity used herein, are trademarks of Caterpillar and may not be used without permission.
©2021 Caterpillar All Rights Reserved
Press Inquiries |
Caterpillar Trade Press Media Representatives Americas Sharon Holling: Holling_Sharon_L@cat.com Johanna Kelly: Kelly_Johanna_L@cat.com Europe, Africa, Middle East Francine Shore: Shore_Francine_M@cat.com |
Reader Requests |