CONTINUOUS POWER, SECURE FACILITY

cumberland
cumberland

Security That Depends on Reliable Backup Power

Location: Crossville, Tennessee, USA

Customer Business Issue: Reliable backup power for jail operations to provide safety for inmates and staff

Solution: Cat® D300 GC diesel generator set

Cat® Dealer: Stowers Machinery

of

The Cumberland County Jail holds up to 212 inmates awaiting trial or sentencing and supports surrounding municipalities.

of

“The most important part of this complex is the jail. We have inmates and staff in here, so if we don’t have power, we’re putting both my staff and the inmates at risk.” –Captain Tim Claflin

of

The Cat® D300 GC diesel generator set fits within the footprint of the previous generator set and utilizes diesel fuel tanks already installed at the jail.

of

A member of the Cumberland County maintenance staff starts the generator on a weekly basis and performs routine inspections

of

The generator set has run numerous times during scheduled outages or grid power failure due to storms, keeping both inmates and staff safe by keeping the facility powered up.

POWER NEED

The Cumberland County Jail is a medium-security detention center located in Crossville, Tennessee. Operated by the Cumberland County Sheriff’s Office, the facility holds up to 212 inmates awaiting trial or sentencing and supports surrounding municipalities that do not have their own long-term lockup capabilities. It also houses electronic monitoring and control systems, as well as administrative offices.

Due to the critical nature of the facility, the Tennessee Correctional Institute requires the jail to have a backup source of power.

“The most important part of this complex is the jail,” said Captain Tim Claflin, lead administrator for the Cumberland County Jail. “We have inmates and staff in here, so if we don’t have power, we’re putting both my staff and the inmates at risk.”

In October 2019, a 28-year-old diesel generator set that provided backup power to both the jail and the jail administration offices failed, requiring an immediate solution. Repairing the unit proved too costly, which prompted Cumberland County officials to seek a solution that would fit within the original footprint and use the diesel fuel tanks already installed at the facility.

SOLUTION

County officials selected Stowers Machinery, the local Cat® dealer, to supply a 300 kW Cat D300 GC diesel generator set for the jail. Stowers Machinery supplied a mobile generator set while the new system was installed, and the dealer will provide ongoing support through a Customer Value Agreement (CVA).

To purchase the generator set, Cumberland County utilized Sourcewell, a municipal contracting agency that serves government, education and nonprofit organizations with a cooperative purchasing program that manages solicitation requirements and offers a network of awarded contracts.

“Cost was a big factor, and I think it will be proven over time that we made the right decision,” Claflin emphasized.

Cat GC diesel generator sets are configured with an optimized mix of common features that offer excellent customer value by delivering performance with a minimal footprint. They are engineered to Caterpillar’s high standards for reliability and productivity, with best-in-class support from the Cat dealer network.

“The Cumberland County Sheriff’s Office depends on reliable power for the safety of its inmates and staff,” said Jason Kaiser, general manager for Caterpillar Retail Electric Power Solutions. “The Cat GC generator set for the Cumberland County Sheriff’s Office demonstrates how we can deliver the performance our customers need in a right-sized package that minimizes purchasing and installation costs.”

RESULTS 

 Commissioned in the spring of 2020, the generator set has run numerous times during scheduled outages and when power from the grid was lost due to storms.

“It comes on and we hardly know that it’s running,” Claflin noted. “It does exactly what it’s supposed to do, and we’re happy with the choice we made.”

A member of the Cumberland County maintenance staff starts the generator on a weekly basis and performs routine inspections, while technicians from Stowers will provide semi-annual inspections and preventive maintenance. 

“It’s just a great working relationship that we have with Stowers. We’re very pleased with them and with Caterpillar in the product that we got,” Claflin concluded. “We sure love the idea of having a good product that will last and deliver reliable power for years to come.”

Download the Power Profile

Featured Products

  • D300 GC
    Maximum Rating
    300 ekW
    300 ekW
    Minimum Rating
    300 ekW
    300 ekW
    Emissions/Fuel Strategy
    EPA Stationary Emergency
    EPA Stationary Emergency

    D300 GC

    Producing reliable power of 300 ekW at 60 Hz, our D300 GC diesel generator set are designed to ISO 8528-5 transient response requirements. The D300 GC generator sets are engineered to EPA Stationary Emergency (Tier 3) emissions standards.

    Learn More

Electric Power products

Any size or shape. In any regulatory environment. When you need power, Caterpillar is equal to the challenge. Our generators are used in a variety of applications.

View Electric Power products
electric power
electric power

Generator Set Sizing Calculators

Cat Electric Power now has two tools available for sizing gensets in any application. 

Size Now
genset sizing
genset sizing

Municipality

You’re trusted to provide the power your community lives on — and makes a living with. Whether it’s standby power for emergency use or additional systems to handle peak hours, be there when the people you serve need it most.

View Municipality Page
Municipality
Municipality

CAT DEALERS MAKE THE DIFFERENCE

Your Cat dealer is committed to maximizing your success, helping you get the most out of your operations with site-level solutions, service, and support.

CONNECT WITH YOUR DEALER TODAY
dealers
dealers