If you already have an existing account with another Cat App, you can use the same account to sign in here
One Account. All of Cat.
Your Caterpillar account is the single account you use to log in to select services and applications we offer. Shop for parts and machines online, manage your fleet, go mobile, and more.
Account Information
Site Settings
Security
Customer: Tift Regional Medical Center
Location: Tifton, Georgia, USA
Customer Business Issue: Standby power for mission critical facility
Solution:
• One Cat C32 diesel generator set
• Cat Automatic Transfer Switch
• Cat paralleling switchgear
• Start up, testing, commissioning, maintenance
Cat Dealer: Yancey Power Systems
Tift Regional Health System is a not-for-profit hospital network serving 12 counties in southern Georgia. The main campus, Tift Regional Medical Center (TRMC), is a 191- bed facility located in Tifton that offers a full line of specialty medical services, including oncology, cardiovascular, radiology, robotics, neuro-diagnostics, geriatric psychology and women’s health, to name a few.
Established in 1965 as a general hospital, TRMC developed from humble beginnings, but it would be hard to see that today. Multiple expansions over the last 50 years have made the hospital Tift County’s largest employer, with more than 125 physicians covering 30 specialties.
To ensure the campus has a continuous supply of power, even in crisis situations, TRMC requires emergency backup power for life-safety systems and other essential operations.
“Operating solely on 1MW and 600kW generator sets, we were at our capacity and required an additional reliable backup power source,” said Don Gay, director of facilities, engineering and safety for TRMC.
TRMC’s needs went beyond standby emergency power, the existing backup power equipment was not capable of providing thorough and accurate computer generated reports. A Joint Commission accredited healthcare facility must prove either a 30 percent load on generators monthly or operate a load bank once a year with resistive loads. With handwritten reports, TRMC had no way of verifying the load to inspectors.
“We were accustomed to working off of handwritten reports during a time when software-generated reports of run times and power loads were the standard,” stated Robert Setters, plant operations manager for TRMC. They attempted to work with their existing power system supplier, “Ultimately, we switched gears and decided to give Caterpillar a look,” he said.
TRMC worked with the local Cat® dealer, Yancey Power Systems, to develop a customized standby power solution. The new system runs on an additional Cat C32 diesel generator set with upgraded paralleling switchgear to control all three generators including the existing 1MW and 600 kW units and provide 2.6 MW of backup power.
“The upgraded paralleling switchgear was a good fit for TRMC,” explained Danny Barber, aftermarket sales manager for Caterpillar Switchgear. “Due to the service experience of our technicians, the transition was made with minimal risk to the hospital and maintained uptime of the backup power while seamlessly modifying the controls and testing the equipment.”
In order to feed additional power loads to the ever-growing hospital, an Automatic Transfer Switch (ATS) solution was installed during the process. It redirects power between main and backup sources and offers improved control for continuous power and continued safety, a necessity in a mission-critical facility.
The system software was also replaced with an upgraded program that provided positioning, run requests, run times for ATS, and real-time reporting on all generator sets.
As a life-saving facility, it’s not an option for backup power equipment to stop working. The facility’s operating rooms and intensive care units demand a reliable backup power source in the event of unexpected failures.
If there’s an interruption of power from the main grid, the new Cat generator sets will power the system within 10 seconds – per code.
But beyond a backup power source, the new system must comply with all Joint Commission standards. The system is now programmed to conduct a 30-minute test at 30 percent load, and then deliver a thorough report to power plant managers.
“Now each month when I run the generator sets, it gives me a printable report that has all the information needed to pass accreditation,” added Setters. “From a finished product standpoint, we now have a seamless operation.”
The operation is more cost-effective too.
“The electronic reporting saves us approximately $4,000 a year, which should be doubled for the two consecutive years that it does not need to be done. So, that’s $8,000 in immediate savings right off the top,” Setters said.
In addition to an adequate power supply and thorough reporting, Yancey Power Systems also provides annual preventative and scheduled maintenance.
“The fast-paced healthcare field needs equipment that can keep up. We ensure that with our meticulous maintenance regimen, which analyzes oil and updates the system’s valves and hoses yearly,” stated Craig Smith of Power Systems Sales at Yancey Power Systems.
With an ever-expanding facility, TRMC appreciates a collaborator who will grow along with them.
“We’re not looking for a service company, we’re looking for a partner,” said Setters. “The question I always pose to any partner is, ‘Are you going to own my problems?’ Caterpillar said yes. And to this day, they have.”
Producing reliable power from 830 to 1250 ekW at 60 Hz, our C32 diesel generator sets are made to meet your mission critical,…
Learn More