Cat® 320D3 GC Excavator
Cat® 320D3 GC Excavator

Design updates for the Cat® 320D3 GC Excavator improve reliability and increase machine travel speed

 

For Release in India: January 2024
Release Number: 18PR24

 

  • New heavy-duty boom and reinforced stick expand operating capabilities 
  • New two-speed drive increases travel speed by 47%

 

The Cat® 320D3 GC Excavator is built for versatile operation and fuel efficiency to deliver the lowest cost per hour operation. Design updates to the boom and stick help to increase excavator flexibility, while a new standard two-speed final drive increases travel speed to improve on-site operating efficiency. Added machine telematics capabilities now allow for remote monitoring of fuel consumption and remote machine derating.

Like the 320D3 model, the current production 320D3 GC excavator now comes standard with a 5.7-m heavy duty boom. Increasing durability and reliability compared to previous designs, its standard reinforced 2.25-m stick features thicker plates and a boom nose redesign. These upgrades remove previous operating restrictions, so the excavator is now suitable for use with hammers.

Two travel speeds – 3.8 km/h in first gear and 5.6 km/h in second – enable the updated excavator to move more quickly from one area of the jobsite to another, improving efficiency. In-cab design enhancements include a new, more comfortable operator’s seat that features a dual slider mechanism that allows for independent leg length and arm length adjustments. Its new key start design allows operators to start/stop the excavator without the need for an engine kill lever.

The reliable 320D3 GC excavator is known for delivering low fuel consumption and owning costs. Typical fuel consumption in earthmoving applications averages as low as 11 liters per hour. A new optional fuel meter offers the ability to remotely track machine fuel consumption via Cat VisionLink®. Additionally, the machine can be remotely derated to 50% operating capabilities as a theft deterrent and to increase the chances of recovering a stolen machine.

The 320D3 GC excavator features a design that simplifies routine maintenance to lower costs. Virtually all daily maintenance can be performed at ground level to increase efficiency and safety. Hydraulic oil change intervals of 6,000 operating hours with a long 3,000-hour oil filter service intervals allows the excavator to spend more time at the jobsite and less time in the shop.

For more information about the new Cat 320D3 GC Excavator, contact a Cat dealer or visit: www.cat.com.

 

Download the press release and images 

Download Now

 

 

of

Cat 320D3 GC Excavator loading a truck.

View Full Size Image
of

Cat 320D3 GC Excavator placing a pipe in a trench.

View Full Size Image
of

Cat 320D3 GC Excavator digging and loading a truck.

View Full Size Image
of

Cat 320D3 GC Excavator cleaning up a berm.

View Full Size Image
of

Cat 320D3 GC Excavator with bucket, boom and stick dumping dirt.

View Full Size Image
of

Cat 320D3 GC Excavator digging a trench.

View Full Size Image
of

Cat 320D3 GC Excavator digging a trench.

View Full Size Image

 

 

of

The Cat® 320D3 GC Hydraulic Excavator – Dig More Profit. With improved engineering from the bucket to the tracks and everywhere in between, the 320D3 GC gives you dependable performance, low operating costs, and more comfort for operators. The Cat 320D3 GC is a smart choice for operations where high reliability and low cost-per-hour performance are priority

of

With improved engineering from the bucket to the tracks and everywhere in between, the 320D3 GC gives you dependable performance, lower operating costs, and more comfort for operators. The Cat 320D3 GC is a smart choice for operations where high reliability and low cost-per-hour performance are priority.

Product & Service News

See the latest product and engine announcements from Caterpillar.

See the Latest News

 

 

# # #

 


Note to Editors: Caterpillar rolls out products and services in each of its regions at different time intervals. Although every effort is made to ensure that product information is released only after Caterpillar has received confirmation from its independent dealer network, plants, and marketing subsidiaries that products and services are available in the relevant region, editors are kindly requested to verify with a Cat dealer for product availability and specifications.

CAT, CATERPILLAR, LET’S DO THE WORK, their respective logos, VisionLink, “Caterpillar Corporate Yellow,” the “Power Edge” and Cat “Modern Hex” trade dress, as well as corporate and product identity used herein, are trademarks of Caterpillar and may not be used without permission.

VisionLink is a trademark of Caterpillar Inc., registered in the United States and in other countries.

©2024 Caterpillar All Rights Reserved 

 

 

Press Inquiries

Caterpillar Trade Press Media Representatives

Americas
Kate Kenny: Kenny_Kate@cat.com
Johanna Kelly: Kelly_Johanna_L@cat.com

Europe, Africa, Middle East
Amy Doughty : Amy.Doughty@cat.com