Fully integrated for optimal performance, the wheel loaders can be easily upgraded with optional technologies as work demands it.
IRVING, Texas, May 6, 2025―Next generation Cat® medium wheel loaders are infused with the latest technologies to advance safety and help customers work faster and with greater accuracy. Fully integrated for optimal performance, the wheel loaders can be easily upgraded with optional technologies as work demands it.
Caterpillar announces new technology options available for next generation Cat 950, 962, 966, 966 XE, 972, 972 XE, 980, 980 XE, 982 and 982 XE wheel loaders.
Frank Stadelmann
Caterpillar global product application specialist for medium wheel loaders
Caterpillar
Frank Stadelmann
Caterpillar global product application specialist for medium wheel loaders
Caterpillar
Starting with a foundation of the standard HD rear camera with an integrated touchscreen, Cat medium wheel loaders offer a progressive building block of optional technologies, including the Multiview (360°) Vision System, Rear Object Detection and now Collision Warning System with Motion Inhibit.
The new system uses radar and vision sensors to detect hazard potential, alert operators and inhibit motion when initiating reverse motion from a stationary position. Targeting collision potentials that emerge from behind the loader, the Collision Warning System leverages both smart camera and radar technology to give audible and visual alerts to help operators see, mitigate and manage hazards that might otherwise go unnoticed. The system’s three color zones – yellow for awareness, amber for caution and red for critical – approximate the distance of the object to the anticipated path of the loader.
The embedded Motion Inhibit feature prevents direct reverse gear engagement when shifting from neutral and automatically applies the brake when the system detects an object or worker in the critical alarm zone behind the loader. When this occurs, the operator is alerted by an on-screen notification. If the loader is stationary for at least 15 seconds and the operator shifts from park to reverse, Motion Inhibit prevents the machine from engaging reverse when the rear detection system identifies something in the critical alarm zone. The loader will reverse once the operator shifts back into neutral and steers to clear the detection.
People Detection utilizes the smart camera to alert the operator when a person is detected behind the loader. Three levels of alerts dynamically adjust based on the person’s proximity to the machine, and the system highlights people in red bounding boxes on the in-cab monitor to distinguish and manage the potential risk.
Standard Cat Payload delivers precise bucket load information with on-the-go weighing to help prevent overloading or underloading. Upgrading to the Advanced Payload system expands automation features and capabilities, including automatic tip-off assist for the final bucket process to help precisely meet target payloads. A new multitask mode within Advanced Payload tracks two loading processes simultaneously, while split mode allows for loading multiple bodies, tracking individual targets and tabulating grand totals of each load.
Optional Cat Advanced Payload is a system upgrade that offers expanded features and capabilities. Tip-off assist adds automation to the final bucket process. Multitask mode tracks two loading processes simultaneously. Split mode allows for loading multiple bodies while tracking individual targets and grand totals. Add Dispatch for Loading** to integrate the loader into the scale house process.
The Cat Payload for Trade* option for Cat Advanced Payload allows you to integrate scale data directly into your business processes. It is type approved by the International Organization of Legal Metrology and retains all the features of the standard version of Cat Advanced Payload.
From material handling and truck loading to general construction and stockpiling, the integrated Cat medium wheel loader technologies help operators of all skill levels work more efficiently and productively with less fatigue. These new technologies increase the machine’s capabilities by building on a number of standard and optional features already available, including:
Removing the operator from the machine, the recently announced Command for Loading technology offers remote control of next generation medium wheel loaders. An ergonomic Command console enables line-of-sight remote control of basic machine functions such as startup/shutdown, bucket rack/dump and lift/lower. For non-line-of-sight operation, the Command Station can connect to multiple machines and allow the user to operate one machine at a time, either on-site or from miles away.
More information on the new technology upgrades for Cat® wheel loaders can be found by contacting a Cat dealer or visiting cat.com.
* Available in Europe. Country certifications vary. Contact your Cat dealer for more information.
** Subscription and compatible scale house software are required.
# # #
About Caterpillar:
With 2024 sales and revenues of $64.8 billion, Caterpillar Inc. is the world’s leading manufacturer of construction and mining equipment, off-highway diesel and natural gas engines, industrial gas turbines and diesel-electric locomotives. For 100 years, we’ve been helping customers build a better, more sustainable world and are committed and contributing to a reduced-carbon future. Our innovative products and services, backed by our global dealer network, provide exceptional value that helps customers succeed. Caterpillar does business on every continent, principally operating through three primary segments – Construction Industries, Resource Industries and Energy & Transportation – and providing financing and related services through our Financial Products segment. Visit us at caterpillar.com or join the conversation on our social media channels at caterpillar.com/en/news/social-media.html.
NOTE TO EDITORS: Caterpillar rolls out products and services in each of its regions at different time intervals. Although every effort is made to ensure that product information is released only after Caterpillar has received confirmation from its independent dealer network, plants, and marketing subsidiaries that products and services are available in the relevant region, editors are kindly requested to verify with a Cat dealer for product availability and specifications.
CAT, CATERPILLAR, LET’S DO THE WORK, their respective logos, “Caterpillar Corporate Yellow,” the “Power Edge” and Cat “Modern Hex” trade dress, as well as corporate and product identity used herein, are trademarks of Caterpillar and may not be used without permission.
VisionLink is a trademark of Caterpillar Inc., registered in the United States and in other countries.
Caterpillar is one of four exhibitors awarded Gold for Stand Design at the 2025 Eventex Awards.
Learn MoreCaterpillar announces multiple updates for its Cat® Hydraulic Excavator line as part of its annual product update (APU) program.
Learn MoreThe new Cat® Single Life Cutting Edges for Cat medium wheel loaders feature a single bevel design that eliminates the need to monitor wear for flipping edges.
Learn MoreThe machine is the first next generation design of off-highway trucks for the company. Distinguishing it from the previous 775 models, this 65-tonne (71-ton) payload hauler is engineered to enable fully autonomous capabilities in the future.
Learn More