CATERPILLAR LAUNCHES DIESEL GENERATOR SETS WITH FACTORY-INSTALLED DYNAMIC GAS BLENDING™


For Worldwide Release: April 24, 2018
Release Number: EEPR0718

Industry-leading Dynamic Gas Blending™ (DGB™) package dramatically lowers fuel costs while ensuring engine performance within safe operating limits

PEORIA, IL – Caterpillar Inc. today announced the introduction of the company’s Dynamic Gas Blending™ (DGB™) dual-fuel technology as a factory-installed option for diesel generator sets. This system allows Cat® diesel engines to burn a mixture of diesel and natural gas, in many cases cutting fuel costs by up to $100/eMW for each hour of generator set operation while maintaining diesel engine performance.

Since 2013, Caterpillar has offered DGB retrofit kits for power solutions primarily used in the oil and gas industry. With the introduction of factory-installed DGB technology, Caterpillar is able to provide complete product support, including standard warranty coverage for the entire generator set with the DGB hardware.

Available now, the DGB factory-installed option is applicable for six prime- and continuous-rated Cat 3516B diesel generator sets for unregulated emissions applications in Latin America and other global markets. These high-speed generator sets feature power ratings from 1750 kVA to 2275 kVA for 50-Hz applications and from 1640 ekW to 1825 ekW for 60-Hz applications.

“By far, fuel consumption accounts for the largest percentage of operating expenses for power solutions at remote sites,” said Jason Kaiser, product manager for Caterpillar Large Electric Power Division. “Only Caterpillar can deliver the unmatched performance, convenience, and peace of mind supplied by dual-fuel technology in a factory-installed package that offers a payback in months, rather than years.”

Caterpillar’s DGB technology is fully automatic and has been designed to continually monitor each of the 16 cylinders while optimizing the diesel substitution rate to suit the application demands and environment. This enables the Cat DGB system to protect the engine, maintain diesel performance, and maximize diesel substitution rates in any situation. It can maintain diesel performance levels with up to 70 percent replacement of diesel with gas. No customer input or gas analysis is needed during operation, and no recalibration is required when the equipment is moved or the gas supply changes.

Caterpillar is a leader in the power generation marketplace with power systems engineered to deliver unmatched durability, reliability and value. The company offers worldwide product support, with parts and service available globally through the Cat authorized service and dealer network. In addition, dealer service technicians are trained to service the entire Cat generator set and ancillary equipment.

For more information, visit www.cat.com/powergeneration or e-mail cat_power@cat.com

For more than 90 years, Caterpillar Inc. has been making sustainable progress possible and driving positive change on every continent. Customers turn to Caterpillar to help them develop infrastructure, energy, and natural resource assets. With 2017 sales and revenues of $45.462 billion, Caterpillar is the world’s leading manufacturer of construction and mining equipment, diesel and natural gas engines, industrial gas turbines, and diesel-electric locomotives. The company principally operates through its three product segments - Construction Industries, Resource Industries, and Energy & Transportation - and also provides financing and related services through its Financial Products segment. For more information, visit caterpillar.com. To connect with us on social media, visit caterpillar.com/social-media.

CAT, CATERPILLAR, BUILT FOR IT, their respective logos, “Caterpillar Yellow”, the “Power Edge” trade dress as well as corporate and product identity used herein, are trademarks of Caterpillar and may not be used without permission.

©2018 Caterpillar
All Rights Reserved

 

Press Inquiries

Bob Chase
Gelia
Tel: +1 716 629-3230
bchase@gelia.com

Rachel Perva
Caterpillar Inc.
Tel: +1 309 675-7267
Perva_Rachel@cat.com