Caterpillar unveils Cat® 395 Front Shovel Large Excavator at bauma 2025

This new Caterpillar model takes full advantage of standard next generation features, such as fuel economy and low maintenance costs, while further improving Caterpillar’s world-class levels of operator comfort and control.

IRVING, Texas, March 7, 2025―Caterpillar has chosen bauma to unveil the Cat® 395 Front Shovel Large Excavator, the company’s first new Front Shovel configuration in 15 years.

Designed to meet the exacting needs and expectations of mining and quarry customers, this new Caterpillar model takes full advantage of standard next generation features, such as fuel economy and low maintenance costs, while further improving Caterpillar’s world-class levels of operator comfort and control.

The 395 FS has an official target launch of October 2025, but there’s no better place than bauma to showcase the pre-production model and have potential customers ‘see it in the metal.’ We’re excited to have the 395 FS join the Large Excavator lineup. 

Vincent Migeotte

Senior Product and Sales Consultant

Caterpillar

At the top of the design ‘wish list’ for the 395 FS were three primary objectives: robust digging and breakout force, lightning-quick loading cycles, and rigorous bucket full.

 

Customers repeatedly told us that they need a machine that not only offers peak performance but that can operate consistently at those peak levels.

 

That’s borne out in the 395 FS with a maximum ground level digging force up to truck height, matched by a powerful breakout force at the bucket cutting edge that promises superior material penetration and optimal bucket fill factors.

 

And of course, that’s complemented by bucket capability: here’s a machine that’s compatible with bucket volumes up to 6.5 m3, or maximum material density of up to 1.85 t/m3. That offers operators a big boost in productivity.

Vincent Migeotte

Senior Product and Sales Consultant

Caterpillar

Caterpillar’s values of durability, reliability and serviceability are woven through the design of the 395 FS, evident in features such as the reinforced, extra-durable undercarriage and additional cylinder guards, plus long-life fuel and hydraulic oil filters to reduce costs and downtime. There’s also the assurance conveyed by all next generation models sharing common parts, backed up by Cat dealers’ far-reaching customer service and celebrated product support.

 

Of course, a machine only delivers its best performance when it works in harmony with its operator which is why we’ve paid so much attention to operator optimisation through next generation developments. The 395 FS has been engineered with a parallelogram-type front linkage, coupled with a master cylinder that allows the operator to extract the machine’s maximum capability. By keeping the bucket parallel to the ground, the operator can optimise penetration, loading, sorting and breaking, and complete a smooth floor clean-up when the hard work’s over. Building the 395 FS around the next generation cab, we’ve also fitted a fixed riser which allows the operator to see above the side of the truck body while loading. Premium work task visibility helps increase both productivity and worksite safety.

Vincent Migeotte

Senior Product and Sales Consultant

Caterpillar

Operator-oriented in-cab controls are easily accessible, enhancing material penetration, fast loading and smooth floor clean-up. Inside, the cab features an ergonomic seat, a touchscreen display, climate control, and noise insulation, along with vibration reduction, all contributing to a more comfortable and efficient operating experience.

 

A Century of Innovations

Over the last century, Caterpillar has grown with our customers to help build a better, more sustainable world. To go where you go, you need reliable, dependable equipment. That's why we continue to support our customers with world class machines and work tools that deliver dependability, versatility and efficiency to every fleet. No matter the task at hand, you can work confidently — because your Cat equipment and local Cat dealer are committed to meeting your needs to get the job done. When you choose our products, services and solutions today, you’re gaining 100 years of experience and expertise.

For more information about 395 FS Large Excavator, contact a Cat dealer or visit: www.cat.com

 

395 FS Specifications

 

 

Engine

Cat C18

Net Power* – ISO 14396

405 kW (542 hp)

Operating weight – 4.6 m (15ft 9in) FS Boom, 3.48 m (11ft 42in) FS Stick, 6.5 m³ (8.5 yd³) FS bucket, 650 mm (26in) double grouser shoes, 15,450 kg (34,060 lb) counterweight

93,300 kg (212,300 lb.)

Emissions

Meets U.S. EPA Tier 4 Final, EU Stage V, Japan 2014 and China NR4 emission standards

*Net power advertised is the power available at the flywheel when the engine is equipped with fan, air intake system, exhaust system, and alternator with engine speed at 2,200 rpm. Advertised power is tested per the specified standard in effect at the time of manufacture. 

 

of
of
of

 

 

 Dowload the Press Release

Download Now

Download the Images 

Download Now

 

 

# # #

About Caterpillar:
With 2024 sales and revenues of $64.8 billion, Caterpillar Inc. is the world’s leading manufacturer of construction and mining equipment, off-highway diesel and natural gas engines, industrial gas turbines and diesel-electric locomotives. For 100 years, we’ve been helping customers build a better, more sustainable world and are committed and contributing to a reduced-carbon future. Our innovative products and services, backed by our global dealer network, provide exceptional value that helps customers succeed. Caterpillar does business on every continent, principally operating through three primary segments – Construction Industries, Resource Industries and Energy & Transportation – and providing financing and related services through our Financial Products segment. Visit us at caterpillar.com or join the conversation on our social media channels at caterpillar.com/en/news/social-media.html.

NOTE TO EDITORS: Caterpillar rolls out products and services in each of its regions at different time intervals. Although every effort is made to ensure that product information is released only after Caterpillar has received confirmation from its independent dealer network, plants, and marketing subsidiaries that products and services are available in the relevant region, editors are kindly requested to verify with a Cat dealer for product availability and specifications.

CAT, CATERPILLAR, LET’S DO THE WORK, their respective logos, “Caterpillar Corporate Yellow,” the “Power Edge” and Cat “Modern Hex” trade dress, as well as corporate and product identity used herein, are trademarks of Caterpillar and may not be used without permission.

VisionLink is a trademark of Caterpillar Inc., registered in the United States and in other countries.

 

 

Press Inquiries:

Amy Doughty
Caterpillar Trade Press Media Representative
amy.doughty@cat.com
 
For Release: Europe
Release Number: 56PR25 — March 2025


Large Excavators

Their power, speed, and fuel efficiency make Cat® large excavators the right machine for bulk excavation applications. With powerful, yet efficient engines, advanced hydraulic systems, factory equipped technology, and matching attachments, these machines will help you complete your large-scale projects on time and within budget.

Learn More
Large Excavators
Large Excavators

The Latest Product News

Get the Latest Stories Sent Directly to Your Inbox.

Subscribe Now