If you already have an existing account with another Cat App, you can use the same account to sign in here
One Account. All of Cat.
Your Caterpillar account is the single account you use to log in to select services and applications we offer. Shop for parts and machines online, manage your fleet, go mobile, and more.
Account Information
Site Settings
Security
For Worldwide Release: September 30, 2021
Release Number: EEPR0821
DEERFIELD, IL – Caterpillar Inc. today announced the new 200 kVA Cat® XQP200 mobile generator set, the company’s first mobile power solution meeting European Union (EU) Stage V emission standards for engines used in non-road mobile machinery.
Available through the global Cat dealer network, the Cat XQP200 generator set is the first in a series of EU Stage V mobile generator sets to be introduced by Caterpillar. Since the legislation for mobile generator sets skipped Stage IIIB and IV, Caterpillar engineers delivered a significant leap in technology with a fully integrated solution optimized for performance and usability featuring engine modifications and the introduction of off-engine aftertreatment needed to meet the 93% reduction in nitrogen oxides and other changes specified by EU Stage V standards.
“The Cat XQP200 mobile generator set leverages numerous technological advances from Caterpillar’s equipment portfolio to deliver the consistent performance, reliability and fuel efficiency that improve the competitiveness and productivity of mobile equipment users,” said Tom Caldwell, global general manager for electric power rental solutions at Caterpillar. “At the same time, it helps our customers meet their sustainability goals while addressing current regulatory standards, which is especially timely as growing numbers of European municipalities institute low emission zones.”
Rental-Ready Benefits
The Cat XQP200 generator set offers numerous features that make it ideal for rental applications. It delivers increased flexibility by easily switching between 50 and 60 Hz and across a range of voltages. This allows one machine to satisfy varying load requirements in diverse regions and applications, such as mining, manufacturing, oil and gas, and construction.
It is equipped with the EMCP 4.2B digital control panel, which provides all generator set controls and system indicators in a single, easy-to-access interface. Programmable logic controller (PLC) functionality improves reliability and flexibility for accommodating changes in processes or application requirements.
The Cat XQP200 generator set is designed with a dual-wall, open-top fuel tank that helps to protect the environment by containing spills, while Costal Insulation Protection (CIP) enables operation in harsh conditions.
Its wide, impact-absorbing base frame, customer connections isolated from circuit breakers, and optional CEE sockets are designed to facilitate transportation, set-up and use. Forklift pockets, dragging points, and a lifting arch help to simplify loading, unloading, and placement around the worksite.
Fully designed and tested by Caterpillar, the Cat XQP200 uses proven technology to enable simple, reliable operation. It can be equipped with Cat Connect technology to remotely track and manage the generator set and improve operational efficiency. The telematics can send real-time information on fuel level, diesel exhaust fluid (DEF) level, battery voltage and status (Run/Stop/Auto). Connected assets support peak operation at any emission tier, and especially for EU Stage V products. This timely insight allows customers to better control costs, improve performance and reduce risks.
All Cat mobile generator sets are available through the worldwide Cat dealer network. Cat dealers work 24 hours a day, seven days a week to assist with emergency rental needs and service every aspect of Cat equipment.
For more information, visit Stage V emissions or e-mail Electric_Power@cat.com.
###
About Caterpillar
Since 1925, Caterpillar Inc. has been helping our customers build a better world – making sustainable progress possible and driving positive change on every continent. With 2020 sales and revenues of $41.7 billion, Caterpillar is the world’s leading manufacturer of construction and mining equipment, diesel and natural gas engines, industrial gas turbines and diesel-electric locomotives. Services offered throughout the product life cycle, cutting-edge technology and decades of product expertise set Caterpillar apart, providing exceptional value to help our customers succeed. The company principally operates through three primary segments - Construction Industries, Resource Industries and Energy & Transportation - and provides financing and related services through its Financial Products segment. For more information, visit caterpillar.com. To connect on social media, visit caterpillar.com/social-media.
© 2021 Caterpillar. All Rights Reserved. CAT, CATERPILLAR, LET’S DO THE WORK, their respective logos, “Caterpillar Corporate Yellow,” the “Power Edge” and Cat “Modern Hex” trade dress, as well as corporate and product identity used herein, are trademarks of Caterpillar and may not be used without permission.
Press Inquiries
Bob Chase
Gelia
Tel: +1 716-629-3230
bchase@gelia.com
Áine Fitzsimons
Caterpillar Inc.
Tel: +353 2890-49-5212
fitzsimons_aine@cat.com
Reader Requests
Caterpillar Inc.
Electric Power Division
P.O. Box 0610
Mossville, IL 61552-0610