Power from Renewable Liquid Fuels

Biodiesel and HVO

Renewable Liquid Fuels
Renewable Liquid Fuels

Rethink Your Fuel

Renewable Liquid Fuels for Cat® Generators

What are Renewable Liquid Fuels?

Biodiesel and HVO are biofuels produced from renewable resources such as vegetable oils, including soybean oil, canola oil, and palm oil, as well as used cooking oils and animal fats. While the resources may vary globally, finished fuel specifications are independent of the feedstock. 

 

of

What is the Difference Between Biodiesel and HVO Fuel?

HVO and biodiesel are the two main renewable liquid fuels readily available for end users, but they have several differences:

  Biodiesel (FAME) Hydrotreated Vegetable Oil (HVO) (Renewable Diesel)
Source Vegetable oils and fats Vegetable oils and fats
Process Transesterification Hydrotreating
Chemistry    
Product Oxygenated, ester Non-oxygenated, paraffin
Replacement for diesel? Yes, with some cautions Yes
Specifications ASTM D6751, EN 14214, Cat Spec EN 15940

 

  • Note that hydrotreated vegetable oil (HVO)/renewable diesel (RD) is per diesel fuel specifications except for density. HVO has lower density than diesel fuels.
  • Biodiesel and HVO are sourced from the same feedstocks but differ in the processing and in the final product chemistry.
  • HVO can be used in both standby and prime applications, whereas biodiesel is better suited to prime applications.
  • Both fuels can be used “neat” or blended with conventional diesel to various percentages. Refer to Cat® publications and/or your Cat dealer for acceptable blend levels.

What are the Benefits of HVO?

  • Running generators on HVO provides similar performance to running on diesel including similar rated power output, transient response, start-up time, and NOx emissions.
  • HVO fuel is a drop-in replacement for diesel.
  • HVO has a long shelf life and can be stored in hot and cold conditions.
  • Although HVO does not significantly reduce CO2 emissions at the tailpipe, switching to HVO will reduce lifecycle greenhouse gas emissions compared to diesel.
  • Lower visible smoke emissions when using biofuels.
  • HVO is available now and is easy to switch to.
of

What are the Benefits of Biodiesel?

  • Running generators on biodiesel provides similar performance to running on diesel.
  • Lower visible smoke emissions when using biodiesel.
  • Although biodiesel does not significantly reduce CO2 emissions at the tailpipe, switching to biodiesel will reduce lifecycle greenhouse gas emissions compared to diesel.
  • Biodiesel is widely available and is easy to switch to.

Can Cat® Generators Run on Biofuels?

Cat diesel generators can run on biofuels and have accommodated the use of biodiesel and HVO for over a decade. These fuels are available now, and your local Cat dealer can provide guidance and recommendations for switching to renewable liquid fuels.

View diesel generators page
Renewable Liquid Fuels
Renewable Liquid Fuels

In the News

Data Center Transitions to 100% HVO

Caterpillar announced LCL Brussels-West data center has commissioned a new 13.5 MVA standby power solution, making it the first data center in Belgium to operate exclusively on 100% hydrotreated vegetable oil (HVO) fuel.

view press release
LCL Brussels-West data center
LCL Brussels-West data center

Providing Sustainable Backup Power to Microsoft

Microsoft’s newest data centers in Sweden depend on Cat standby generators that can operate on renewable liquid fuel, supporting their sustainability goals and uptime commitments.

view press release
Microsoft press release
Microsoft press release

Cat® Rental Power Solutions Deployed by Peterson Power Systems Surpass 8 Million Gallons in HVO Fuel Use

Customers using Cat rental power solutions supplied by Peterson Power Systems, the local Cat dealer in Northern California, Oregon and Southwest Washington, have generated power using more than 8 million gallons of hydrotreated vegetable oil (HVO) since 2022.

view press release
Peterson Power Systems Surpass 8 Million Gallons in HVO Fuel Use
Peterson Power Systems Surpass 8 Million Gallons in HVO Fuel Use

Testimonials

LCL Data Centers Fuels Standby Power System With HVO, A Renewable Alternative To Diesel

LCL Data Centers has grown quickly, with five independent locations serving customers across Belgium. With a deep commitment to sustainability, LCL aims to generate 40% of its energy from its own green power sources by 2030. Working with Cat dealer Eneria, LCL chose to install a new Cat standby power solution consisting of six diesel generator sets operating exclusively on 100% hydrotreated vegetable oil.

Read More
LCL Data Centers
LCL Data Centers

White Papers

Interested in finding out the difference of running on HVO instead of diesel fuel? Click on any of the white papers below.

Considerations for Use of Renewable Liquid Fuels

There is a difference in applicability of biodiesel and HVO for prime and standby power:

Power Biodiesel HVO
Prime, Continuous Blend levels per Caterpillar guidance Any blend level with diesel
Standby B5 Maximum blend level Any blend level with diesel

 

The differences in applicability of biodiesel and HVO in standby power applications are due to the nature of the fuels. Biodiesel can age with storage and degrade in quality as it ages. As such, it does not support use in standby power applications and, particularly emergency generator applications.

Generator engines fueled by renewable liquid fuels have similar performance to those fueled with conventional diesel but may experience a small decrease in maximum power output. Fuel consumption may also increase due to the potentially lower energy content of the specific renewable fuel being used. The cold temperature properties of both HVO and biodiesel need to be appropriate for the ambient environment of the generator. Your local Cat dealer can talk you through any adaptations that may need to be made to your installation.

of

Some regions or municipalities, particularly where mandates for renewable fuel use exist, may have abundant availability of biodiesel and of HVO. Other areas may not, which can mean fuels need to be transported to the location if needed. Transport over long distances may reduce the positive environmental impact of these fuels. 

Only purchase biodiesel and HVO fuels from reputable dealers selling commercial grade fuels that meet the relevant specifications.  

of

The price of biodiesel blends varies depending on geographic area, base material (corn, soybeans, etc.), supplier, and government tax and other incentives. Although renewable liquid fuels can cost more than petroleum diesel, diesel generator set owners can transition to these fuels without purchasing new engines. In the case of fleets, managers can transition to renewable liquid fuels without acquiring new spare parts inventories.

of

Detailed guidance on the use of renewable liquid fuels exists, and users should be aware of the differences in the maintenance requirements associated with them compared to diesel fuels and each other.

When switching from diesel fuel to biodiesel for the first time, shorter maintenance intervals are recommended with focus on fuel filters, hoses, pumps, and seals. Always consult your local Cat dealer for guidance and information relating to new or existing equipment.

HVO fuels have similar aging properties to diesel. Biodiesel, however, has a shorter shelf life due to its composition. Shelf life is based on the blend level.

Contamination control measures are critical for application of any fuel, diesel or renewable. Fuels must be protected from water and dirt.

of

Specifications & Standards

Biodiesel is registered with the U.S. Environmental Protection Agency (EPA) and is legal for use at any blend level in both highway and nonroad diesel engines. In the U.S., the applicable blending specification for B100 is ASTM D6751. B20 blend specifications in the US are ASTM D7467.

European fuel standard EN 14214 ensures that biodiesel is suitable for even the most modern engines. EN 16709 describes B20 and B30 biodiesel blends.

HVO fuels must be per EU 15940 specification. HVO fuels also satisfy the diesel fuels specifications ASTM D975 and EN 590, except for density. 

Only purchase biodiesel and HVO fuels from reputable dealers selling commercial grade biodiesel. 

of

Resources

National Renewable Energy Lab Guide

View Guide
Lab Guide
Lab Guide

Operation and Maintenance Manual

Cat Commercial Diesel Engine Fluids Recommendations

View Manual
Operation and Maintenance Manual
Operation and Maintenance Manual

Cat Machine Fluids Recommendations

Cat Machine Fluids Recommendations

View Manual
Operation and Maintenance Manual
Operation and Maintenance Manual

FAQs

Want to discover if renewable liquid fuels might be a solution for your power system? Check out our Frequently Asked Questions document featuring information on the use of renewable liquid fuels, primarily HVO and biodiesel, in the Cat 3500 and C175 series generator sets.

FIND ANSWERS
Operation and Maintenance Manual
Operation and Maintenance Manual

Blog

Webinar: Alternative Fuels for Electric Power generator sets

The most common fuels used to power generator sets are diesel and natural gas, but did you know there are other options? Engines to power generator sets are available in a wide range of configurations, capable of burning a broad spectrum of fuels. Participants will gain an understanding of what other fuel options exist and what an owner/operator would need to know before using them. 

Learn More
Alternative Fuels for Electric Power generator sets
Alternative Fuels for Electric Power generator sets

Industries Served

With the industry's widest range of diesel, gas, and mobile generator sets, hybrid energy storage solutions, automatic transfer switches, and switchgear, the Cat team will work directly with you for the life of your power system – from configuration to installation to operation.

View Industries
industries served
industries served

Sustainability

For Caterpillar, sustainability is not a new concept. It’s part of who we are and what we do every single day.

View Sustainability page
Sustainability
Sustainability

View Diesel Generator Sets

Any size or shape. In any regulatory environment. When you need power, Caterpillar is equal to the challenge. Our commercial and industrial generator sets are used in a variety of applications.

Diesel Generator Sets
diesel generator sets
diesel generator sets

Rental Power

Cat Rental Power delivers clean, reliable, fuel-efficient gensets whenever and wherever you need them. 

View Rental Page
Rental
Rental

Cat GC Models and Technical Information

View and compare the latest information and technical specifications, including power output, package performance, overall dimensions, and available options.

VIEW CAT GC MODELS
CAT GC MODELS AND TECHNICAL INFORMATION
CAT GC MODELS AND TECHNICAL INFORMATION

Product Support

Caterpillar and your Cat dealer are dedicated to making sure you get the most from your equipment with outstanding service and support. Let’s explore what services we have to offer.

What to Expect From Your Cat Dealer

Click on the button to fill out a short form. An experienced dealer will contact you to discuss a custom solution and pricing options that best suit your needs.

of

Cat Connect for Electric Power

Know how your operation is running from anywhere. Cat Connect gives you the information you need to make well-informed, timely decisions.

Learn More
cat connect
cat connect

Brochures and Testimonials

We have an Information Library of product literature, white papers, customer stories, and more. Find what you’re looking for.

View library
industry information
industry information

Generator Set Sizing Calculators

Caterpillar Electric Power now has two tools available for sizing gensets in any application. 

Size Now
specsizer
specsizer

Cat Dealers Make the Difference

Your Cat dealer is committed to maximizing your success, helping you get the most out of your operations with site-level solutions, service and support.

Learn More
dealers
dealers

Electric Power Newsletter

Get the latest information on Cat products and industry topics focused on helping you get the most from your investment. 

Sign Up
ep newsletter
ep newsletter

Electric Power News

Read the latest electric power news and articles relating to Cat electric power products by people in the know, on topics that matter to your business.  

Read More
ep news
ep news