Exclusive new Cat® Track Wear Sensor provides remote, no-touch wear monitoring and alerts at key wear percentages

 

For Worldwide Release: July 2024
Release Number: 169PR24

 

  • Remote monitoring of undercarriage track wear to increase fleet coverage
  • Alerts at 40%, 70% and 100% wear intervals for easy maintenance planning
  • Durable, waterproof design with long battery life 

 

With 120 years of undercarriage experience, Caterpillar continues to innovate, so customers get the most from their investment. Exclusive to Cat® machines and undercarriages, the proprietary Cat Track Wear Sensor (CTWS) remotely monitors undercarriage wear to better predict wear out, plan maintenance and increase machine uptime.

Monitored within the Cat Wear Management System, the new CTWS wirelessly communicates critical track link wear information from the machine to the dealer for monitoring. Timed alert intervals – a 40% wear alert for possible bushing turns, 70% to signal for measuring and replacement part ordering, and 100% for required replacement – improve inspection scheduling and streamline ordering of replacement parts. The real-time track wear status enables no-touch track link measurements, increases fleet coverage by automating inspections, provides visibility to track wear when operating in remote locations and allows for prioritized timing of service visits by helping optimize manual inspections.

Field tested for proven reliability throughout the expected track life, more than 2,000 Cat machines have been shipped with the innovative sensor technology. The small electronic sensor installs in a customized pocket in the track link for protection. Each link assembly includes a smart link, resulting in two sensors on a machine, one on each side. The CTWS survives high frequency shock loads and meets sensor functional and environmental tests. Subject to operating conditions, sensor battery life has been shown to last up to seven (7) years.

The wear sensor is standard on new Cat D5, D6 and D8 dozers, and 953 and 963 track loader models in select regions with planned expansion to models in the dozer line in the future. It can be retrofitted on eligible dozer undercarriages.

For more information about the new Cat Track Wear Sensor, contact a Cat dealer or visit: www.cat.com.

 

Download the press release and images 

Download Now

 

 

of

CTWS graphic

View Full Size Image
of

Undercarriage and CTWS

View Full Size Image
of

CTWS link on machine

View Full Size Image
of

Discover the revolutionary Cat® Track Wear Sensors (CTWS) in this detailed review and see how they can transform your fleet management and maintenance. The CTWS is designed exclusively for Cat Machines, enhancing reliability by monitoring undercarriage wear in real-time. This innovative sensor enables automated alerts at critical wear points, ensuring optimal performance and reducing downtime significantly.

 

 

Product & Service News

See the latest product and engine announcements from Caterpillar.

See the Latest News

 

 

# # #

 

Note to Editors: Caterpillar rolls out products and services in each of its regions at different time intervals. Although every effort is made to ensure that product information is released only after Caterpillar has received confirmation from its independent dealer network, plants, and marketing subsidiaries that products and services are available in the relevant region, editors are kindly requested to verify with a Cat dealer for product availability and specifications.

CAT, CATERPILLAR, LET’S DO THE WORK, their respective logos, VisionLink, “Caterpillar Corporate Yellow,” the “Power Edge” and Cat “Modern Hex” trade dress, as well as corporate and product identity used herein, are trademarks of Caterpillar and may not be used without permission.

VisionLink is a trademark of Caterpillar Inc., registered in the United States and in other countries.

©2024 Caterpillar All Rights Reserved

 

 

Press Inquiries

Caterpillar Trade Press Media Representatives

Americas
Kate Kenny: Kenny_Kate@cat.com
Johanna Kelly: Kelly_Johanna_L@cat.com

Europe, Africa, Middle East
Amy Doughty: Amy.Doughty@cat.com

 

warning

Internet Explorer users may experience issues with certain features of our site.
Please try a current version of an alternate browser (i.e. Google Chrome, Microsoft Edge, Mozilla Firefox) for the full Cat.com experience.