Cat® PM300 Cold Planer series
Cat® PM300 Cold Planer series

Caterpillar announces updates to the Cat® PM300 Cold Planer series

 

For Worldwide Release: March 2024
Release Number: 104PR24

 

  • The latest engine offers increases in peak torque, gross power
  • Upgraded design to improve working environment for operators
  • Conveyor sealing redesigns contain more material and reduce build-up

 

Today’s Cat® PM310, PM312 and PM313 Cold Planers feature multiple design enhancements that help to improve machine performance, operating comfort and milling power. The PM300 Series excels in small to medium applications where a compact, highly maneuverable machine with high production capabilities is required.

The latest PM300 models integrate the Cat C9.3B engine that delivers an increase in gross power and more available torque, based on standard performance testing.

Offering a gross power rating of 256 kW (343 hp), the Cat C9.3B is available in configurations that meet U.S. EPA Tier 4 Final, EU Stage V, Korea Stage V emission standards or Brazil MAR-1 emission standards, equivalent to U.S. EPA Tier 3 and EU Stage IIIA.

The Cat C9.3B engine features lower complexity and improved electronic, fuel and air systems. Easier access to engine oil filters simplifies maintenance, while multipiece, cartridge-style engine filters reduce waste and lower replacement costs.

Performance, comfort upgrades

The latest PM300 series design includes a redesign of the transition flashing between primary and loading conveyors, improving containment of material and reducing build-up on the front machine frame. Further containment of material is achieved through feature enhancements to the right-hand side plate, chamber-to-conveyor sealing, and loading conveyor belt sealing. Front track deflectors positioned in front of the drive motors offer additional protection from debris impact and build-up, improving service life.

Operators can now track the cutting edge from either side of the machine thanks to the addition of an adjustable on-screen guidance line feature to the left-hand camera. Ground personnel can also now control the obstacle jump capability from the rear ground controls to improve milling efficiency.

Wide-dispersion LED working and LED roading light options for the PM310, PM312 and PM313 improve safety and visibility during milling and transportation around the jobsite. Offering the ability to be stowed when not in use, an exhaust deflector option redirects exhaust away from buildings and ground personnel to improve the working environment. The optional dust abatement ducting has been redesigned to further increase sealing and suction.

For more information about the most recent updates to the Cat PM310, PM312 and PM313 Cold Planers, contact a Cat dealer or visit www.cat.com.

 

Download the press release and images 

Download Now

 

 

of

Cat PM310 Cold Planer

View Full Size Image
of

Cat PM312 Cold Planer

View Full Size Image
of

Cat PM312 Cold Planer

View Full Size Image
of

Cat PM312 Cold Planer

View Full Size Image
of

Cat PM313 Cold Planer

View Full Size Image

Product & Service News

See the latest product and engine announcements from Caterpillar.

See the Latest News

 

 

# # #

 

Note to Editors: Caterpillar rolls out products and services in each of its regions at different time intervals. Although every effort is made to ensure that product information is released only after Caterpillar has received confirmation from its independent dealer network, plants, and marketing subsidiaries that products and services are available in the relevant region, editors are kindly requested to verify with a Cat dealer for product availability and specifications.


CAT, CATERPILLAR, LET’S DO THE WORK, their respective logos, VisionLink, “Caterpillar Corporate Yellow,” the “Power Edge” and Cat “Modern Hex” trade dress, as well as corporate and product identity used herein, are trademarks of Caterpillar and may not be used without permission.

©2023 Caterpillar. All Rights Reserved 

 

Press Inquiries

Caterpillar Trade Press Media Representatives

Americas

Kate Kenny: Kenny_Kate@cat.com

Johanna Kelly: Kelly_Johanna_L@cat.com

Europe, Africa, Middle East

Amy Doughty: Amy.Doughty@cat.com

 

warning

Internet Explorer users may experience issues with certain features of our site.
Please try a current version of an alternate browser (i.e. Google Chrome, Microsoft Edge, Mozilla Firefox) for the full Cat.com experience.