If you already have an existing account with another Cat App, you can use the same account to sign in here
One Account. All of Cat.
Your Caterpillar account is the single account you use to log in to select services and applications we offer. Shop for parts and machines online, manage your fleet, go mobile, and more.
Account Information
Site Settings
Security
For Release in Europe, Australia, and New Zealand: November 2022
Release Number: 772PR22
Cat® 349, 352, 374 and 395 large hydraulic excavators can now be equipped with Cat Command for Excavating. The remote-control system removes operators from potentially hazardous jobsite conditions by keeping them at a safe distance, and it reduces potential safety risks from climbing on and off machines.
The Cat Command station allows for non-line-of-sight remote control, where users can comfortably control all basic machine functions like digging, lifting and tracking. Additionally, Caterpillar exclusive machine technologies like Cat Grade with 3D for Excavators, Grade with Assist for boom and bucket, Swing Assist, E-Fence, and others can be set, activated, and used remotely.
The technology helps improve machine productivity on various projects like operating in unstable underfoot conditions, brownfields, shore work, and demolition. It also allows production to restart immediately following disruptive processes such as blasting in quarry applications.
Flexible, precise control
The Cat Command station provides non-line-of-site operation from the comfort of an air-conditioned office on site or many miles away. Distance is limited only by the capabilities of the network. The Cat Command station comfortably seats the operator in a customized “virtual cab” with familiar controls and machine displays. Users can control up to five different machines, one at a time, at the same or other locations, reducing downtime for shift changes or the need to travel to the jobsite. Touchscreen monitors similar to the in-cab displays offer the same machine information and access to machine setting just like in the machine. Screens mounted in front of the user provides an easy view of the excavator’s camera feeds.
By removing the operator from the cab, Cat Command for Excavating offers a solution to workforce shortages and training advantages for newer operators. It opens opportunities to those with physical limitations that prevent them from climbing into the equipment, attracting a new generation of workers, and increasing the longevity of experienced operators.
The new large hydraulic excavator models join the existing Cat Command-ready excavators (320-340) and medium dozers (D5- D7) which can be operated from the same Command station.
More information about Cat Command for Excavating can be found by contacting a Cat dealer.
# # #
Note to Editors: Caterpillar rolls out products and services in each of its territories at different time intervals. Although every effort is made to ensure that product information is released only after Caterpillar has received confirmation from our dealer network, our plants, and our marketing subsidiaries that products and services are available in the relevant region, editors are kindly requested to verify with their local dealer for product availability and specifications.
CAT, CATERPILLAR, LET’S DO THE WORK, their respective logos, VisionLink, “Caterpillar Corporate Yellow,” the “Power Edge” and Cat “Modern Hex” trade dress, as well as corporate and product identity used herein, are trademarks of Caterpillar and may not be used without permission.
©2022 Caterpillar All Rights Reserved
Press Inquiries |
Caterpillar Trade Press Media Representatives Americas Johanna Kelly: Kelly_Johanna_L@cat.com Europe, Africa, Middle East Francine Shore: Shore_Francine_M@cat.com |
Reader Requests |