New Cat® DG450 Compact Natural Gas Generator Set Expands Demand Response Opportunities for Customers in Non-attainment Areas

For Worldwide Release: March 28, 2024


IRVING, TEXAS – Caterpillar Inc. today announced the introduction of the Cat® DG450 Compact natural gas generator set, a new 450 kW ultra-low NOx power solution specifically configured for non-emergency applications in non-attainment areas designated by the U.S. Environmental Protection Agency (EPA).

Now available at Cat dealers throughout North America, the Cat DG450 Compact generator set uses up to 60% less space when compared with traditional multi-unit generator set specifications, reducing site preparation costs and offering budget-conscious power system redundancy. 

The new gas generator set is compatible with the Cat Active Management Platform (AMP), a proven distributed energy resource management system (DERMS) solution that helps customers monitor, manage, and monetize these natural gas generator sets and other Cat power solutions. It can be applied with other distributed energy resource (DER) system components, such as Cat Energy Storage Solutions, while also managing customer load reductions. The platform monitors patterns from the grid and client facilities, analyzes opportunities in the energy industry, and then dispatches DERs to maximize return and monetize results without disrupting normal business operations.

The Cat DG450 Compact generator set offers superior performance across a wide range of pipeline natural-gas fuel pressures. It is suitable for prime power, peak shaving and demand response applications, making it the versatile choice for small- and medium-sized industrial and manufacturing applications, agriculture facilities, municipal infrastructure, commercial enterprises and office buildings.

“As demand response programs become more prevalent as a means for rapidly expanding power capacity in non-attainment areas, the Cat DG450 Compact generator set is positioned to offer customers reliable solutions that can be readily monetized at times of high energy demand,” said Jaime Mineart, senior vice president of Caterpillar Electric Power Division.

Non-attainment areas are regions in the U.S. designated by the EPA that exceed limits for one or more criteria pollutants where local regulatory authorities may establish stationary emission limits that are more stringent than standard EPA levels. There are hundreds of U.S. counties designated as non-attainment areas, including Southern California, the Eastern Seaboard from New England through the mid-Atlantic, and large municipalities in East Texas.

The Cat DG450 Compact generator set is available with optional, factory-installed switchgear in an easy-to-use single- or multi-mains control module with automatic transfer switch capabilities. Its grid communication hardware enables the monitoring and control of multiple assets to facilitate DERs monetization, while pre-cut cable kit connection options simplify the installation of up to four units.

The generator set is designed to meet the NFPA power restoration requirement for Level 1 systems and accept 100 percent block load in one step. It meets ISO 8528-5 requirements for steady state and load acceptance, and it is UL 2200 listed.

Hardware is pre-installed on each generator set to enable access to Cat Connect Remote Asset Monitoring, which provides data visualization, reporting and alerts through an easy-to-use web interface or mobile app. Available with a subscription, it enables operators and Cat dealers to track and manage generator set operation, identify potential problems, perform remote troubleshooting, manage operational expenses, and leverage long-term archives of site performance history to identify opportunities for further operational and system enhancements.

Extensive Portfolio of Natural-Gas Power Solutions

The Cat DG450 Compact generator set is the latest addition to Caterpillar’s extensive line of power solutions fueled by natural gas, providing customers with a versatile range of options that generate power when needed while allowing them to participate in energy market programs.

The company recently introduced four new Cat gas generator sets for small- to medium-sized standby and demand response applications from 350 kW to 500 kW, offering improved power density, fuel efficiency and emissions performance.

Additionally, Caterpillar announced the introduction of 15 new gas generator sets from 20 to 200 kW rated for emergency standby, demand response and prime operation in small 60-Hz applications. They provide exceptional fuel flexibility by running on pipeline natural gas, propane and renewable natural gas with dual-fuel auto changeover technology, allowing users to connect both propane and natural gas sources to a single unit.

Caterpillar delivers innovative power systems engineered for durability, reliability and value. The company offers worldwide product support, with parts and services through customer value agreements available through the Cat authorized service and dealer network. In addition, Cat dealer technicians are trained to provide a comprehensive range of maintenance and services that help customers optimize the total cost of ownership of Cat equipment.

of

Cat® DG450 Compact natural gas generator set

Product and Services News

See the latest product and engine announcements from Caterpillar.

See the Latest News

 

###

 

About Caterpillar

With 2023 sales and revenues of $67.1 billion, Caterpillar Inc. is the world’s leading manufacturer of construction and mining equipment, off-highway diesel and natural gas engines, industrial gas turbines and diesel-electric locomotives. For 100 years, we’ve been helping customers build a better, more sustainable world and are committed and contributing to a reduced-carbon future. Our innovative products and services, backed by our global dealer network, provide exceptional value that helps customers succeed. Caterpillar does business on every continent, principally operating through three primary segments – Construction Industries, Resource Industries and Energy & Transportation – and providing financing and related services through our Financial Products segment. Visit us at caterpillar.com or join the conversation on our social media channels.

© 2024 Caterpillar. All Rights Reserved. CAT, CATERPILLAR, LET’S DO THE WORK, their respective logos, “Caterpillar Corporate Yellow,” the “Power Edge” and Cat “Modern Hex” trade dress, as well as corporate and product identity used herein, are trademarks of Caterpillar and may not be used without permission.

Press Inquiries

Bob Chase
Gelia
Tel: +1 716-629-3230
bchase@gelia.com

Amber Cawthorne
Caterpillar Inc.
Cawthorne_amber_r@cat.com

   

 

 

warning

Internet Explorer users may experience issues with certain features of our site.
Please try a current version of an alternate browser (i.e. Google Chrome, Microsoft Edge, Mozilla Firefox) for the full Cat.com experience.