Cat® Temporary Connection Boxes Are a Flexible New Solution  for Mobile Generator Sets

For Worldwide Release: September 2020 
Release Number: EEPR0220

DEERFIELD, IL –Caterpillar Inc. today introduced a flexible new family of Cat® temporary connection boxes for mobile generator sets. These facility connection boxes provide an easily accessible docking station to quickly connect a rental generator set to a building's electrical system, delivering temporary power in a matter of seconds. Typical markets include healthcare, pharmaceutical, industrial, manufacturing and light commercial construction.

Permanently mounted on the outside of a building, Cat temporary connection boxes feature a NEMA 3R weatherproof, wall-mounted enclosure with a door for cable access. Four configurations are offered to meet a range of needs.

  • The lug-to-lug tap box is designed for an application in which the end-user's connections to their distribution system are simply connected via lugs into the box, where mobile generator set cables are quickly landed to a second set of lugs. This configuration supports 200 to 3,000 amps.
  • An enclosed circuit breaker arrangement is also available for those who don't have a spare circuit breaker inside their building or are in need of additional circuit isolation for both safety and system protection. Supporting 200 to 800 amps, a circuit breaker disconnect and circuit protection are already built into the box and ready to utilize on a moment’s notice.
  • Two quick-connect weatherproof camlock configurations are also available with varied ampacity. The wall-mounted camlock tap box supports 400 to 2,400 amps, and the freestanding camlock tap box supports 1,600 to 4,000 amps.

"Understanding where and how to connect to your facility’s emergency power system is an essential component of a well-designed contingency preparedness plan," said Tom Caldwell, rental power general manager at Caterpillar. "The new Cat temporary connection boxes are designed with ancillary connection options, ensuring that Cat XQ mobile generator sets, which are immediately available through our extensive Cat dealer network and at Cat Rental Stores, can be safely and quickly connected to supply critical power during emergencies or when performing service on existing permanent units.”

Various options suited to meet individual needs can be selected that facilitate ease of use with Cat XQ mobile generator sets. For safety, a phase reversal relay provides visual indication of correct phase rotation. A remote start signal connection is also available so that the temporary generator set can be called on by the facility’s existing transfer switch, and a block heater shore power receptacle includes two 30-amp twist-lock receptacles wired to an internal disconnect to keep the mobile unit pre-warmed and ready for any outage.

"These boxes have been engineered to provide a simple connection for a mobile generator set or load bank, assuring the facility has a solid mechanism for maintaining and testing their permanent assets without interrupting their back-up power capabilities," said Marc Godwin, switchgear business development manager for Caterpillar. "A prime example are legally required emergency systems that provide power to hospitals and many other locations where reliable electric power is critical to ensure the safety of building occupants."

These new Cat temporary connection boxes are designed to help facility managers comply with recent updates to the U.S. National Electric Code (NEC) standards for emergency and standby power systems. The NEC requires facilities with an emergency generator set permanently installed in a standby application to provide an alternate source of electrical power in the event that the normal electrical power source is disabled for maintenance or otherwise unavailable.

Cat temporary connection boxes are now available for customers across North and South America. More information about them can be found at https://bit.ly/2EV2XjJ. A white paper was recently published about how the Electric Power industry can use connection boxes (docking boxes) for maintenance and it is available at https://bit.ly/3hTJHld.

Cat dealers have the ability to provide and install rental generator sets that may be quickly connected via these connection boxes in the event of a non-scheduled service need for the facility’s permanent generator set.

For more information about rental power, visit the Cat Rental Store online at www.catrentalstore.com. Details on our wide range of Cat Electric Power products and services can be found at cat.com/powergeneration or by emailing electric_power@cat.com. To stay up-to-date on the latest Electric Power news and interact with other power generation professionals, check out our social channels at www.cat.com/en_US/articles/social/ep-social-media.html

of

Cat® Temporary Connection Boxes

Product and Services News

See the latest product and engine announcements from Caterpillar.

See the Latest News

 

###

About Caterpillar

Since 1925, Caterpillar Inc. has been helping our customers build a better world – making sustainable progress possible and driving positive change on every continent. With 2019 sales and revenues of $53.8 billion, Caterpillar is the world’s leading manufacturer of construction and mining equipment, diesel and natural gas engines, industrial gas turbines, and diesel-electric locomotives. Services offered throughout the product life cycle, cutting-edge technology and decades of product expertise set Caterpillar apart, providing exceptional value to help our customers succeed. The company principally operates through three primary segments - Construction Industries, Resource Industries and Energy & Transportation - and provides financing and related services through its Financial Products segment. For more information, visit caterpillar.com. To connect on social media, visit caterpillar.com/social-media.

© 2020 Caterpillar. All Rights Reserved. CAT, CATERPILLAR, LET’S DO THE WORK, their respective logos, “Caterpillar Corporate Yellow,” the “Power Edge” and Cat “Modern Hex” trade dress, as well as corporate and product identity used herein, are trademarks of Caterpillar and may not be used without permission.

Press Inquiries

Erin Collins
Gelia
Tel: +1 716-629-3176
ecollins@gelia.com

Rachel Perva
Caterpillar Inc.
Tel: +1 309-675-7267
Perva_Rachel@cat.com

 

Reader Requests

Caterpillar Inc.
Electric Power Division
P.O. Box 0610
Mossville, IL 61552-0610

warning

Internet Explorer users may experience issues with certain features of our site.
Please try a current version of an alternate browser (i.e. Google Chrome, Microsoft Edge, Mozilla Firefox) for the full Cat.com experience.